<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 iMX RT1064, Segger, Debug Program &amp;gt;2MB</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/iMX-RT1064-Segger-Debug-Program-gt-2MB/m-p/1050427#M5644</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing a program for an iMX RT1064 using the Segger J-Link. My program has recently grown to greater than 2MB.&lt;/P&gt;&lt;P&gt;I am using 10.3 MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I debug, Segger J-Link downloads a small, low memory, 0x70002000, flash update as soon as I step from main(). Only one or two breakpoints are set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the same behavior when there are more breakpoints than are available in the hardware breakpoint list (6).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, after the brief download the program does not stop at the next instruction. It is always at a hardware fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I updated to 11.1 MCUXpresso and the problem appears to have been resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There appears to be possibly two related problems. 1) The mechanism to support breakpoints &amp;gt; hardware breakpoints is fixed (no hardware fault) and 2) The downloading of programs &amp;gt;2MB had some issue, also resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are these&amp;nbsp;known problems that were resolved in 11.1? Is so, please&amp;nbsp;indicate the release notes describing the resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;====&lt;/P&gt;&lt;P&gt;One reason I am using 10.3 MUCXpresso and not 11.1 is that I am unable to connect to NXP server to use Config to create mex files for the iMX RT1064.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The connection is in some way blocked by my company's firewall. However, 10.3 works just fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is first use of Config for iMX RT1064 requires retrieval from NXP for the 'config' definitions&amp;nbsp;for the RT1064. If I use Config not connected to my company's firewall, Config works as the file is downloaded and use of Config is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error is a network connection error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did report this issue. There was no response and I can't find the original post.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2020 11:09:39 GMT</pubDate>
    <dc:creator>Keith4DSmith</dc:creator>
    <dc:date>2020-05-06T11:09:39Z</dc:date>
    <item>
      <title>iMX RT1064, Segger, Debug Program &gt;2MB</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/iMX-RT1064-Segger-Debug-Program-gt-2MB/m-p/1050427#M5644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing a program for an iMX RT1064 using the Segger J-Link. My program has recently grown to greater than 2MB.&lt;/P&gt;&lt;P&gt;I am using 10.3 MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I debug, Segger J-Link downloads a small, low memory, 0x70002000, flash update as soon as I step from main(). Only one or two breakpoints are set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the same behavior when there are more breakpoints than are available in the hardware breakpoint list (6).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, after the brief download the program does not stop at the next instruction. It is always at a hardware fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I updated to 11.1 MCUXpresso and the problem appears to have been resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There appears to be possibly two related problems. 1) The mechanism to support breakpoints &amp;gt; hardware breakpoints is fixed (no hardware fault) and 2) The downloading of programs &amp;gt;2MB had some issue, also resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are these&amp;nbsp;known problems that were resolved in 11.1? Is so, please&amp;nbsp;indicate the release notes describing the resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;====&lt;/P&gt;&lt;P&gt;One reason I am using 10.3 MUCXpresso and not 11.1 is that I am unable to connect to NXP server to use Config to create mex files for the iMX RT1064.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The connection is in some way blocked by my company's firewall. However, 10.3 works just fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is first use of Config for iMX RT1064 requires retrieval from NXP for the 'config' definitions&amp;nbsp;for the RT1064. If I use Config not connected to my company's firewall, Config works as the file is downloaded and use of Config is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error is a network connection error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did report this issue. There was no response and I can't find the original post.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 11:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/iMX-RT1064-Segger-Debug-Program-gt-2MB/m-p/1050427#M5644</guid>
      <dc:creator>Keith4DSmith</dc:creator>
      <dc:date>2020-05-06T11:09:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX RT1064, Segger, Debug Program &gt;2MB</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/iMX-RT1064-Segger-Debug-Program-gt-2MB/m-p/1050428#M5645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-userid="40376" data-username="Keith4DSmith" href="https://community.nxp.com/people/Keith4DSmith"&gt;Keith Smith&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;The attachment is the release note of the MCUXpresso IDE, and I don't find the above two issue in it actually.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2020 02:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/iMX-RT1064-Segger-Debug-Program-gt-2MB/m-p/1050428#M5645</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-05-08T02:16:27Z</dc:date>
    </item>
  </channel>
</rss>