<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Refresh MCU Cache</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Refresh-MCU-Cache/m-p/1031231#M5454</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff,&lt;/P&gt;&lt;P&gt;Hope you are doing well.&lt;/P&gt;&lt;P&gt;If a project is built using part support from an SDK and is then exported – for example to share the project with a colleague who also uses MCUXpresso IDE, then the colleague must also install an SDK providing part support for the project’s MCU. Since&amp;nbsp;device support is included in the SDK, it is recommended that any required SDKs are installed before a project requiring SDK part support is imported. However, if this is not done beforehand, simply select the imported project in the project explorer and right click and select: C/C++ Build -&amp;gt; MCU settings ensure the correct MCU is selected and click &lt;STRONG&gt;Refresh MCU Cache&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 01 Mar 2020 23:29:41 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2020-03-01T23:29:41Z</dc:date>
    <item>
      <title>Refresh MCU Cache</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Refresh-MCU-Cache/m-p/1031230#M5453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can someone explain the '&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Refresh MCU Cache' button in the MCU Settings page of the project properties? What does it do, and how do I know when to use it? For reference, I'm using MCUXpresso 11.1.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Feb 2020 11:41:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Refresh-MCU-Cache/m-p/1031230#M5453</guid>
      <dc:creator>jeffthompson</dc:creator>
      <dc:date>2020-02-28T11:41:07Z</dc:date>
    </item>
    <item>
      <title>Re: Refresh MCU Cache</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Refresh-MCU-Cache/m-p/1031231#M5454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff,&lt;/P&gt;&lt;P&gt;Hope you are doing well.&lt;/P&gt;&lt;P&gt;If a project is built using part support from an SDK and is then exported – for example to share the project with a colleague who also uses MCUXpresso IDE, then the colleague must also install an SDK providing part support for the project’s MCU. Since&amp;nbsp;device support is included in the SDK, it is recommended that any required SDKs are installed before a project requiring SDK part support is imported. However, if this is not done beforehand, simply select the imported project in the project explorer and right click and select: C/C++ Build -&amp;gt; MCU settings ensure the correct MCU is selected and click &lt;STRONG&gt;Refresh MCU Cache&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Mar 2020 23:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Refresh-MCU-Cache/m-p/1031231#M5454</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-03-01T23:29:41Z</dc:date>
    </item>
  </channel>
</rss>