<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: &amp;quot;Could not connect to core&amp;quot; with LPCXpresso546xx board in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675352#M541</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The RevC board doesn't have a display, I have the one with the CAN shield. Also, I am powering through both J1 (power) and J8 (debug) through a powered USB hub. Still doesn't work.&lt;/P&gt;&lt;P&gt;If power was the issue, I also wouldn't understand why it works with no problem in uVision debugger and Flash Magic.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jul 2017 13:23:09 GMT</pubDate>
    <dc:creator>ChrisN</dc:creator>
    <dc:date>2017-07-19T13:23:09Z</dc:date>
    <item>
      <title>"Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675350#M539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have latest MCUXpresso 10.0.2 with all drivers updated. Windows 10 machine and starting with a simple gpio_led_output example from the SDK (2.2). I can build fine. When I start the debugger, I get to the "Connect to target: LPC54618J512" dialog that says "1 probe found". The probe name is "LPC-LINK2 CMSIS-DAP V5.182". Under "Supported Probes" there is "MCUXpresso IDE Link Server (incl. CMSIS-DAP) probes". So far so good.&lt;/P&gt;&lt;P&gt;When I continue I get these "Error reported by target", though:&lt;/P&gt;&lt;PRE&gt;&amp;nbsp; 02: Failed on connect
&amp;nbsp; Could not connect to core.
&amp;nbsp; 31: No connection to chip's debug port&lt;/PRE&gt;&lt;P&gt;In the console I see:&lt;/P&gt;&lt;PRE&gt;MCUXpresso RedlinkMulti Driver v10.0 (Jun 22 2017 23:31:55 - crt_emu_cm_redlink build 272)
Found chip XML file in C:/Users/XXXXX/Documents/MCUXpressoIDE_10.0.2_411/workspace/lpcxpresso54618_driver_examples_gpio_led_output/Debug\LPC54618J512.xml
(&amp;nbsp; 5) Remote configuration complete
Reconnected to existing redlink server (PID 4294967295)
Connecting to probe 1 core 0 (server PID unknown) gave 'Ee(36). Could not connect to core.'
Connecting to probe 1 core 0 (server PID unknown) gave 'Ee(36). Could not connect to core.'
Connecting to probe 1 core 0 (server PID unknown) gave 'Ee(36). Could not connect to core.'
Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(36). Could not connect to core.
Failed on connect: Ee(36). Could not connect to core.
No connection to chip's debug port
error closing down debug session - Em(02). MEM-AP is not selected.&lt;/PRE&gt;&lt;P&gt;The DFU-Link jumper JP5 is inserted but it doesn't matter even if I remove it since the debugger has the latest firmware.&lt;/P&gt;&lt;P&gt;The same board works fine in the Keil uVision debugger (with JP5 removed) and I can program it with Flash Magic (with JP5 inserted). My board is a Rev.C. I also have a second board (Rev.B) that behaves exactly the same.&lt;/P&gt;&lt;P&gt;I even tried the previous version 10.0.0 of MCUXpresso and I tried different USB ports (USB 2.0, 3.0, directly on the PC, via hub) but nothing makes any difference.&lt;/P&gt;&lt;P&gt;I am really at the end of my wits. Help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 09:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675350#M539</guid>
      <dc:creator>ChrisN</dc:creator>
      <dc:date>2017-07-19T09:15:26Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675351#M540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The normal issue with these boards is power (mainly due to the LCD on the back). Just relying on power supplied through the debug port is often not sufficient. Make sure you also power via J1/Power connector as well (preferably from a USB powered hub or USB power plug).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 10:13:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675351#M540</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-07-19T10:13:58Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675352#M541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The RevC board doesn't have a display, I have the one with the CAN shield. Also, I am powering through both J1 (power) and J8 (debug) through a powered USB hub. Still doesn't work.&lt;/P&gt;&lt;P&gt;If power was the issue, I also wouldn't understand why it works with no problem in uVision debugger and Flash Magic.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 13:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675352#M541</guid>
      <dc:creator>ChrisN</dc:creator>
      <dc:date>2017-07-19T13:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675353#M542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In that case, the next step is to check out section 14.12, "Using and troubleshooting LPC-Link2" of the MCUXpresso IDE v10.0.2 User Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 15:47:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675353#M542</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-07-19T15:47:48Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675354#M543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This was never resolved and I believe that something "deeper" is going on that warrants investigation.&lt;/P&gt;&lt;P&gt;With the LPCXpresso546xx board I had eventually worked around the issue by programming the on-board OpenSDA interface with the J-Link firmware which is thankfully also supported in MCUXpresso.&lt;/P&gt;&lt;P&gt;Now I have a FRDM-KW36 board here that I have to work with and J-Link firmware is not available. So I am back to CMSIS-DAP and back to the same "could not connect to core" issue also with this board.&lt;/P&gt;&lt;P&gt;I tried the ARM uVision debugger that also supports CMSIS-DAP and there, I can program the flash and debug without any apparent problems. So we can exclude any power/hardware/cabling issues or even issues with the USB drivers.&lt;/P&gt;&lt;P&gt;But in MCUXpresso, I was not even once successful in doing that, not even erasing the flash or anything, and this is what I'll have to use.&lt;/P&gt;&lt;P&gt;By the way, I got so desparate that I have reinstalled anything related to USB, used USB 2.0 setting in the BIOS, even used a plug-in (ExpressCard) USB controller card, all to no avail, all returning the same error. Of course a complete uninstall/reinstall of MCUXpresso, too, and I can't even count the number of times I have recreated a new startup configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;What can I do to track this down? Is there a way to turn on extra-verbose logging to see what's going on at low level?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 17:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675354#M543</guid>
      <dc:creator>ChrisN</dc:creator>
      <dc:date>2018-03-16T17:29:47Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675355#M544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We (and many many customers) use CMSIS-DAP connections actively on a daily basis with MCUXpresso IDE without any problem, so&amp;nbsp;I am sorry to hear that you continue to have problems.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regards to your LPCXpresso54608 board, I would suggest looking at&amp;nbsp;section 16.9, "Using and troubleshooting LPC-Link2" of the MCUXpresso IDE v10.1 User Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regards to&amp;nbsp;FRDM-KW36, the first thing to do is ensure that you have the latest probe firmware installed (from&amp;nbsp;&lt;A class="link-titled" href="http://nxp.com/opensda" title="http://nxp.com/opensda"&gt;OpenSDA Serial and Debug Adapter|NXP&lt;/A&gt;&amp;nbsp;). Also as you are using Windows 10, you might want to check out :&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-330935"&gt;Freedom OpenSDA Firmware Issues Reported on Windows 10&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But following on from that, please can you post the full text contents from the Debug log and redlinkserv consoles when you attempt to start a debug connection (as per section 16.8, "The Console View" of the MCUXpresso IDE v10.1 User Guide). &amp;nbsp;Please also check how your board shows up in Windows "Devices and Printers" when plugged in.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please also confirm the version of MCUXpresso IDE that you are currently using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Mar 2018 10:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675355#M544</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-19T10:01:25Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675356#M545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The tips from section 16.9, "Using and troubleshooting LPC-Link2" of the MCUXpresso IDE v10.1 User Guide I have already gone through to no avail. There is also no new probe firmware for the KW36 freedom board (it's not listed because it is so new) and since I am getting the same error with different boards and also whenever I am trying to use the LPC-Link2 I can say it happens the same with different versions of hardware and software. Lastly, the Windows 10 issue talk about the PC not being able to talk to the debug probe at all which is not my issue.&lt;/P&gt;&lt;P&gt;The debug log is:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;MCUXpresso RedlinkMulti Driver v10.1 (Dec 19 2017 16:58:35 - crt_emu_cm_redlink build 390)&lt;BR /&gt;Reconnected to existing redlink server (PID 4294967295)&lt;BR /&gt;Connecting to probe 1 core 0 (server PID unknown) gave 'Ee(36). Could not connect to core.'&lt;BR /&gt;Connecting to probe 1 core 0 (server PID unknown) gave 'Ee(36). Could not connect to core.'&lt;BR /&gt;Connecting to probe 1 core 0 (server PID unknown) gave 'Ee(36). Could not connect to core.'&lt;BR /&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(36). Could not connect to core.&lt;BR /&gt;Failed on connect: Ee(36). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port&lt;BR /&gt;error closing down debug session - Em(02). MEM-AP is not selected.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The redlinkserv console log is:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Connected on port 3025]&lt;BR /&gt;redlink&amp;gt;ProbeList&lt;BR /&gt;Index = 1&lt;BR /&gt;Manufacturer = ARM&lt;BR /&gt;Description = DAPLink CMSIS-DAP&lt;BR /&gt;Serial Number = 0251000041114e4500553004b60f003ea6e1000097969900&lt;BR /&gt;VID:PID = 0D28:0204&lt;BR /&gt;Path = \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#b&amp;amp;3020deaf&amp;amp;1&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;redlink&amp;gt;ProbeStatus&lt;BR /&gt;Index = 1&lt;BR /&gt;Manufacturer = ARM&lt;BR /&gt;Description = DAPLink CMSIS-DAP&lt;BR /&gt;Serial Number = 0251000041114e4500553004b60f003ea6e1000097969900&lt;BR /&gt;VID:PID = 0D28:0204&lt;BR /&gt;Path = \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#b&amp;amp;3020deaf&amp;amp;1&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;IsOpen = FALSE&lt;BR /&gt;WireInitialized = FALSE&lt;BR /&gt;WireProtocol = JTAG&lt;BR /&gt;CoresConfigured = FALSE&lt;BR /&gt;PacketSize = 64&lt;BR /&gt;Reference Count = 0&lt;BR /&gt;HasSWV = FALSE&lt;BR /&gt;HasETM = FALSE&lt;BR /&gt;HasJTAG = TRUE&lt;BR /&gt;HasSWD = TRUE&lt;BR /&gt;Probe Type = CMSIS-DAP&lt;BR /&gt;Probe Reference Count = 0&lt;BR /&gt;redlink&amp;gt;ProbeIsOpen 1&lt;BR /&gt;FALSE&lt;BR /&gt;redlink&amp;gt;ProbeOpenByIndex 1 &lt;BR /&gt;Probe not open&lt;BR /&gt;redlink&amp;gt;WireIsConnected 1&lt;BR /&gt;FALSE&lt;BR /&gt;redlink&amp;gt;WireSwdConnect 1&lt;BR /&gt;Probe not open&lt;BR /&gt;redlink&amp;gt;CoresConfigured 1&lt;BR /&gt;FALSE&lt;BR /&gt;redlink&amp;gt;CoreConfig 1&lt;BR /&gt;Probe not open&lt;BR /&gt;redlink&amp;gt;ProbeStatus&lt;BR /&gt;Index = 1&lt;BR /&gt;Manufacturer = ARM&lt;BR /&gt;Description = DAPLink CMSIS-DAP&lt;BR /&gt;Serial Number = 0251000041114e4500553004b60f003ea6e1000097969900&lt;BR /&gt;VID:PID = 0D28:0204&lt;BR /&gt;Path = \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#b&amp;amp;3020deaf&amp;amp;1&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;IsOpen = FALSE&lt;BR /&gt;WireInitialized = FALSE&lt;BR /&gt;WireProtocol = JTAG&lt;BR /&gt;CoresConfigured = FALSE&lt;BR /&gt;PacketSize = 64&lt;BR /&gt;Reference Count = 0&lt;BR /&gt;HasSWV = FALSE&lt;BR /&gt;HasETM = FALSE&lt;BR /&gt;HasJTAG = TRUE&lt;BR /&gt;HasSWD = TRUE&lt;BR /&gt;Probe Type = CMSIS-DAP&lt;BR /&gt;Probe Reference Count = 0&lt;BR /&gt;redlink&amp;gt;quit&lt;BR /&gt;[Closed]&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The MCUXpresso version is:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;MCUXpresso IDE v10.1.1 [Build 606] [2018-01-02]&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Mar 2018 20:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675356#M545</guid>
      <dc:creator>ChrisN</dc:creator>
      <dc:date>2018-03-25T20:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675357#M546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't reproduce your connection problem. This is a new part, so I'm curious if you were provided early access to the preliminary FRDM-KW36 SDK build. If so, what example project(s) are you attempting to debug? If you are not using an SDK, I'd like you to post a screen shot of your debug configuration settings. You need to specify the kinetisconnect.scp start up script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debug Configurations -&amp;gt; C/C++ (NXP Semiconductors) MCU Application -&amp;gt; &amp;lt;Project&amp;gt; Debug -&amp;gt; Debugger &amp;lt;tab&amp;gt; -&amp;gt; Connect Script&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Mar 2018 18:54:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675357#M546</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-26T18:54:57Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675358#M547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having the same issue with LPCXpresso1769 board.. I tested it with Ubuntu on the same machine, with MacOS on a MacBook. The board is working. However, on Windows it detects the probe, but gaves the following when debugging:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;"Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Dec 2018 14:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675358#M547</guid>
      <dc:creator>denizcan</dc:creator>
      <dc:date>2018-12-22T14:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675359#M548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I mentioned above, on unix systems it works, but on windows it does not.. Can it be a "path" problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Dec 2018 14:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675359#M548</guid>
      <dc:creator>denizcan</dc:creator>
      <dc:date>2018-12-22T14:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: "Could not connect to core" with LPCXpresso546xx board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675360#M549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reinstalling Windows solved issue.. That was a burden by the way..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Dec 2018 20:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/quot-Could-not-connect-to-core-quot-with-LPCXpresso546xx-board/m-p/675360#M549</guid>
      <dc:creator>denizcan</dc:creator>
      <dc:date>2018-12-27T20:30:42Z</dc:date>
    </item>
  </channel>
</rss>