<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: No middelware options while making new project</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613827#M54</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, there is an option in the IDE to enable the displaying of middleware components in the new project wizard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But as Erich stated, the current SDKs do not contain the required metadata to make this work correctly. Thus any such project you create is likely to not build successfully, certainly without manual tweaking, as the SDK metadata does not yet provide all of the necessary dependency data. This&amp;nbsp;is why the IDE option&amp;nbsp;hides the middleware components by&amp;nbsp;default. But having this&amp;nbsp;option means that once an enhanced SDK is&amp;nbsp;released, you will be able to turn on the ability to make use of it within&amp;nbsp;the IDE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 25 Mar 2017 11:47:38 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2017-03-25T11:47:38Z</dc:date>
    <item>
      <title>No middelware options while making new project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613824#M51</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our MCUXpresso-SDK is build with the middleware LwIP. If we then make a new project (file -&amp;gt; new -&amp;gt; project) and then new C/C++ project we can chose our SDK and we have all kind of options, like which OS, drivers etc. But I don't see any options to chose the middleware . &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I chose the middleware while make a new C/C++ project? Or do I have to copy it manually from the SDK to our newly crated project?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 15:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613824#M51</guid>
      <dc:creator>wilcovm</dc:creator>
      <dc:date>2017-03-23T15:49:13Z</dc:date>
    </item>
    <item>
      <title>Re: No middelware options while making new project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613825#M52</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wilco,&lt;/P&gt;&lt;P&gt;yes, this is currently not possible, becaue the SDK manifest file (XML description) does not include that information yet. To my understanding a future revision of the SDK should have this described in the manifest, so the middleware components beyond the RTOS can be included (or added later on).&lt;/P&gt;&lt;P&gt;Until then, you can import and clone existing middleware projects:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15605i8CDCBC1041928D08/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 20:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613825#M52</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-03-23T20:32:49Z</dc:date>
    </item>
    <item>
      <title>Re: No middelware options while making new project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613826#M53</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reaction. After playing around with the right settings a lot more I found a setting that will do the trick.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Windows -&amp;gt; Preferences &lt;BR /&gt;and then&lt;BR /&gt;MCUXpresso -&amp;gt; SDK Options&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There you can disable "hide middleware options ....".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By doing so it will enable or disable the middleware options when creating a new project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don'n know which xml file you mean but it seems the middleware is there as options when creating a new project. Until now I didn't test the middleware itself. Or is this the wrong way to do?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wilco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Mar 2017 08:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613826#M53</guid>
      <dc:creator>wilcovm</dc:creator>
      <dc:date>2017-03-25T08:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: No middelware options while making new project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613827#M54</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, there is an option in the IDE to enable the displaying of middleware components in the new project wizard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But as Erich stated, the current SDKs do not contain the required metadata to make this work correctly. Thus any such project you create is likely to not build successfully, certainly without manual tweaking, as the SDK metadata does not yet provide all of the necessary dependency data. This&amp;nbsp;is why the IDE option&amp;nbsp;hides the middleware components by&amp;nbsp;default. But having this&amp;nbsp;option means that once an enhanced SDK is&amp;nbsp;released, you will be able to turn on the ability to make use of it within&amp;nbsp;the IDE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Mar 2017 11:47:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613827#M54</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-03-25T11:47:38Z</dc:date>
    </item>
    <item>
      <title>Re: No middelware options while making new project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613828#M55</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wilco,&lt;/P&gt;&lt;P&gt;I think it is disabled for a reason. So projects you create that way might not compile/work without further edits.&lt;/P&gt;&lt;P&gt;But you certainly can go from there. Otherwise I would recommend to use one of the example projects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Mar 2017 11:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613828#M55</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-03-25T11:53:19Z</dc:date>
    </item>
    <item>
      <title>Re: No middelware options while making new project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613829#M56</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That’s interesting to know, thanks. I have two questions left.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Is this hide SDK option automatically disabled when importing a SDK that has the middleware functionality in the XML? Or does it only depend on the IDE version.&lt;/P&gt;&lt;P&gt;2) The only way to know the middleware should work, when installed by disabling the hide SDK option and cratering a new project, is by experiencing it when using?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wilco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Mar 2017 07:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/No-middelware-options-while-making-new-project/m-p/613829#M56</guid>
      <dc:creator>wilcovm</dc:creator>
      <dc:date>2017-03-27T07:27:29Z</dc:date>
    </item>
  </channel>
</rss>