<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NO PORTB or PORTE IRQ handler in KL26/KL16? in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/NO-PORTB-or-PORTE-IRQ-handler-in-KL26-KL16/m-p/1013901#M5301</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abhishek:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you are right. KL26 only supports external interrupt for PORTA,PORTC and PORTD.&amp;nbsp; No hardware support for interrupt IRQ PORTB and PORTE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Nov 2019 06:06:52 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2019-11-22T06:06:52Z</dc:date>
    <item>
      <title>NO PORTB or PORTE IRQ handler in KL26/KL16?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/NO-PORTB-or-PORTE-IRQ-handler-in-KL26-KL16/m-p/1013900#M5300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As per the KL26/KL16 series reference Manual, there are no IRQ handlers for PORT B and PORT E.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But PORT A is available (irq 30) and Port C and Port D are available on One ISR (irq 31).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to have PORT B and PORT E also to be used as Interrupt pins but they are unavailable to generate an ISFR bit set when they are configured as (PCR Reg using&amp;nbsp; PORT_SetPinInterruptConfig()).&lt;/P&gt;&lt;P&gt;Is this to say there are no Hardware module present internal to chip responsible for these ports Interrupt. ( ISFR are available but they are going to be useless) there is no hardware detection for when these port pins are asserted?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also,&amp;nbsp;is there a way to configure them at all on KL chips? As also software interrupts are also not available on KL chips/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Advise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Abhi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 23:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/NO-PORTB-or-PORTE-IRQ-handler-in-KL26-KL16/m-p/1013900#M5300</guid>
      <dc:creator>abhishekvishwak</dc:creator>
      <dc:date>2019-11-19T23:13:39Z</dc:date>
    </item>
    <item>
      <title>Re: NO PORTB or PORTE IRQ handler in KL26/KL16?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/NO-PORTB-or-PORTE-IRQ-handler-in-KL26-KL16/m-p/1013901#M5301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abhishek:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you are right. KL26 only supports external interrupt for PORTA,PORTC and PORTD.&amp;nbsp; No hardware support for interrupt IRQ PORTB and PORTE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Nov 2019 06:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/NO-PORTB-or-PORTE-IRQ-handler-in-KL26-KL16/m-p/1013901#M5301</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-11-22T06:06:52Z</dc:date>
    </item>
    <item>
      <title>Re: NO PORTB or PORTE IRQ handler in KL26/KL16?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/NO-PORTB-or-PORTE-IRQ-handler-in-KL26-KL16/m-p/1013902#M5302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply, Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 16:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/NO-PORTB-or-PORTE-IRQ-handler-in-KL26-KL16/m-p/1013902#M5302</guid>
      <dc:creator>abhishekvishwak</dc:creator>
      <dc:date>2019-11-27T16:14:10Z</dc:date>
    </item>
  </channel>
</rss>