<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using MCUXprsesso IDE with non NXP target in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Using-MCUXprsesso-IDE-with-non-NXP-target/m-p/997976#M5136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your replying,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand it's non-NXP device, and I didn't expect&amp;nbsp;support as such. Was just wondering if any users have used the same IDE for non-NXP targets.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;It's a great tool, and with non NXP locked hardware debugger/monitor it could work for other SoC /MCU makers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Jan 2020 01:43:01 GMT</pubDate>
    <dc:creator>dry</dc:creator>
    <dc:date>2020-01-12T01:43:01Z</dc:date>
    <item>
      <title>Using MCUXprsesso IDE with non NXP target</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Using-MCUXprsesso-IDE-with-non-NXP-target/m-p/997974#M5134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to use MCUXpresso for a non Freescale/NXP board/target, for it's built-in IDE debugging functionality and integration with J-Link.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Anyone has ever done it successfully?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;I'm&amp;nbsp;seasoned with J-Link , I would say, and I can start GDBServer on command line and load and start debugging my target with the sample binary I built - no issues&amp;nbsp; at that level.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;With MCUXpresso , after configuring the Segger J-Link launch profile, I get into error which says (non exact copy)&amp;nbsp; cannot acquire jtag .. Which is odd, as I configure J-Link GDBServer to use SWD to begin with.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;I can see, from the log/console, that the GDBServer is launched correctly, and connects to the target with no-errors, but the error it _seems_ coming from some stage at or after gdb client invocation - I do not see it connecting to server, just exist , it seems, after running some init script.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;I don't know how / what that Segger J-link plugin in MCUXpresso does wrt to target selection: i can see the list is limited to NXP /Freescale chips only. So does that mean it does some other 'magic' behind the scene besides just passing this parameter as the value to "-device XXX" to the J-Link?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;(Because, ultimately I'm replacing that -device flag with non-NXP device )&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Nov 2019 12:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Using-MCUXprsesso-IDE-with-non-NXP-target/m-p/997974#M5134</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2019-11-02T12:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: Using MCUXprsesso IDE with non NXP target</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Using-MCUXprsesso-IDE-with-non-NXP-target/m-p/997975#M5135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MCUXpresso IDE is explicitly designed and licensed for use with NXP's MCUs - in particular LPC, Kinetis and i.MX RT devices. &amp;nbsp;Thus&amp;nbsp;I am afraid that we cannot provide any assistance with use of MCUXpresso IDE with non-NXP devices.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2019 20:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Using-MCUXprsesso-IDE-with-non-NXP-target/m-p/997975#M5135</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-11-04T20:27:25Z</dc:date>
    </item>
    <item>
      <title>Re: Using MCUXprsesso IDE with non NXP target</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Using-MCUXprsesso-IDE-with-non-NXP-target/m-p/997976#M5136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your replying,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand it's non-NXP device, and I didn't expect&amp;nbsp;support as such. Was just wondering if any users have used the same IDE for non-NXP targets.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;It's a great tool, and with non NXP locked hardware debugger/monitor it could work for other SoC /MCU makers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jan 2020 01:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Using-MCUXprsesso-IDE-with-non-NXP-target/m-p/997976#M5136</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2020-01-12T01:43:01Z</dc:date>
    </item>
  </channel>
</rss>