<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S69 cycle counter in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC55S69-cycle-counter/m-p/987954#M5007</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to profile a code with&amp;nbsp; LPCXpresso55S69. I am using MCUXpresso IDE.I load the hello_world_swo project example. I run the specific function (From Breakpoint to Breakpoint) with 12MHz clock default from the Project and &lt;STRONG&gt;cycles&amp;nbsp;&lt;/STRONG&gt;Register (or same&amp;nbsp;&lt;STRONG&gt;Cycle Counter&lt;/STRONG&gt; from&amp;nbsp; SWO) had the value 38765.&lt;/P&gt;&lt;P&gt;After that, i tried to run the same code with 150MHz clock ( i replaced&amp;nbsp;&amp;nbsp;BOARD_BootClockFRO12M(); with&amp;nbsp;&amp;nbsp;BOARD_BootClockPLL150M() ) and the &lt;STRONG&gt;cycles&amp;nbsp;&lt;/STRONG&gt;value was 51400.&lt;/P&gt;&lt;P&gt;All the other project settings was the same.&lt;/P&gt;&lt;P&gt;1)Shouldn't be these cycles the same and independent from the clock of the system while the code is exactly the same?&lt;/P&gt;&lt;P&gt;2)Am i missing something?&amp;nbsp;&lt;/P&gt;&lt;P&gt;3)Is there something else i should change to run 150MHz clock?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Theo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2020 13:22:55 GMT</pubDate>
    <dc:creator>tkontogiorgis</dc:creator>
    <dc:date>2020-03-19T13:22:55Z</dc:date>
    <item>
      <title>LPC55S69 cycle counter</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC55S69-cycle-counter/m-p/987954#M5007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to profile a code with&amp;nbsp; LPCXpresso55S69. I am using MCUXpresso IDE.I load the hello_world_swo project example. I run the specific function (From Breakpoint to Breakpoint) with 12MHz clock default from the Project and &lt;STRONG&gt;cycles&amp;nbsp;&lt;/STRONG&gt;Register (or same&amp;nbsp;&lt;STRONG&gt;Cycle Counter&lt;/STRONG&gt; from&amp;nbsp; SWO) had the value 38765.&lt;/P&gt;&lt;P&gt;After that, i tried to run the same code with 150MHz clock ( i replaced&amp;nbsp;&amp;nbsp;BOARD_BootClockFRO12M(); with&amp;nbsp;&amp;nbsp;BOARD_BootClockPLL150M() ) and the &lt;STRONG&gt;cycles&amp;nbsp;&lt;/STRONG&gt;value was 51400.&lt;/P&gt;&lt;P&gt;All the other project settings was the same.&lt;/P&gt;&lt;P&gt;1)Shouldn't be these cycles the same and independent from the clock of the system while the code is exactly the same?&lt;/P&gt;&lt;P&gt;2)Am i missing something?&amp;nbsp;&lt;/P&gt;&lt;P&gt;3)Is there something else i should change to run 150MHz clock?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Theo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 13:22:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC55S69-cycle-counter/m-p/987954#M5007</guid>
      <dc:creator>tkontogiorgis</dc:creator>
      <dc:date>2020-03-19T13:22:55Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 cycle counter</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC55S69-cycle-counter/m-p/987955#M5008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No. The flash is not zero wait state, and is has different wait states for higher frequencies.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 18:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC55S69-cycle-counter/m-p/987955#M5008</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-03-19T18:06:42Z</dc:date>
    </item>
  </channel>
</rss>