<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: MCUXpresso on Linux</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983338#M4981</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I received the solution via the Manjaro forum. This method was quick and painless.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So for Linux Manjaro users, you need to enable AUR support in Pamac, then search for &lt;CODE&gt;mcuxpresso&lt;/CODE&gt; and you will get two available packages for the IDE and one for the config tools.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; If done from terminal: First search and confirm version availability&lt;BR /&gt; &lt;CODE&gt;pamac search mcuxpresso&lt;/CODE&gt;&lt;BR /&gt; For the latest version available on AUR, just run:&lt;BR /&gt; &lt;CODE&gt;pamac build mcuxpresso-ide&lt;/CODE&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jun 2020 14:08:17 GMT</pubDate>
    <dc:creator>gerrikoio</dc:creator>
    <dc:date>2020-06-04T14:08:17Z</dc:date>
    <item>
      <title>MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983335#M4978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I installed MCUXPresso on three different versions of Linux (as an experiment to decide which version to use).&lt;/P&gt;&lt;P&gt;I can't get it to install on Manjaro (Arch Linux), it appears to work perfectly on Mint (Ubuntu) and almost works on Elementary OS (also Ubuntu).&lt;/P&gt;&lt;P&gt;The Elementary OS Faults are the most interesting:&lt;/P&gt;&lt;P&gt;1) Whenever it opens a window it is drawn centred on another identically titled but transparent window that is 50% bigger.&lt;/P&gt;&lt;P&gt;2) It won't build - gives the error&amp;nbsp;&lt;/P&gt;&lt;P&gt;"make -r -j4 all&lt;/P&gt;&lt;P&gt;Cannot run program "make": Unknown error&lt;/P&gt;&lt;P&gt;Error: Program "make" not found in path."&lt;/P&gt;&lt;P&gt;I have tried this on three laptops, all using the same download of the .deb.bin file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas? Especially on Elementary OS, as that would be my preferred version (though currently Mint has to be my preferred version due to being the only one that works)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 16:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983335#M4978</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2019-11-13T16:45:54Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983336#M4979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;I don’t think that Elementary OS is a very popular Linux Distro - at least as far as this forum goes.&amp;nbsp;Therefore, I think it unlikely somebody here is going to be able to help you. You will also be on a system that is not going to be supported by NXP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, you might try searching for ‘installing eclipse on Elementary OS’ to see what other people have been doing to get Eclipse working on your OS (MCUXpresso uses Eclipse).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your OS doesn’t have make, you are going to need to install a development package that includes it. I think you need the build-essential package.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 17:12:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983336#M4979</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2019-11-13T17:12:32Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983337#M4980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I too can't get it to install on Manjaro (Arch Linux). I have found an option to manually convert a debian package to arch linux but this is no good with the auto installer. Was there a reason for using this auto installer process as not very generic, in my opinion, considering there are other Linux distro's out there. I note that other vendors use compressed tar.gz files which works. For example, the standard Eclipse IDE installer too have an easy Linux install method too. Maybe replicate this method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, please could you advise as how to install on Manjaro (Arch Linux). Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2020 17:38:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983337#M4980</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2020-06-03T17:38:50Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983338#M4981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I received the solution via the Manjaro forum. This method was quick and painless.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So for Linux Manjaro users, you need to enable AUR support in Pamac, then search for &lt;CODE&gt;mcuxpresso&lt;/CODE&gt; and you will get two available packages for the IDE and one for the config tools.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; If done from terminal: First search and confirm version availability&lt;BR /&gt; &lt;CODE&gt;pamac search mcuxpresso&lt;/CODE&gt;&lt;BR /&gt; For the latest version available on AUR, just run:&lt;BR /&gt; &lt;CODE&gt;pamac build mcuxpresso-ide&lt;/CODE&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 14:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983338#M4981</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2020-06-04T14:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983339#M4982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I did this and it surely installs MCUXpresso but it doesn't work properly i.e I can't install any board on it. How do you use it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2020 07:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/983339#M4982</guid>
      <dc:creator>alvarobolro</dc:creator>
      <dc:date>2020-07-08T07:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/1138829#M6101</link>
      <description>&lt;P&gt;Did you ever resolve this issue? I have had to download the board packages and drag the zip files myself. However I don't get&amp;nbsp; update notifications&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 19:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-on-Linux/m-p/1138829#M6101</guid>
      <dc:creator>aguirrem</dc:creator>
      <dc:date>2020-09-03T19:09:24Z</dc:date>
    </item>
  </channel>
</rss>