<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: foreard-looking Project setup in MCUExpresso</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/foreard-looking-Project-setup-in-MCUExpresso/m-p/669581#M483</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Christian.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if I understand your question accurately. From I understanding you started your project based on an existing SDK demo code, and you need add your own code/file to it. Correct?&lt;/P&gt;&lt;P&gt;If yes, you can do it. But we need to know SDK uses its own header file, start up code,etc. User code must&amp;nbsp; be compatible with these SDK files. Thus I suggest you add user code part by part. If you need add new file, please also make sure the file path is included in the project path setting.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 May 2017 08:07:34 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2017-05-19T08:07:34Z</dc:date>
    <item>
      <title>foreard-looking Project setup in MCUExpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/foreard-looking-Project-setup-in-MCUExpresso/m-p/669580#M482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We started our project based on a SDK example. &lt;/P&gt;&lt;P&gt;Now, how do we need to re-arrange our files in order to be able to update the SDK with minimal effort on our own files?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 13:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/foreard-looking-Project-setup-in-MCUExpresso/m-p/669580#M482</guid>
      <dc:creator>christianhonegg</dc:creator>
      <dc:date>2017-05-05T13:31:46Z</dc:date>
    </item>
    <item>
      <title>Re: foreard-looking Project setup in MCUExpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/foreard-looking-Project-setup-in-MCUExpresso/m-p/669581#M483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Christian.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if I understand your question accurately. From I understanding you started your project based on an existing SDK demo code, and you need add your own code/file to it. Correct?&lt;/P&gt;&lt;P&gt;If yes, you can do it. But we need to know SDK uses its own header file, start up code,etc. User code must&amp;nbsp; be compatible with these SDK files. Thus I suggest you add user code part by part. If you need add new file, please also make sure the file path is included in the project path setting.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 May 2017 08:07:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/foreard-looking-Project-setup-in-MCUExpresso/m-p/669581#M483</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-05-19T08:07:34Z</dc:date>
    </item>
  </channel>
</rss>