<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCUXpresso IDE 11.0.0 dbus-launch errors in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-0-0-dbus-launch-errors/m-p/956348#M4653</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I install MCUXpresso inside an Ubuntu 16.04 64-bit VM with minimum dependencies and noticed the following error in the console when trying to launch dialog boxes (which still appeared to work however).&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;(MCUXpresso IDE:17774): dconf-WARNING **: failed to commit changes to dconf: Failed to execute child process "dbus-launch" (No such file or directory)&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;This is caused by the missing dependency on &lt;SPAN style="font-family: 'andale mono', monospace;"&gt;dbus-x11&lt;/SPAN&gt;, which I fix with the following.&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;apt-get install -y dbus-x11
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jun 2019 11:49:53 GMT</pubDate>
    <dc:creator>lucasrangit</dc:creator>
    <dc:date>2019-06-21T11:49:53Z</dc:date>
    <item>
      <title>MCUXpresso IDE 11.0.0 dbus-launch errors</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-0-0-dbus-launch-errors/m-p/956348#M4653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I install MCUXpresso inside an Ubuntu 16.04 64-bit VM with minimum dependencies and noticed the following error in the console when trying to launch dialog boxes (which still appeared to work however).&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;(MCUXpresso IDE:17774): dconf-WARNING **: failed to commit changes to dconf: Failed to execute child process "dbus-launch" (No such file or directory)&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;This is caused by the missing dependency on &lt;SPAN style="font-family: 'andale mono', monospace;"&gt;dbus-x11&lt;/SPAN&gt;, which I fix with the following.&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;apt-get install -y dbus-x11
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2019 11:49:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-0-0-dbus-launch-errors/m-p/956348#M4653</guid>
      <dc:creator>lucasrangit</dc:creator>
      <dc:date>2019-06-21T11:49:53Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE 11.0.0 dbus-launch errors</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-0-0-dbus-launch-errors/m-p/956349#M4654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your feedback. It sounds like you have installed a more minimal install of Ubuntu than we have done during our testing. We'll log this dependency issue for fixing in a future IDE release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 09:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-0-0-dbus-launch-errors/m-p/956349#M4654</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-06-24T09:34:28Z</dc:date>
    </item>
  </channel>
</rss>