<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: peripherals+ view is empty</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667551#M464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use P&amp;amp;E OpenSDA interface with FRDM-K64F. There is no problem to check registers in prepheral+ window. See attached video.&lt;/P&gt;&lt;P&gt;I also attach the FRDM-K64F P&amp;amp;E OpenSDA interface I am using.&lt;/P&gt;&lt;P&gt;How it works if you follow the same steps?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 May 2017 06:51:10 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2017-05-05T06:51:10Z</dc:date>
    <item>
      <title>peripherals+ view is empty</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667550#M463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have installe KSDK 2.2 for FRDM-K64 but peripherals+ view is empty&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19894i3B91A85D138A275A/image-size/large?v=v2&amp;amp;px=999" title="Schermata del 2017-05-04 18-08-53.png" alt="Schermata del 2017-05-04 18-08-53.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the project preferences I have set correctly the MCU&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19941i421DCD68308770C1/image-size/large?v=v2&amp;amp;px=999" title="Istantanea_2017-05-04_18-12-45.png" alt="Istantanea_2017-05-04_18-12-45.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where am I wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 16:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667550#M463</guid>
      <dc:creator>mastupristi</dc:creator>
      <dc:date>2017-05-04T16:15:33Z</dc:date>
    </item>
    <item>
      <title>Re: peripherals+ view is empty</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667551#M464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use P&amp;amp;E OpenSDA interface with FRDM-K64F. There is no problem to check registers in prepheral+ window. See attached video.&lt;/P&gt;&lt;P&gt;I also attach the FRDM-K64F P&amp;amp;E OpenSDA interface I am using.&lt;/P&gt;&lt;P&gt;How it works if you follow the same steps?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 06:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667551#M464</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-05-05T06:51:10Z</dc:date>
    </item>
    <item>
      <title>Re: peripherals+ view is empty</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667552#M465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is this actually an IDE created project - did you actually use the "Import SDK examples" or "New project" options in the Quickstart Panel? If you created it via other mechanisms, then it is quite probable that the appropriate settings and linkages are not in place.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 11:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667552#M465</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-05-05T11:03:53Z</dc:date>
    </item>
    <item>
      <title>Re: peripherals+ view is empty</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667553#M466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro" style="min-height: 8pt; padding: 0px;"&gt;Is this actually an IDE created project - did you actually use the "Import SDK examples" or "New project" options in the Quickstart Panel? If you created it via other mechanisms, then it is quite probable that the appropriate settings and linkages are not in place.&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is a project that works fine in KDS 3.2, it a makefile project, and in KDS I can debug and access periphreral registers through EmbSys register view. I tryed to to import it (Existing code as Makefile project) in MCUXpresso ide, the I setup MCU as depicted by screenshots, but something is missing, since the peripherals+ view is still empty.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 12:52:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/peripherals-view-is-empty/m-p/667553#M466</guid>
      <dc:creator>mastupristi</dc:creator>
      <dc:date>2017-05-05T12:52:08Z</dc:date>
    </item>
  </channel>
</rss>