<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: MCUXpresso Debug Questions</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Debug-Questions/m-p/950131#M4566</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Just discovered that the LPC Link2 doesn't work for the 1347&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Why do you think this? I would expect no issue using LPC-Link2 with an LPC1347.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the assumption that you have the LPC1347 mounted on your own board (rather than an off-the-shelf one), then make sure you check&amp;nbsp;&lt;A href="https://community.nxp.com/message/630601"&gt;https://community.nxp.com/message/630601&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And to debug, all you should need to do is click the "Debug" button in the Quickstart Panel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jul 2019 13:33:52 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2019-07-23T13:33:52Z</dc:date>
    <item>
      <title>MCUXpresso Debug Questions</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Debug-Questions/m-p/950129#M4564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm nu-bee so any pointers are gratefully appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're committed to using the LPC1347 MCU. .A nice chip.&amp;nbsp;Just discovered that the LPC Link2 doesn't work for the 1347, so&amp;nbsp;we have a new LPC Link1 connected.&lt;/P&gt;&lt;P&gt;Question#1: I have only the 4 wire SWDIO/.SWCLK lines connected. The LPC1347 does not support Instruction trace I discovered. What other debug features don't work for this chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question2: is it necessary to do a Debug-build in MCUXpresso when using the LPC Link, or just leave it set as a Release build and click Debug? Debug As? where is the best place to invoke the debugger? I've noticed dong the latter doesn't the Debug/Release property for all the included projects in the build. Is it necessary t manually setup all files for Debug. Or can you just Debug a release build and the right thing happens?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question3: Does Debug as "local C/C++ application" actually run a software emulator in a window somewhere? what are the limitations of that? Can external Input be emulated?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Jul 2019 22:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Debug-Questions/m-p/950129#M4564</guid>
      <dc:creator>harvey1</dc:creator>
      <dc:date>2019-07-21T22:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Debug Questions</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Debug-Questions/m-p/950130#M4565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="344980" data-username="harvey@starrlabs.com" href="https://community.nxp.com/people/harvey@starrlabs.com"&gt;Harvey Starr&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Question#1:The LPC1347 does not support Instruction trace I discovered. What other debug features don't work for this chip?&lt;/P&gt;&lt;P&gt;I just wondering why do you think LPC1347 doesn't support Instruction Trace?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2&amp;amp;Q3:&amp;nbsp; About debug on MCUXpresso IDE, please refer to &amp;lt;MCUXpresso_IDE_User_Guide.pdf&amp;gt; -&amp;gt;&lt;/P&gt;&lt;P&gt;5.1 Starting a Debug Session&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 02:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Debug-Questions/m-p/950130#M4565</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-07-23T02:27:35Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Debug Questions</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Debug-Questions/m-p/950131#M4566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Just discovered that the LPC Link2 doesn't work for the 1347&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Why do you think this? I would expect no issue using LPC-Link2 with an LPC1347.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the assumption that you have the LPC1347 mounted on your own board (rather than an off-the-shelf one), then make sure you check&amp;nbsp;&lt;A href="https://community.nxp.com/message/630601"&gt;https://community.nxp.com/message/630601&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And to debug, all you should need to do is click the "Debug" button in the Quickstart Panel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 13:33:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Debug-Questions/m-p/950131#M4566</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-07-23T13:33:52Z</dc:date>
    </item>
  </channel>
</rss>