<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCUXpresso error in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939226#M4367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I only have one board connected to my pc when I am debugging a project, and all jumpers are in the same default place, but the 2 boards are not working and have the same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to change Non Bridged or VCOM but still same problem.&lt;/P&gt;&lt;P&gt;I also tried to install LPCScrypt and run Program_CMSIS but still same problem.&lt;/P&gt;&lt;P&gt;I have installed MCUXpresso and the SDK on an new other computer (windows this time), and I have the exactly same problem/error (with a new SDK code example this time).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is it not working since yesterday ? (I think it started after&amp;nbsp;I tried an SDK SPI Slave code example where I shorted JP6 but I am not sure because it worked a few time after this)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And how do I solve this annoying and frustrating problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much in advance,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hugo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jul 2019 12:29:04 GMT</pubDate>
    <dc:creator>hugo_nicolas</dc:creator>
    <dc:date>2019-07-04T12:29:04Z</dc:date>
    <item>
      <title>MCUXpresso error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939224#M4365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with 2 LPCXpresso5411x board and since yesterday, I can not use both of them because I am not able to see the probe in MCUXpresso, often, it even says :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture d’écran 2019-07-04 à 10.08.33.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90384i42B94BE5514F8F9F/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture d’écran 2019-07-04 à 10.08.33.png" alt="Capture d’écran 2019-07-04 à 10.08.33.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the board is heating very quickly (around U25,Y2, and the probe).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I solve this problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hugo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 08:12:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939224#M4365</guid>
      <dc:creator>hugo_nicolas</dc:creator>
      <dc:date>2019-07-04T08:12:17Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939225#M4366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hugo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are trying to use two LPCXpresso Boards connected to a single PC then you must be aware of a couple of things:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - if the 'DFU Link' is fitted - these board will expect to boot with LPC-Link2 firmware by default.&lt;/P&gt;&lt;P&gt;a - only one unbooted board can be connected at any time&lt;/P&gt;&lt;P&gt;b - the default version of LPC-Link2 firmware requests a large USB bandwidth from the host OS - it is unlikely that the OS can fully support two (full) LPC-Link2 implementations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE can offer to boot lower bandwidth versions of LPC-Link2 via a preferences - I would suggest setting the Non Bridged or VCOM options:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90399iA80209BA24A1E412/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2 - if the DFU Link is not fitted, then a prebuilt version of firmware will be used (if present). If multiple boards are to be used then pre-built firmware is preferred since this avoids the DFU boot issue mentioned above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The utility &lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2.1.0:LPCSCRYPT" title="https://www.nxp.com/support/developer-resources/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2.1.0:LPCSCRYPT"&gt;LPCScrypt v2.1.0 | NXP&lt;/A&gt; can be used to program LPC-Link2 firmware onto these boards. Again, I would recommend using the Non Bridged or Serial versions to avoid exceeding the bandwidth of the Host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I am mistaken and you are simply unable to use a single board - please restart the IDE, create a new project and perform a debug operation via the Quick Start Panel 'Debug' button, then send us a copy of the Debug log (Console -&amp;gt; Debug Messages).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 11:14:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939225#M4366</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-07-04T11:14:23Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939226#M4367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I only have one board connected to my pc when I am debugging a project, and all jumpers are in the same default place, but the 2 boards are not working and have the same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to change Non Bridged or VCOM but still same problem.&lt;/P&gt;&lt;P&gt;I also tried to install LPCScrypt and run Program_CMSIS but still same problem.&lt;/P&gt;&lt;P&gt;I have installed MCUXpresso and the SDK on an new other computer (windows this time), and I have the exactly same problem/error (with a new SDK code example this time).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is it not working since yesterday ? (I think it started after&amp;nbsp;I tried an SDK SPI Slave code example where I shorted JP6 but I am not sure because it worked a few time after this)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And how do I solve this annoying and frustrating problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much in advance,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hugo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 12:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939226#M4367</guid>
      <dc:creator>hugo_nicolas</dc:creator>
      <dc:date>2019-07-04T12:29:04Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939227#M4368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like I have finally solved the problem by plugging the board (using the 2 USB cables), and pushing ISP0. While ISP0 is still pushed, press and release RESET, and then release ISP0. The board is now usable (both of them).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hugo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 08:04:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-error/m-p/939227#M4368</guid>
      <dc:creator>hugo_nicolas</dc:creator>
      <dc:date>2019-07-05T08:04:06Z</dc:date>
    </item>
  </channel>
</rss>