<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933710#M4298</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For production programming, use a dedicated device for this, e.g. the Cyclone: &lt;A class="jivelink12" href="http://www.pemicro.com/cyclone/" title="http://www.pemicro.com/cyclone/"&gt;http://www.pemicro.com/cyclone/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jul 2019 13:59:30 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2019-07-03T13:59:30Z</dc:date>
    <item>
      <title>How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933706#M4294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder how could I flash KL27 processor in a custom board that I developed.&lt;/P&gt;&lt;P&gt;I have the code in .bin format and the PE micro multlink universal fx.&lt;/P&gt;&lt;P&gt;Is there a way to program the board using MCUxpresso IDE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;João Paulo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2019 21:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933706#M4294</guid>
      <dc:creator>joãopaulo</dc:creator>
      <dc:date>2019-07-02T21:39:34Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933707#M4295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See &lt;A class="link-titled" href="https://mcuoneclipse.com/2017/05/06/using-eclipse-to-program-binary-files-to-an-embedded-target/" title="https://mcuoneclipse.com/2017/05/06/using-eclipse-to-program-binary-files-to-an-embedded-target/"&gt;Using Eclipse to Program Binary Files to an Embedded Target | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2019 06:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933707#M4295</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-07-03T06:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933708#M4296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="303323" data-username="joãopaulo" href="https://community.nxp.com/people/joãopaulo"&gt;João Paulo&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our current integration of the PE Micro debug solution only support the flash programming of .axf files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, LinkServer (CMSIS-DAP) and SEGGER JLink debug solutions do offer support for binary file programming. We hope to bring in this feature in a later release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2019 10:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933708#M4296</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-07-03T10:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933709#M4297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't want to debug anymore, the project is ready for production.&lt;/P&gt;&lt;P&gt;I would like to flash the code on the boards without debbuging feature.&lt;/P&gt;&lt;P&gt;Do you have any recommendation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;João Paulo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2019 13:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933709#M4297</guid>
      <dc:creator>joãopaulo</dc:creator>
      <dc:date>2019-07-03T13:50:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933710#M4298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For production programming, use a dedicated device for this, e.g. the Cyclone: &lt;A class="jivelink12" href="http://www.pemicro.com/cyclone/" title="http://www.pemicro.com/cyclone/"&gt;http://www.pemicro.com/cyclone/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2019 13:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933710#M4298</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-07-03T13:59:30Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933711#M4299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi João,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more thought on this topic...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you only have a .bin format available then you can convert this to an srecord or intel hex file format and program this through the GUI Flash Programmer via P&amp;amp;E debug probe within MCUXpresso IDE. Simply invoke the GUI flash programmer and browse to the file via the File System (All Files) option etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90588i85ED5972159313C8/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also note, programming an .axf file onto a board only programs the binary content of the file i.e. the contents of the flash will be identical either way &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2019 15:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933711#M4299</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-07-08T15:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933712#M4300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have all the Project files because I developed it.&lt;/P&gt;&lt;P&gt;The point here is that I need to send it for production but I can't send the source code, the hole Project..&lt;/P&gt;&lt;P&gt;I would like to send them only the .bin or srecord, because I think it's more secure.&lt;/P&gt;&lt;P&gt;The company that will do the production has the &lt;SPAN style="display: inline !important; float: none; background-color: #ffffff; color: #51626f; font-family: inherit; font-size: 100%; font-style: inherit; font-variant: normal; font-weight: inherit; letter-spacing: normal; orphans: 2; overflow-wrap: break-word; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px;"&gt;PE micro multlink universal fx, that's why I did the question.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="display: inline !important; float: none; background-color: #ffffff; color: #51626f; font-family: inherit; font-size: 100%; font-style: inherit; font-variant: normal; font-weight: inherit; letter-spacing: normal; orphans: 2; overflow-wrap: break-word; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px;"&gt;What's the best way to do production process?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="display: inline !important; float: none; background-color: #ffffff; color: #51626f; font-family: inherit; font-size: 100%; font-style: inherit; font-variant: normal; font-weight: inherit; letter-spacing: normal; orphans: 2; overflow-wrap: break-word; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px;"&gt;Thanks in advance!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000011; background-color: #ffffff;"&gt;Best Regards!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 15:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933712#M4300</guid>
      <dc:creator>joãopaulo</dc:creator>
      <dc:date>2019-07-09T15:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933713#M4301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could use the -s option to generate a binary without the symbols:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90675i0B74F1A482681888/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 16:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933713#M4301</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-07-09T16:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash KL27 using bin file through PE Micro Multlink universal fx</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933714#M4302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering whether there has been an update in the meantime?&lt;BR /&gt;&lt;BR /&gt;According to the MCUXpressor IDE user guide there is an option to load binary files (although maybe not for all debuggers) but when I use a P&amp;amp;E debugger/programmer there are no options other than *.axf.&lt;BR /&gt;&lt;BR /&gt;Trying *.s19 it doesn't look to do anything (as it doesn't when selecting a binary file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having to use an old KDS version for SREC programming and an even older Codewarrior version to do binary programming, but it certainly would be easier to just be able to use the newest tool to do such things. Is this still missing or is it somehow possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2020 05:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-flash-KL27-using-bin-file-through-PE-Micro-Multlink/m-p/933714#M4302</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-01-27T05:02:06Z</dc:date>
    </item>
  </channel>
</rss>