<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Stacked registers display in MCUXpresso Fault tab  in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stacked-registers-display-in-MCUXpresso-Fault-tab/m-p/917467#M4078</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There may be an error in how MCUXpresso shows the values of the stacked registers after a hard fault. It always appears to&amp;nbsp;show the data from the Main Stack Pointer. I've a situation where the exception happens during thread mode and the registers are saved on the Process Stack Pointer. The LR has a value of 0xffffffed. In this case it would be more helpful if the IDE showed the registers from the PSP. In particular, the unstacked LR and PC are misleading as they are not related to the code that was executing at the time of the exception.&lt;/P&gt;&lt;P&gt;MCUXpresso version 10.3.1 and 11.0.0&lt;/P&gt;&lt;P&gt;iMXRT1021 EVAL board&lt;/P&gt;&lt;P&gt;LCP-LINK2 emulator probe&lt;/P&gt;&lt;P&gt;Windows 7 64-bit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Aug 2019 12:07:50 GMT</pubDate>
    <dc:creator>jaldridge</dc:creator>
    <dc:date>2019-08-28T12:07:50Z</dc:date>
    <item>
      <title>Stacked registers display in MCUXpresso Fault tab</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stacked-registers-display-in-MCUXpresso-Fault-tab/m-p/917467#M4078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There may be an error in how MCUXpresso shows the values of the stacked registers after a hard fault. It always appears to&amp;nbsp;show the data from the Main Stack Pointer. I've a situation where the exception happens during thread mode and the registers are saved on the Process Stack Pointer. The LR has a value of 0xffffffed. In this case it would be more helpful if the IDE showed the registers from the PSP. In particular, the unstacked LR and PC are misleading as they are not related to the code that was executing at the time of the exception.&lt;/P&gt;&lt;P&gt;MCUXpresso version 10.3.1 and 11.0.0&lt;/P&gt;&lt;P&gt;iMXRT1021 EVAL board&lt;/P&gt;&lt;P&gt;LCP-LINK2 emulator probe&lt;/P&gt;&lt;P&gt;Windows 7 64-bit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 12:07:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stacked-registers-display-in-MCUXpresso-Fault-tab/m-p/917467#M4078</guid>
      <dc:creator>jaldridge</dc:creator>
      <dc:date>2019-08-28T12:07:50Z</dc:date>
    </item>
    <item>
      <title>Re: Stacked registers display in MCUXpresso Fault tab</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stacked-registers-display-in-MCUXpresso-Fault-tab/m-p/917468#M4079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the feedback - we'll take a look.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 13:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stacked-registers-display-in-MCUXpresso-Fault-tab/m-p/917468#M4079</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-08-29T13:26:39Z</dc:date>
    </item>
  </channel>
</rss>