<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mcux sdk components in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/mcux-sdk-components/m-p/916796#M4077</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Henning:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP released SDK_2.6.0_FRDM-K64F. I would suggest you try to download it from below link&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and try it again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jun 2019 06:24:14 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2019-06-17T06:24:14Z</dc:date>
    <item>
      <title>mcux sdk components</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/mcux-sdk-components/m-p/916795#M4076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with the k64f freedom board in mcuxpresso with sdk 2.5. In the example code there is this folder called components. I find myself unable to create a new sdk project with these components, and I have also been unsuccessfull in finding the documentation related to their use. (except the docstrings in the headers)&lt;/P&gt;&lt;P&gt;They are not selectable from the list of libraries etc. that is included in the project creation, and the only "components" that is included by default is serial_manager and uart. I would like to play around with the other "components" as well.&lt;/P&gt;&lt;P&gt;Are they supposed to be just drag and dropped from the zip archive into the project folder, or is there a more correct way to use them in a project with the correct defines etc.?&lt;/P&gt;&lt;P&gt;Picture related.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 15:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/mcux-sdk-components/m-p/916795#M4076</guid>
      <dc:creator>henning1</dc:creator>
      <dc:date>2019-06-13T15:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: mcux sdk components</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/mcux-sdk-components/m-p/916796#M4077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Henning:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP released SDK_2.6.0_FRDM-K64F. I would suggest you try to download it from below link&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and try it again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 06:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/mcux-sdk-components/m-p/916796#M4077</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-06-17T06:24:14Z</dc:date>
    </item>
  </channel>
</rss>