<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: SDK packages do not include hostlib project examples</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873680#M3702</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Estephania,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your mail. Yes that is correct. When I select all the middlewares the the produced SDK can load me all the examples.&lt;/P&gt;&lt;P&gt;Apparently I have another issue now. When I choose and debug the example xxx_hostlib_main_A71CH.. for the host API project, I can not see the J-Link OpenSDA in the Probes discovered window. Thus after the execution of the program, the connection is failed. I tend to believe that I have to update my board with the OpenSDA application as it is explained here :  &lt;A href="https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&amp;amp;tid=vanOpenSDA#FRDM-K64F" target="test_blank"&gt;https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&amp;amp;tid=vanOpenSDA#FRDM-K64F&lt;/A&gt;  but I have not tried yet.&lt;/P&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Ioannis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Mar 2019 23:56:19 GMT</pubDate>
    <dc:creator>ioannis_kapnisa</dc:creator>
    <dc:date>2019-03-21T23:56:19Z</dc:date>
    <item>
      <title>SDK packages do not include hostlib project examples</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873678#M3700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My issue is that I can not&lt;SPAN style="color: #4a4a4d; background-color: #f2f2f5;"&gt;&amp;nbsp;importing hostlib examples - Unable to perform A71CH API HOST and Configuration examples application examples.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am working on a prototype project where I use the following HW:&lt;/P&gt;&lt;P&gt;NXP FRDM-K64F Kinetic board&lt;/P&gt;&lt;P&gt;OM3710/A71CHARD NXP Arduino Development Kit with a A71CHARD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am following the quick start guide &lt;A href="https://www.nxp.com/docs/en/application-note/AN12135.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12135.pdf&amp;nbsp;&lt;/A&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During the SW set up I faced an issue while trying to import the A71CH&amp;nbsp; project examples from the installed SDK.&lt;/P&gt;&lt;P&gt;My board frdmK64f is detected (photo1) but then in the obtained list with the examples on SDK I do not have the se-hostlib examples (&lt;STRONG&gt;photo 2,&amp;nbsp; I can not obtain the files in the red rectangular&lt;/STRONG&gt;&lt;SPAN style="text-decoration: underline;"&gt;)&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;I followed again the process of downloading and installing SDK package for A71CH but the issue of not reaching the&amp;nbsp; se-hostlib projects was remaining.&lt;/P&gt;&lt;P&gt;Then I decided to import also the A71CH&amp;nbsp; project examples from the local drive without any issue in this case.&lt;/P&gt;&lt;P&gt;In this case only the project examples:&lt;/P&gt;&lt;P&gt;......._freertos_....._demo&lt;/P&gt;&lt;P&gt;shown in photo 3 were imported at MCUxpresso IDE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, when I proceed in the execution of A71CH API host example or Configuration tool example, the needed projects of ''frdmk64f_se_hostlib_examples_mainA71CH'' or ''xxx_se_hostlib_examples_vcomA71CH'' can not be found from the project explorer in the left side. and the error of ''Program File does not exist'' is displayed. Please see photo 4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that the SDK package that I download and install from&amp;nbsp;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/dashboard?uvid=160041" title="https://mcuxpresso.nxp.com/en/dashboard?uvid=160041"&gt;https://mcuxpresso.nxp.com/en/dashboard?uvid=160041&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(photo 5) does not include the needed project examples&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please provide me with some guidelines or suggestions for the reason that create this issue??&lt;/P&gt;&lt;P&gt;Is there an alternative in order to proceed in the examples of API Host and Configuration tool examples?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I thank you in advance for your time&lt;/P&gt;&lt;P&gt;Ioannis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 13:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873678#M3700</guid>
      <dc:creator>ioannis_kapnisa</dc:creator>
      <dc:date>2019-03-20T13:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: SDK packages do not include hostlib project examples</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873679#M3701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When creating the SDK in MCUXpresso, could you please try selecting all components when building the SDK and verify if the examples are available when doing so ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 22:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873679#M3701</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-03-21T22:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: SDK packages do not include hostlib project examples</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873680#M3702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Estephania,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your mail. Yes that is correct. When I select all the middlewares the the produced SDK can load me all the examples.&lt;/P&gt;&lt;P&gt;Apparently I have another issue now. When I choose and debug the example xxx_hostlib_main_A71CH.. for the host API project, I can not see the J-Link OpenSDA in the Probes discovered window. Thus after the execution of the program, the connection is failed. I tend to believe that I have to update my board with the OpenSDA application as it is explained here :  &lt;A href="https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&amp;amp;tid=vanOpenSDA#FRDM-K64F" target="test_blank"&gt;https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&amp;amp;tid=vanOpenSDA#FRDM-K64F&lt;/A&gt;  but I have not tried yet.&lt;/P&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Ioannis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 23:56:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873680#M3702</guid>
      <dc:creator>ioannis_kapnisa</dc:creator>
      <dc:date>2019-03-21T23:56:19Z</dc:date>
    </item>
    <item>
      <title>Re: SDK packages do not include hostlib project examples</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873681#M3703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you try some of the driver examples is it possible for you to debug? Is the issue isolated to the example of the A71CH ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;BR /&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2019 18:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/SDK-packages-do-not-include-hostlib-project-examples/m-p/873681#M3703</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-03-25T18:32:20Z</dc:date>
    </item>
  </channel>
</rss>