<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Stack pointer in wrong memory</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863757#M3613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hiya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok thanks I'll give that a try tomorrow as I'm not in the office today. Your board looks like an older revision as I think my SW7 is a DIP switch type and not jumpers. I used to have it set to 0001 for booting from Hyperflash but since I'm running from SDRAM, I've set it to 0000. I'll let you know how I get on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I sometimes use the OpenSDA port for debugging but mostly use a Segger J-Link because our final product won't have OpenSDA so I need to get used to living without it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jan 2019 08:55:45 GMT</pubDate>
    <dc:creator>gary_metalle</dc:creator>
    <dc:date>2019-01-15T08:55:45Z</dc:date>
    <item>
      <title>Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863749#M3605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having trouble trying to get the stack pointer to be where I want it using MCUExpresso with the imxrt1052.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using version 10.2.1 of the IDE and version 2.5.0 of the EVKB-IMXRT1050 SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My memory is configured thus which is pretty standard:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73962iCEAC8480D45976AC/image-size/large?v=v2&amp;amp;px=999" title="memories.png" alt="memories.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I've configured the linker to link the application to RAM and to set the heap and stack to SDRAM as shown below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74008i5A63BE1A1F17BB74/image-size/large?v=v2&amp;amp;px=999" title="linker.png" alt="linker.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However when I set a breakpoint in the ResetISR function the stack pointer (r13) is always in the internal SRAM_OC area:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74284i467962122B69A483/image-size/large?v=v2&amp;amp;px=999" title="stack.png" alt="stack.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The linker map file shows exactly what I expect it to show as shown here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Reserve and place Heap within memory map */&lt;BR /&gt; _HeapSize = 0x800000;&lt;BR /&gt; .heap : ALIGN(4)&lt;BR /&gt; {&lt;BR /&gt; _pvHeapStart = .;&lt;BR /&gt; . += _HeapSize;&lt;BR /&gt; . = ALIGN(4);&lt;BR /&gt; _pvHeapLimit = .;&lt;BR /&gt; } &amp;gt; BOARD_SDRAM&lt;/P&gt;&lt;P&gt;_StackSize = 0x200000;&lt;BR /&gt; /* Reserve space in memory for Stack */&lt;BR /&gt; .heap2stackfill :&lt;BR /&gt; {&lt;BR /&gt; . += _StackSize;&lt;BR /&gt; } &amp;gt; BOARD_SDRAM&lt;BR /&gt; /* Locate actual Stack in memory map */&lt;BR /&gt; .stack ORIGIN(BOARD_SDRAM) + LENGTH(BOARD_SDRAM) - _StackSize - 0: ALIGN(4)&lt;BR /&gt; {&lt;BR /&gt; _vStackBase = .;&lt;BR /&gt; . = ALIGN(4);&lt;BR /&gt; _vStackTop = . + _StackSize;&lt;BR /&gt; } &amp;gt; BOARD_SDRAM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried cleaning the build and also creating a small application with no frills straight from the SDK and that doesn't help. I've also tried removing the BOARD_FLASH memory and also the internal SRAMs so that I only have SDRAM and that makes no difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you look carefully at the code snippet in the last pic you can see where I've commented out manually setting the sp using the _vStackTop value set by the linker. This kinda does work in that the stack pointer gets set properly, but I find that the application dies after a while due to stack corruption of a C++ object that was created on the stack within main.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 09:35:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863749#M3605</guid>
      <dc:creator>gary_metalle</dc:creator>
      <dc:date>2019-01-09T09:35:43Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863750#M3606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend customer to refer MCUXpresso SDK [hello world] project for MIMXRT1050-EVKB.&lt;/P&gt;&lt;P&gt;During SDK example project importing, please select [Link application to RAM].&lt;/P&gt;&lt;P&gt;Please refer the &amp;lt;evkbimxrt1050_hello_world_Debug.ld&amp;gt; file,&amp;nbsp; I could check the heap and stack located at BOARD_SDRAM.&lt;/P&gt;&lt;P&gt;During debug, the stack pointer located at SDRAM memory:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76829iEC2A7A922E957DB7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I would recommend customer to update MCUXpresso IDE software.&lt;/P&gt;&lt;P&gt;Below is my MCUXpresso IDE software version info:&lt;/P&gt;&lt;P&gt;MCUXpresso IDE v10.3.0_prc3 [Build 2187] [2018-11-18]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 08:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863750#M3606</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-01-10T08:06:48Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863751#M3607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. I did try that before but I did it again just to be sure. I imported the helloworld example from the latest SDK and made sure to select 'Link application to RAM' in the wizard. However it still shows the SP as being in the wrong place as shown in the follow screenshot...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77303i16ED095D16D30EF3/image-size/large?v=v2&amp;amp;px=999" title="helloworld.png" alt="helloworld.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 08:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863751#M3607</guid>
      <dc:creator>gary_metalle</dc:creator>
      <dc:date>2019-01-11T08:17:03Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863752#M3608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you update the MCUXpresso IDE to latest version V10.3?&lt;/P&gt;&lt;P&gt;Below is my MCUXpresso IDE version info:&lt;/P&gt;&lt;P&gt;MCUXpresso IDE v10.3.0_prc3 [Build 2187] [2018-11-18]&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 01:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863752#M3608</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-01-14T01:35:40Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863753#M3609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried installing version 10.3.0 and the problem is still there. I checked the release notes for 10.3.0 and it doesn't mention anything about this issue anyway.&lt;/P&gt;&lt;P&gt;I tried importing the helloworld demo that I had created in the previous version and that still showed the incorrect stack and so I completely deleted this project and created it new with the new IDE. This still shows the wrong stack:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76874iD345C779BAB18ED5/image-size/large?v=v2&amp;amp;px=999" title="ide10.3.png" alt="ide10.3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 08:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863753#M3609</guid>
      <dc:creator>gary_metalle</dc:creator>
      <dc:date>2019-01-14T08:26:56Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863754#M3610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't have access to a board or J-Link to check this right now, but I suspect that it could actually be the debug probe that is setting the SP in the background.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you post the text from the debug messages log in the Console View after you hit the breakpoint you have set in ResetISR() ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 13:44:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863754#M3610</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-01-14T13:44:53Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863755#M3611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hiya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok that sounds plausible. Doesn't look like anything except reads here, but here you go (breakpoint was on main this time not the ResetISR)...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been looking at the start-up code that is presumably produced by the SDK for the actual board and I can't see where the actual SP is set anyway. There's an array called&amp;nbsp;&lt;STRONG&gt;g_pfnVectors&lt;/STRONG&gt; that is copied to the vector table offset register. The first element of this array is what the stack pointer should be set to (and I've checked this is correct), but nothing is being done with this value?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[14-1-2019 01:49:16] Executing Server: "C:\Program Files (x86)\SEGGER\JLink_V640\JLinkGDBServerCL.exe" -nosilent -swoport 2332 -select USB=260108640 -jlinkscriptfile C:\Projects\Nexus\Software\Source\Workspace\BRIGHTWELL_NEXUS_MDU_FW\scripts\evkbimxrt1050_sdram_init.jlinkscript -telnetport 2333 -singlerun -endian little -noir -speed auto -port 2331 -vd -device MCIMXRT1052 -if SWD -halt -reportuseraction&lt;BR /&gt;SEGGER J-Link GDB Server V6.40 Command Line Version&lt;/P&gt;&lt;P&gt;JLinkARM.dll V6.40 (DLL compiled Oct 26 2018 15:06:02)&lt;/P&gt;&lt;P&gt;Command line: -nosilent -swoport 2332 -select USB=260108640 -jlinkscriptfile C:\Projects\Nexus\Software\Source\Workspace\BRIGHTWELL_NEXUS_MDU_FW\scripts\evkbimxrt1050_sdram_init.jlinkscript -telnetport 2333 -singlerun -endian little -noir -speed auto -port 2331 -vd -device MCIMXRT1052 -if SWD -halt -reportuseraction&lt;BR /&gt;-----GDB Server start settings-----&lt;BR /&gt;GDBInit file: none&lt;BR /&gt;GDB Server Listening port: 2331&lt;BR /&gt;SWO raw output listening port: 2332&lt;BR /&gt;Terminal I/O port: 2333&lt;BR /&gt;Accept remote connection: localhost only&lt;BR /&gt;Generate logfile: off&lt;BR /&gt;Verify download: on&lt;BR /&gt;Init regs on start: off&lt;BR /&gt;Silent mode: off&lt;BR /&gt;Single run mode: on&lt;BR /&gt;Target connection timeout: 0 ms&lt;BR /&gt;------J-Link related settings------&lt;BR /&gt;J-Link Host interface: USB&lt;BR /&gt;J-Link script: C:\Projects\Nexus\Software\Source\Workspace\BRIGHTWELL_NEXUS_MDU_FW\scripts\evkbimxrt1050_sdram_init.jlinkscript&lt;BR /&gt;J-Link settings file: none&lt;BR /&gt;------Target related settings------&lt;BR /&gt;Target device: MCIMXRT1052&lt;BR /&gt;Target interface: SWD&lt;BR /&gt;Target interface speed: auto&lt;BR /&gt;Target endian: little&lt;/P&gt;&lt;P&gt;Connecting to J-Link...&lt;BR /&gt;$$UserActionStart$$: Terms of use&lt;BR /&gt;$$UserActionEnd$$: Terms of use&lt;BR /&gt;J-Link is connected.&lt;BR /&gt;Device "MCIMXRT1052" selected.&lt;BR /&gt;Firmware: J-Link V10 compiled Oct 26 2018 12:04:17&lt;BR /&gt;Hardware: V10.10&lt;BR /&gt;S/N: 260108640&lt;BR /&gt;OEM: SEGGER-EDU&lt;BR /&gt;Feature(s): FlashBP, GDB&lt;BR /&gt;Checking target voltage...&lt;BR /&gt;Target voltage: 3.27 V&lt;BR /&gt;Listening on TCP/IP port 2331&lt;BR /&gt;Connecting to target...Executing J-Link script file function: ConfigTargetSettings()&lt;BR /&gt;Config JTAG Speed to 4000kHz&lt;BR /&gt;Found SW-DP with ID 0x0BD11477&lt;BR /&gt;Scanning AP map to find all available APs&lt;BR /&gt;AP[1]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;AP[0]: AHB-AP (IDR: 0x04770041)&lt;BR /&gt;Iterating through AP map to find AHB-AP to use&lt;BR /&gt;AP[0]: Core found&lt;BR /&gt;AP[0]: AHB-AP ROM base: 0xE00FD000&lt;BR /&gt;CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)&lt;BR /&gt;Found Cortex-M7 r1p1, Little endian.&lt;BR /&gt;FPUnit: 8 code (BP) slots and 0 literal slots&lt;BR /&gt;CoreSight components:&lt;BR /&gt;ROMTbl[0] @ E00FD000&lt;BR /&gt;ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table&lt;BR /&gt;ROMTbl[1] @ E00FE000&lt;BR /&gt;ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table&lt;BR /&gt;ROMTbl[2] @ E00FF000&lt;BR /&gt;ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7&lt;BR /&gt;ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT&lt;BR /&gt;ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7&lt;BR /&gt;ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM&lt;BR /&gt;ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7&lt;BR /&gt;ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI&lt;BR /&gt;ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7&lt;BR /&gt;ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG&lt;BR /&gt;Cache: Separate I- and D-cache.&lt;/P&gt;&lt;P&gt;I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way&lt;BR /&gt;D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way&lt;BR /&gt;Enabling i.MXRT SDRAM&lt;BR /&gt;DCDC trim value loaded.&lt;BR /&gt;Clock Init Done&lt;BR /&gt;SDRAM Init Done&lt;BR /&gt;Executing J-Link script file function: ConfigTargetSettings()&lt;BR /&gt;Config JTAG Speed to 4000kHz&lt;BR /&gt;Found SW-DP with ID 0x0BD11477&lt;BR /&gt;AP map detection skipped. Manually configured AP map found.&lt;BR /&gt;AP[0]: AHB-AP (IDR: Not set)&lt;BR /&gt;AP[0]: Core found&lt;BR /&gt;AP[0]: AHB-AP ROM base: 0xE00FD000&lt;BR /&gt;CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)&lt;BR /&gt;Found Cortex-M7 r1p1, Little endian.&lt;BR /&gt;FPUnit: 8 code (BP) slots and 0 literal slots&lt;BR /&gt;CoreSight components:&lt;BR /&gt;ROMTbl[0] @ E00FD000&lt;BR /&gt;ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table&lt;BR /&gt;ROMTbl[1] @ E00FE000&lt;BR /&gt;ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table&lt;BR /&gt;ROMTbl[2] @ E00FF000&lt;BR /&gt;ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7&lt;BR /&gt;ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT&lt;BR /&gt;ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7&lt;BR /&gt;ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM&lt;BR /&gt;ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7&lt;BR /&gt;ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI&lt;BR /&gt;ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7&lt;BR /&gt;ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG&lt;BR /&gt;Cache: Separate I- and D-cache.&lt;/P&gt;&lt;P&gt;I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way&lt;BR /&gt;D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way&lt;BR /&gt;Enabling i.MXRT SDRAM&lt;BR /&gt;DCDC trim value loaded.&lt;BR /&gt;Clock Init Done&lt;BR /&gt;SDRAM Init Done&lt;BR /&gt;Connected to target&lt;BR /&gt;Waiting for GDB connection...Connected to 127.0.0.1&lt;BR /&gt;Reading all registers&lt;BR /&gt;Read 4 bytes @ address 0x0020C746 (Data = 0x6148F8D0)&lt;BR /&gt;Read 2 bytes @ address 0x0020C746 (Data = 0xF8D0)&lt;BR /&gt;Received monitor command: reset&lt;BR /&gt;Executing J-Link script file function: ResetTarget()&lt;BR /&gt;J-Link script: ResetTarget()&lt;BR /&gt;DP0: 0x0BD11477&lt;BR /&gt;DP1: 0xF0000040&lt;BR /&gt;AHB-AP0: 0x03000042&lt;BR /&gt;AHB-AP1: 0xE000EDF0&lt;BR /&gt;AHB-AP3: 0x00030003&lt;BR /&gt;AHB-AP3: 0x00030003&lt;BR /&gt;DCDC trim value loaded.&lt;BR /&gt;Clock Init Done&lt;BR /&gt;SDRAM Init Done&lt;BR /&gt;Resetting target&lt;BR /&gt;Downloading 16128 bytes @ address 0x80000000 - Verified OK&lt;BR /&gt;Downloading 6352 bytes @ address 0x80003F00 - Verified OK&lt;BR /&gt;Downloading 4 bytes @ address 0x800057D0 - Verified OK&lt;BR /&gt;Writing register (PC = 0x80000304)&lt;BR /&gt;Read 4 bytes @ address 0x80000304 (Data = 0xB672B510)&lt;BR /&gt;Reading all registers&lt;BR /&gt;Read 4 bytes @ address 0x80000304 (Data = 0xB672B510)&lt;BR /&gt;Reading 64 bytes @ address 0x80000540&lt;BR /&gt;Read 2 bytes @ address 0x80000552 (Data = 0xF001)&lt;BR /&gt;Received monitor command: semihosting enable&lt;BR /&gt;Semi-hosting enabled (Handle on BKPT)&lt;BR /&gt;Received monitor command: exec SetRestartOnClose=0&lt;BR /&gt;Executed SetRestartOnClose=0&lt;BR /&gt;Setting breakpoint @ address 0x80000552, Size = 2, BPHandle = 0x0001&lt;BR /&gt;Starting target CPU...&lt;BR /&gt;...Breakpoint reached @ address 0x80000552&lt;BR /&gt;Reading all registers&lt;BR /&gt;Removing breakpoint @ address 0x80000552, Size = 2&lt;BR /&gt;Read 4 bytes @ address 0x80000552 (Data = 0xFB19F001)&lt;BR /&gt;Reading register (MSP = 0x20200F60)&lt;BR /&gt;Reading register (PRIMASK = 0x 0)&lt;BR /&gt;Reading register (PSP = 0x 0)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 13:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863755#M3611</guid>
      <dc:creator>gary_metalle</dc:creator>
      <dc:date>2019-01-14T13:56:47Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863756#M3612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you check the board jumper setting?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76919iF8C8B6810EB0F75D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BTW: The SW7 value is 0110.&lt;/P&gt;&lt;P&gt;During the debug, I am using on board OpenSDA.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 01:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863756#M3612</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-01-15T01:21:10Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863757#M3613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hiya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok thanks I'll give that a try tomorrow as I'm not in the office today. Your board looks like an older revision as I think my SW7 is a DIP switch type and not jumpers. I used to have it set to 0001 for booting from Hyperflash but since I'm running from SDRAM, I've set it to 0000. I'll let you know how I get on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I sometimes use the OpenSDA port for debugging but mostly use a Segger J-Link because our final product won't have OpenSDA so I need to get used to living without it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 08:55:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863757#M3613</guid>
      <dc:creator>gary_metalle</dc:creator>
      <dc:date>2019-01-15T08:55:45Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863758#M3614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can regenerate the issue with a standalone Segger J-Link Plus tool.&lt;/P&gt;&lt;P&gt;The stack point at 0x20200fe8.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3854iB67A2D91A0CC0C2B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I am checking with Segger about this issue.&lt;/P&gt;&lt;P&gt;I will let you know when there with any feedback.&lt;/P&gt;&lt;P&gt;Thanks for the patience.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 01:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863758#M3614</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-01-16T01:51:52Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863759#M3615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok thanks, yes do let me know about the Segger issue. It will be annoying if that is the case as we already have an ongoing issue in that the Flash can't be mass erased using the JLINK debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently trying to use OpenSDA for debugging but I've found it's not very reliable when configuring a project to run from external SDRAM. I have had it working in the past though so will keep on that. I have got to the point though where I can see that the MSP/SP are at definitely in SDRAM and with the value I'd expect. It's odd that the debug output from JLINK doesn't show that it is setting the stack pointer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 12:39:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863759#M3615</guid>
      <dc:creator>gary_metalle</dc:creator>
      <dc:date>2019-01-17T12:39:46Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863760#M3616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the later reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got below feedback from Segger engineer:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74999iDFB28E76437CAAC2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 08:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863760#M3616</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-02-20T08:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863761#M3617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OK thanks for passing that on. We'll leave our workaround in place that sets the stack pointer. For anyone else that needs this, here is what to do:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the startup/startup_mimxrt1052.cpp file add the following two lines in the ResetISR function right after the asm instruction that disables interrupts:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;__attribute__ ((section(".after_vectors.reset")))&lt;BR /&gt;void ResetISR(void) {&lt;/P&gt;&lt;P&gt;// Disable interrupts&lt;BR /&gt; __asm volatile ("cpsid i");&lt;/P&gt;&lt;P&gt;// Set the main stack pointer...&lt;BR /&gt; register volatile unsigned int sp __asm("sp");&lt;BR /&gt; sp = reinterpret_cast&amp;lt;unsigned int&amp;gt;(&amp;amp;_vStackTop);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: #000000; "&gt;If there is someone from NXP that produces the MIMXRT1050 SDK reading this&lt;/STRONG&gt;, then please add this extra code to the startup file because without it, setting the stack to anything other than OCRAM in the IDE will be pointless because it will never get set. The OCRAM is quite small and for any sizeable project other than a simple 'hello world' I think you'd need to have the stack in external (SDRAM) memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 08:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863761#M3617</guid>
      <dc:creator>gary_metalle</dc:creator>
      <dc:date>2019-02-20T08:17:14Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863762#M3618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the sharing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2019 00:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863762#M3618</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-02-21T00:50:15Z</dc:date>
    </item>
    <item>
      <title>Re: Stack pointer in wrong memory</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863763#M3619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue you are seeing is a consequence of debugging a RAM based image with SEGGER and is described correctly by SEGGER in that their debug environment does not set the initial stack pointer based on the image - instead it is inherited from the previous application (likely the bootROM).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In contrast a LinkServer/CMSIS-DAP debug (the default if using the OpenSDA debug probe) will identify that you are debugging from RAM and setup the stack based on the setting in the image - e.g. see text snip from a LinkServer debug log below:&lt;/P&gt;&lt;PRE&gt;  Starting execution using soft reset with PC 0x200002F1 SP 0x20020000 from load at 0x20000000&lt;/PRE&gt;&lt;P&gt;Note: in this example, the SP is set to the top of the first RAM bank i.e. the top of the D_TCM in this case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you look at the binary values at the start of the image in RAM, you will see the linker has correctly inserted the SP value (first entry) based on the managed linkerscript settings and also the entry point for the image:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_16.png"&gt;&lt;IMG alt="pastedImage_16.png" src="https://community.nxp.com/t5/image/serverpage/image-id/78064i9AD71B0BA493D2EA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_16.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If an image is run using an actual reset (e.g. from Flash) then the bootROM would mimic the cortex hardware setup and set the stack based on the image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Stack-pointer-in-wrong-memory/m-p/863763#M3619</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2020-11-02T14:17:20Z</dc:date>
    </item>
  </channel>
</rss>