<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Firmware update using MCUxpresso in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Firmware-update-using-MCUxpresso/m-p/863411#M3597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The S19 file format contains the address information (where to load the data) and the data itself with a CRC.&lt;/P&gt;&lt;P&gt;From this perspecitve it is very universal and can be both used by debuggers and bootloaders/DFU tools.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jan 2019 13:55:51 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2019-01-09T13:55:51Z</dc:date>
    <item>
      <title>Firmware update using MCUxpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Firmware-update-using-MCUxpresso/m-p/863410#M3596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #741b47;"&gt;We have used CodeWarrior 10.xx and created firmware( converting .s19 file (which are generated by CodeWarrior 10.xx) to .bin file using Burner software)).&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #741b47;"&gt;I have some query Regarding MCUXpresso as below&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #741b47;"&gt;1) Can We use same bootloader and same firmware tool (DFU-Demo) to update firmware after migration?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #741b47;"&gt;2) If No, than whats will be the process to update firmware which are running on field?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 11:16:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Firmware-update-using-MCUxpresso/m-p/863410#M3596</guid>
      <dc:creator>sanket_joshi</dc:creator>
      <dc:date>2019-01-09T11:16:43Z</dc:date>
    </item>
    <item>
      <title>Re: Firmware update using MCUxpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Firmware-update-using-MCUxpresso/m-p/863411#M3597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The S19 file format contains the address information (where to load the data) and the data itself with a CRC.&lt;/P&gt;&lt;P&gt;From this perspecitve it is very universal and can be both used by debuggers and bootloaders/DFU tools.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 13:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Firmware-update-using-MCUxpresso/m-p/863411#M3597</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-01-09T13:55:51Z</dc:date>
    </item>
  </channel>
</rss>