<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Memory address tool tip error.</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857484#M3510</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The 'traditional' rending shows the address with the base address plus the offset (in the post-rendered position). I think this is by design that way in the traditional rendering in Ecliopse. I agree that this might be confusing. I'm using the Hex rendering or I set the cell size to 1 to see the address.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71977iD6D6D29B0126FA65/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Feb 2019 11:31:34 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2019-02-12T11:31:34Z</dc:date>
    <item>
      <title>Memory address tool tip error.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857483#M3509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the memory window there is a tool tip showing the address pointed to by the cursor, as shown here with the cursor pointing to the "D9" character in the long word 2020B6D9 starting at address 0x20000000.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72019i2A2822BFACE9483A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Unfortunately the address shown does not account for endian. In this example, character D9 is actually at address 0x20000000.&lt;/P&gt;&lt;P&gt;System: iMXRT1020 EVK with on board OpenSDA debug and gdb.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 09:39:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857483#M3509</guid>
      <dc:creator>jaldridge</dc:creator>
      <dc:date>2019-02-12T09:39:05Z</dc:date>
    </item>
    <item>
      <title>Re: Memory address tool tip error.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857484#M3510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The 'traditional' rending shows the address with the base address plus the offset (in the post-rendered position). I think this is by design that way in the traditional rendering in Ecliopse. I agree that this might be confusing. I'm using the Hex rendering or I set the cell size to 1 to see the address.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71977iD6D6D29B0126FA65/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 11:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857484#M3510</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-02-12T11:31:34Z</dc:date>
    </item>
    <item>
      <title>Re: Memory address tool tip error.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857485#M3511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply. I should have mentioned that this is only a problem with wider data types and that the tip works fine with a cell size of 1. It's a&amp;nbsp;bit trivial, but I thought it might be possible to correct the issue. &lt;A href="mailto:I@m"&gt;I&lt;/A&gt;'m happy to consider the discussion closed whether or not you chose to modify the behavior.&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 11:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857485#M3511</guid>
      <dc:creator>jaldridge</dc:creator>
      <dc:date>2019-02-12T11:51:11Z</dc:date>
    </item>
    <item>
      <title>Re: Memory address tool tip error.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857486#M3512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;this behaviour is 'standard Eclipse', so part of Eclipse CDT (&lt;A class="link-titled" href="https://www.eclipse.org/cdt/" title="https://www.eclipse.org/cdt/"&gt;Eclipse CDT | The Eclipse Foundation&lt;/A&gt;&amp;nbsp;), I have to check with it with the Photon release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 12:35:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Memory-address-tool-tip-error/m-p/857486#M3512</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-02-12T12:35:11Z</dc:date>
    </item>
  </channel>
</rss>