<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GUI flash tool fails on &amp;quot;error on restart - Ee(07)&amp;quot; in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/844566#M3347</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have seen occasional issues with RT10xx devices when pulling the default systemreset to trigger a reset of the MCU/board after programming the flash (particularly with the built-in OpenSDA probe's default firmware). In the circumstance of using the GUI Flash Programmer this should definitely be harmless - I presume that if you press reset on your board manually after programming, you can see your code is running OK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But you may well be able to avoid this&amp;nbsp;by changing the "Reset Handling" option in the GUI Flash Tool from "Default" to "VECTRESET" (to pull a core reset only after programming, rather than a full system one). Or else unticking the "Reset target on completion" option (and then manually resetting the board).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Oct 2018 16:57:11 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2018-10-29T16:57:11Z</dc:date>
    <item>
      <title>GUI flash tool fails on "error on restart - Ee(07)"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/844565#M3346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MIMXRT1050-EVK with SDK 2.3.0&lt;/P&gt;&lt;P&gt;On trying to use Gui flash tool, it seems that the programming works fine (according to printing after reset).&lt;/P&gt;&lt;P&gt;Yet, for some reason I get most of the time (more than 50%) the following error:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Executing flash operation 'Program' (Program file into flash: evkmimxrt1050_hello_world_xip.axf) - Sun Oct 28 13:17:06 IST 2018&lt;BR /&gt;Checking MCU info...&lt;BR /&gt;Scanning for targets...&lt;BR /&gt;Executing flash action...&lt;BR /&gt;MCUXpresso IDE RedlinkMulti Driver v10.2 (Jul 25 2018 11:25:37 - crt_emu_cm_redlink.exe build 555)&lt;BR /&gt;( 0) Reading remote configuration&lt;BR /&gt;Wc(03). No cache support.&lt;BR /&gt;Found chip XML file in C:/Users/ransh/Documents/MCUXpressoIDE_10.2.1_795/workspace/evkmimxrt1050_hello_world_xip/Debug\MIMXRT1052xxxxx.xml&lt;BR /&gt;( 5) Remote configuration complete&lt;BR /&gt;Reconnected to existing link server&lt;BR /&gt;Connecting to probe 1 core 0:0 (using server started externally) gave 'OK'&lt;BR /&gt;Probe Firmware: CMSIS-DAP (ARM)&lt;BR /&gt;Serial Number: 0227000040214e4500231018c89200449e11000097969900&lt;BR /&gt;VID:PID: 0D28:0204&lt;BR /&gt;USB Path: \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#7&amp;amp;1c929f40&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;Using memory from core 0:0 after searching for a good core&lt;BR /&gt;( 30) Emulator Connected&lt;BR /&gt;( 40) Debug Halt&lt;BR /&gt;( 50) CPU ID&lt;BR /&gt;debug interface type = Cortex-M7 (DAP DP ID 0BD11477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 8&lt;BR /&gt;number of flash patches = 0&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 0BD11477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FD000: CID B105100D PID 000008E88C ROM dev (type 0x1)&lt;BR /&gt;ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM dev (type 0x1)&lt;BR /&gt;ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM dev (type 0x1)&lt;BR /&gt;ROM 3 E000E000: CID B105E00D PID 04000BB00C ChipIP dev SCS (type 0x0)&lt;BR /&gt;ROM 3 E0001000: CID B105E00D PID 04000BB002 ChipIP dev DWT (type 0x0)&lt;BR /&gt;ROM 3 E0002000: CID B105E00D PID 04000BB00E ChipIP dev (type 0x0)&lt;BR /&gt;ROM 3 E0000000: CID B105E00D PID 04000BB001 ChipIP dev ITM (type 0x0)&lt;BR /&gt;ROM 2 E0041000: CID B105900D PID 04001BB975 ARCH 23B:4A13r0 CoreSight dev type 0x13 Trace Source - core&lt;BR /&gt;ROM 2 E0042000: CID B105900D PID 04004BB906 CoreSight dev type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A9 CoreSight dev type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0043000: CID B105F00D PID 04001BB101 System dev (type 0x0)&lt;BR /&gt;Inspected v.2 External Flash Device on SPI MIMXRT1050-EVK_S26KS512S.cfx&lt;BR /&gt;Image 'MIMXRT1050-EVK_S26KS512SOct 19 2017 16:37:47'&lt;BR /&gt;Opening flash driver MIMXRT1050-EVK_S26KS512S.cfx&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;Flash variant 'S26KS512S' detected (64MB = 256*256K at 0x60000000)&lt;BR /&gt;Closing flash driver MIMXRT1050-EVK_S26KS512S.cfx&lt;BR /&gt;Non-standard DAP stride detected - 1024 bytes&lt;BR /&gt;NXP: MIMXRT1052xxxxx&lt;BR /&gt;( 65) Chip Setup Complete&lt;BR /&gt;Connected: was_reset=true. was_stopped=false&lt;BR /&gt;( 70) License Check Complete&lt;BR /&gt;Loading 'evkmimxrt1050_hello_world_xip.axf' ELF 0x60000000 len 0x5A0C&lt;BR /&gt;Opening flash driver MIMXRT1050-EVK_S26KS512S.cfx (already resident)&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;Flash variant 'S26KS512S' detected (64MB = 256*256K at 0x60000000)&lt;BR /&gt;Writing 23052 bytes to address 0x60000000 in Flash&lt;BR /&gt;( 0) Mass erasing Flash&lt;BR /&gt;Mass erased flash in 3844msec&lt;BR /&gt;1 of 1 ( 0) Writing pages 0-0 at 0x60000000 with 23052 bytes&lt;BR /&gt;( 0) at 60000000: 0 bytes - 0/23052&lt;BR /&gt;( 71) at 60000000: 16384 bytes - 16384/23052&lt;BR /&gt;(100) at 60004000: 16384 bytes - 32768/23052&lt;BR /&gt;Wrote page 0-0 with 23052 bytes in 1360msec&lt;BR /&gt;Closing flash driver MIMXRT1050-EVK_S26KS512S.cfx&lt;BR /&gt;(100) Finished writing Flash successfully.&lt;BR /&gt;Flash Write Done&lt;BR /&gt;Loaded 0x5A0C bytes in 5581ms (about 4kB/s)&lt;BR /&gt;Reset target (system)&lt;BR /&gt;Starting execution using system reset&lt;BR /&gt;&lt;STRONG&gt;error on restart - Ee(07). Bad ACK returned from status - wire error.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;(100) Target Connection Failed&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Unable to perform operation!&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Command failed with exit code 1&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What does it mean ? Should I just ignore this error ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;ranran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Oct 2018 11:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/844565#M3346</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2018-10-28T11:21:35Z</dc:date>
    </item>
    <item>
      <title>Re: GUI flash tool fails on "error on restart - Ee(07)"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/844566#M3347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have seen occasional issues with RT10xx devices when pulling the default systemreset to trigger a reset of the MCU/board after programming the flash (particularly with the built-in OpenSDA probe's default firmware). In the circumstance of using the GUI Flash Programmer this should definitely be harmless - I presume that if you press reset on your board manually after programming, you can see your code is running OK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But you may well be able to avoid this&amp;nbsp;by changing the "Reset Handling" option in the GUI Flash Tool from "Default" to "VECTRESET" (to pull a core reset only after programming, rather than a full system one). Or else unticking the "Reset target on completion" option (and then manually resetting the board).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2018 16:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/844566#M3347</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-10-29T16:57:11Z</dc:date>
    </item>
    <item>
      <title>Re: GUI flash tool fails on "error on restart - Ee(07)"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/844567#M3348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you NXP for replying&amp;nbsp;to this issue.&amp;nbsp; I had exactly the same problem (although using Embedded Artists i.MX RT5052 Developers Kit) and followed your advice to untick the "Reset target on completion" option.&amp;nbsp; After that the error no longer appears, and pressing reset button on the board will have the code running perfectly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2018 18:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/844567#M3348</guid>
      <dc:creator>socalsparky</dc:creator>
      <dc:date>2018-11-07T18:39:01Z</dc:date>
    </item>
    <item>
      <title>Re: GUI flash tool fails on "error on restart - Ee(07)"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/1249191#M6819</link>
      <description>&lt;P&gt;In case you need the automatic reset, try the following command (shown here for windows command):&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;%MCUX_IDE_BIN%/crt_emu_cm_redlink --reset hard&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Note that&amp;nbsp;&lt;EM&gt;MCUX_IDE_BIN&amp;nbsp;&lt;/EM&gt;comes from&amp;nbsp;&lt;EM&gt;GUI Flash Tool --&amp;gt; Preview Command&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Worked on RT1170 EVK and MCUXPresso 11.3.0&lt;/P&gt;</description>
      <pubDate>Sun, 21 Mar 2021 13:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/GUI-flash-tool-fails-on-quot-error-on-restart-Ee-07-quot/m-p/1249191#M6819</guid>
      <dc:creator>dbl</dc:creator>
      <dc:date>2021-03-21T13:00:11Z</dc:date>
    </item>
  </channel>
</rss>