<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CMSIS DAP Problem in Windows 10 in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/CMSIS-DAP-Problem-in-Windows-10/m-p/825434#M3078</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reinstalling Windows solved the problem..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Dec 2018 20:32:02 GMT</pubDate>
    <dc:creator>denizcan</dc:creator>
    <dc:date>2018-12-27T20:32:02Z</dc:date>
    <item>
      <title>CMSIS DAP Problem in Windows 10</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/CMSIS-DAP-Problem-in-Windows-10/m-p/825433#M3077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In MacOS on MacBook and in Ubuntu 18.04 on PC LpcLink with CMSIS-DAP works OK. However, on the same machine in Windows 10, I get the following console output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE style="padding-left: 30px;"&gt;MCUXpresso IDE RedlinkMulti Driver v10.3 (Nov 28 2018 02:33:57 - crt_emu_cm_redlink build 748)
Found part description in XML file nxp_lpc17xx.xme
Reconnected to existing link server
Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'
Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'
Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'
Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
Failed on connect: Ee(42). Could not connect to core.
No connection to chip's debug port&lt;/PRE&gt;&lt;P&gt;In the RedlinkServer console, I got the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE style="padding-left: 30px;"&gt;probelist
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC11U3x CMSIS-DAP v1.0.7
Serial Number = 0B023028
VID:PID = 1FC9:0132
Path = \\?\hid#vid_1fc9&amp;amp;pid_0132&amp;amp;mi_00#9&amp;amp;236ef90&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}

probestatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC11U3x CMSIS-DAP v1.0.7
Serial Number = 0B023028
VID:PID = 1FC9:0132
Path = \\?\hid#vid_1fc9&amp;amp;pid_0132&amp;amp;mi_00#9&amp;amp;236ef90&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 64
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = CMSIS-DAP
Probe Reference Count = 0

probeopenbyindex 1
Probe not open&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the same PC, the probe works in virtual machine as well..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What shall I do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Dec 2018 11:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/CMSIS-DAP-Problem-in-Windows-10/m-p/825433#M3077</guid>
      <dc:creator>denizcan</dc:creator>
      <dc:date>2018-12-23T11:50:22Z</dc:date>
    </item>
    <item>
      <title>Re: CMSIS DAP Problem in Windows 10</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/CMSIS-DAP-Problem-in-Windows-10/m-p/825434#M3078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reinstalling Windows solved the problem..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Dec 2018 20:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/CMSIS-DAP-Problem-in-Windows-10/m-p/825434#M3078</guid>
      <dc:creator>denizcan</dc:creator>
      <dc:date>2018-12-27T20:32:02Z</dc:date>
    </item>
  </channel>
</rss>