<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How do I reset the project part number? in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-do-I-reset-the-project-part-number/m-p/821862#M3068</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sean Hudson,&lt;/P&gt;&lt;P&gt;I'd recommend to create new project and move your source code to the new project.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Can you describe how did you change package version in PINS tool? Such operation should not be available in MCU IDE.&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Aug 2018 09:37:27 GMT</pubDate>
    <dc:creator>marek-trmac</dc:creator>
    <dc:date>2018-08-07T09:37:27Z</dc:date>
    <item>
      <title>How do I reset the project part number?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-do-I-reset-the-project-part-number/m-p/821861#M3067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I started with one package version of a MK82 part, but subsequently changed it in the PINS tool.&amp;nbsp; How do I tell MCUXpresso to change the target for the project?&amp;nbsp; I currently&amp;nbsp;see an error in the&amp;nbsp;PINS tool. (see screenshot below)&amp;nbsp; After grep'ing around, it appears that the project setting&amp;nbsp;is completely contained in&amp;nbsp;the .cproject file.&amp;nbsp; I am hesitant to modify that directly.&amp;nbsp; Further, it appears that that setting is used to create and pass several #defines into the project that will influence compilation.&amp;nbsp; What's my best approach here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screen Shot 2018-08-06 at 8.41.08 AM.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79683i3B8E0D93269E09ED/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screen Shot 2018-08-06 at 8.41.08 AM.png" alt="Screen Shot 2018-08-06 at 8.41.08 AM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2018 13:46:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-do-I-reset-the-project-part-number/m-p/821861#M3067</guid>
      <dc:creator>seanhudson</dc:creator>
      <dc:date>2018-08-06T13:46:00Z</dc:date>
    </item>
    <item>
      <title>Re: How do I reset the project part number?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-do-I-reset-the-project-part-number/m-p/821862#M3068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sean Hudson,&lt;/P&gt;&lt;P&gt;I'd recommend to create new project and move your source code to the new project.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Can you describe how did you change package version in PINS tool? Such operation should not be available in MCU IDE.&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 09:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-do-I-reset-the-project-part-number/m-p/821862#M3068</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2018-08-07T09:37:27Z</dc:date>
    </item>
  </channel>
</rss>