<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 LPC1549: multiple CAN filters using ccan_rom API</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818799#M3044</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm utilizing the LPCOpen libraries called "ccan_rom.c," "rom_can_15xx.h," and "romapi_15xx.h" to set up a basic CAN interface for the LPC1549.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the example code, there is this excerpt:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/* Configure message object 1 to receive all 11-bit messages 0x400-0x4FF */&lt;BR /&gt;msg_obj.msgobj = 1;&lt;BR /&gt;msg_obj.mode_id = 0x400;&lt;BR /&gt;msg_obj.mask = 0x700;&lt;/P&gt;&lt;P&gt;LPC_CAND_API-&amp;gt;hwCAN_ConfigRxmsgobj(pCanHandle, &amp;amp;msg_obj);&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Which is used to configure a receive object filter.&lt;/P&gt;&lt;P&gt;This sets up one filter, essentially.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to modify this code to the following:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;msg_obj.msgobj = 1;&lt;BR /&gt;msg_obj.mode_id = 0x400;&lt;BR /&gt;msg_obj.mask = 0x700;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;LPC_CAND_API-&amp;gt;hwCAN_ConfigRxmsgobj(pCanHandle, &amp;amp;msg_obj);&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;msg2_obj.msgobj = 2;&lt;/SPAN&gt;&lt;BR style="background-color: #f6f6f6;" /&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;msg2_obj.mode_id = 0x10000320;&lt;/SPAN&gt;&lt;BR style="background-color: #f6f6f6;" /&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;msg2_obj.mask = 0x10000400;&lt;/SPAN&gt;&lt;BR style="background-color: #f6f6f6;" /&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;LPC_CAND_API-&amp;gt;hwCAN_ConfigRxmsgobj(pCanHandle, &amp;amp;msg2_obj);&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;In an attempt to add multiple filters.&lt;BR /&gt;I thought this would create two receive message objects with different filters, but it does not seem to.&lt;BR /&gt;No matter what I do, the ISR is only thrown for the first entry. If I comment out the msg_obj code portion, then the 0x10000320 filter is applied. If I leave the msg_obj code portion uncommented, then the 0x400 filter is applied, and the 0x10000320 filter is not.&lt;BR /&gt;&lt;BR /&gt;What is the right way to add multiple filters, or multiple receive message objects using the ccan_rom API?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Oct 2018 05:49:45 GMT</pubDate>
    <dc:creator>jkingeet</dc:creator>
    <dc:date>2018-10-23T05:49:45Z</dc:date>
    <item>
      <title>LPC1549: multiple CAN filters using ccan_rom API</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818799#M3044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm utilizing the LPCOpen libraries called "ccan_rom.c," "rom_can_15xx.h," and "romapi_15xx.h" to set up a basic CAN interface for the LPC1549.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the example code, there is this excerpt:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/* Configure message object 1 to receive all 11-bit messages 0x400-0x4FF */&lt;BR /&gt;msg_obj.msgobj = 1;&lt;BR /&gt;msg_obj.mode_id = 0x400;&lt;BR /&gt;msg_obj.mask = 0x700;&lt;/P&gt;&lt;P&gt;LPC_CAND_API-&amp;gt;hwCAN_ConfigRxmsgobj(pCanHandle, &amp;amp;msg_obj);&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Which is used to configure a receive object filter.&lt;/P&gt;&lt;P&gt;This sets up one filter, essentially.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to modify this code to the following:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;msg_obj.msgobj = 1;&lt;BR /&gt;msg_obj.mode_id = 0x400;&lt;BR /&gt;msg_obj.mask = 0x700;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;LPC_CAND_API-&amp;gt;hwCAN_ConfigRxmsgobj(pCanHandle, &amp;amp;msg_obj);&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;msg2_obj.msgobj = 2;&lt;/SPAN&gt;&lt;BR style="background-color: #f6f6f6;" /&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;msg2_obj.mode_id = 0x10000320;&lt;/SPAN&gt;&lt;BR style="background-color: #f6f6f6;" /&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;msg2_obj.mask = 0x10000400;&lt;/SPAN&gt;&lt;BR style="background-color: #f6f6f6;" /&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;LPC_CAND_API-&amp;gt;hwCAN_ConfigRxmsgobj(pCanHandle, &amp;amp;msg2_obj);&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;In an attempt to add multiple filters.&lt;BR /&gt;I thought this would create two receive message objects with different filters, but it does not seem to.&lt;BR /&gt;No matter what I do, the ISR is only thrown for the first entry. If I comment out the msg_obj code portion, then the 0x10000320 filter is applied. If I leave the msg_obj code portion uncommented, then the 0x400 filter is applied, and the 0x10000320 filter is not.&lt;BR /&gt;&lt;BR /&gt;What is the right way to add multiple filters, or multiple receive message objects using the ccan_rom API?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 05:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818799#M3044</guid>
      <dc:creator>jkingeet</dc:creator>
      <dc:date>2018-10-23T05:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549: multiple CAN filters using ccan_rom API</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818800#M3045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After further research, I have found the solution to this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a post here:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/461266" rel="nofollow noopener noreferrer" target="_blank"&gt;Introduction to CAN&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;That contains this line:&lt;/P&gt;&lt;PRE class="" style="color: #000000; background: #f5f2f0; border: 0px; margin: 0.5em 0px; padding: 1em 1em 1em 3.8em;"&gt;&lt;CODE style="border: 0px; font-weight: inherit;"&gt;msg_obj&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;.&lt;/SPAN&gt;mode_id &lt;SPAN class="" style="color: #a67f59; background: rgba(255, 255, 255, 0.5); border: 0px; font-weight: inherit;"&gt;=&lt;/SPAN&gt; CAN_MSGOBJ_EXT &lt;SPAN class="" style="color: #a67f59; background: rgba(255, 255, 255, 0.5); border: 0px; font-weight: inherit;"&gt;|&lt;/SPAN&gt; &lt;SPAN class="" style="color: #990000; border: 0px; font-weight: inherit;"&gt;0x0&lt;/SPAN&gt;&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;;
&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified my existing code to the following:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#define CAN_MSGOBJ_EXT 0x20000000UL &lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;// CAN 2.0b 29-bit ID&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;// Message object #1&lt;/SPAN&gt;
msg_obj&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;msgobj &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
msg_obj&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;mode_id &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x400&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
msg_obj&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;mask &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x700&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
LPC_CAND_API&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;hwCAN_ConfigRxmsgobj&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;pCanHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;msg_obj&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;// Message object #2&lt;/SPAN&gt;
msg_obj&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;msgobj &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
msg_obj&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;mode_id &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; CAN_MSGOBJ_EXT &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x10000320&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
msg_obj&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;mask &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; CAN_MSGOBJ_EXT &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x10000400&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
LPC_CAND_API&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;hwCAN_ConfigRxmsgobj&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;pCanHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;msg_obj&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And that works. The interrupt triggers on both, and I can check which message object called the interrupt as per the example code:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;CAN_rx&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint8_t msgNumber&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="comment token"&gt;/* Determine which CAN message has been received */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;msg_obj&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;msgobj &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; msgNumber&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="comment token"&gt;/* Now load up the msg_obj structure with the CAN message */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;LPC_CAND_API&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="token function"&gt;hwCAN_MsgReceive&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;pCanHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;msg_obj&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="comment token"&gt;// Message object #1&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;msgNumber &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="token function"&gt;Board_LED_Toggle&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="comment token"&gt;// Message object #2&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;msgNumber &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="token function"&gt;Board_LED_Toggle&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2018 04:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818800#M3045</guid>
      <dc:creator>jkingeet</dc:creator>
      <dc:date>2018-10-24T04:01:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549: multiple CAN filters using ccan_rom API</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818801#M3046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="295799" data-username="jkingeet" href="https://community.nxp.com/people/jkingeet"&gt;Justin King&lt;/A&gt;&lt;/SPAN&gt;，&lt;/P&gt;&lt;P&gt;I'm glad to hear that&lt;BR /&gt;If you have any further questions about it, please feel free to contact me.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2018 09:01:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818801#M3046</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-10-24T09:01:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549: multiple CAN filters using ccan_rom API</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818802#M3047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excuse me,&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jeremyzhou"&gt;jeremyzhou&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Would you like to do me a favor ? There is a question about the FIFO of CAN.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;I'm utilizing the LPCOpen libraries called "ccan_rom.c," "rom_can_15xx.h," and "romapi_15xx.h" to set up a basic CAN interface for the LPC1549.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;Firstly,when I initialize the FIFO of CAN, I have finished the configuration the filter. Secondly, I made it work normally. However, good times don't last long, a question happened that when the frames of CAN reached 500,000 , the FIFO of CAN can not receive it and more. Then I attempt to reconfigure the filter, the FIFO continue to receiving the frame of CAN again.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;So, which measure can prevent this phenomenon from coming into being ?&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;Can you help me to solve this problem ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2020 07:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC1549-multiple-CAN-filters-using-ccan-rom-API/m-p/818802#M3047</guid>
      <dc:creator>chensiyan618</dc:creator>
      <dc:date>2020-01-08T07:27:54Z</dc:date>
    </item>
  </channel>
</rss>