<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Hex file generation</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Hex-file-generation/m-p/813856#M2963</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am fairly new to embedded programming so I apologise if this is trivial.&lt;/P&gt;&lt;P&gt;I have a project with existing C code for custom hardware using LPC4078. Up to now it has been compiled using a make.bat file and a Makefile from the command line but I don't know where these files originated. I am trying to migrate to MCUXpresso so I imported the source files into a project imaginatively named 'foo'. Most settings were left as default. I get a file called libfoo.axf generated but was expecting foo.axf. I followed 18.13 of the user guide to generate a hex file for programming using a post build step but this appears to be looking for foo.axf. Are the compiler and linker generating the outputs they should? Any guidance would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Nov 2018 02:57:24 GMT</pubDate>
    <dc:creator>stephen_hubbard</dc:creator>
    <dc:date>2018-11-29T02:57:24Z</dc:date>
    <item>
      <title>Hex file generation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Hex-file-generation/m-p/813856#M2963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am fairly new to embedded programming so I apologise if this is trivial.&lt;/P&gt;&lt;P&gt;I have a project with existing C code for custom hardware using LPC4078. Up to now it has been compiled using a make.bat file and a Makefile from the command line but I don't know where these files originated. I am trying to migrate to MCUXpresso so I imported the source files into a project imaginatively named 'foo'. Most settings were left as default. I get a file called libfoo.axf generated but was expecting foo.axf. I followed 18.13 of the user guide to generate a hex file for programming using a post build step but this appears to be looking for foo.axf. Are the compiler and linker generating the outputs they should? Any guidance would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 02:57:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Hex-file-generation/m-p/813856#M2963</guid>
      <dc:creator>stephen_hubbard</dc:creator>
      <dc:date>2018-11-29T02:57:24Z</dc:date>
    </item>
    <item>
      <title>Re: Hex file generation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Hex-file-generation/m-p/813857#M2964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It sounds like you may have create a Library project instead of an executable project, except you would then get a libfoo.lib file created.&amp;nbsp;You will need to post your project files (.project and .cproject) for us to be able to understand what you did and provide help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 08:58:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Hex-file-generation/m-p/813857#M2964</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2018-11-29T08:58:18Z</dc:date>
    </item>
  </channel>
</rss>