<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Intruction trace with Kinetis KV46 in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809244#M2934</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="33318" data-username="zorrotz" href="https://community.nxp.com/people/zorrotz"&gt;Pablo Igor Vicente&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;It seems the Instruction Trace function on MCUXpreso IDE doesn't support KV series,&lt;/P&gt;&lt;P&gt;only support KL and K series.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76157i7DE2B8B41EB058E7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;While I will configure it with development .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Oct 2018 07:12:03 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2018-10-23T07:12:03Z</dc:date>
    <item>
      <title>Intruction trace with Kinetis KV46</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809243#M2933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to use Intruction Trace funtionallity of MCUXpresso IDE version 10.2.1 with Kinetis KV46 and Multilink Universal FX debug probe?&lt;/P&gt;&lt;P&gt;When I launch Intruction Trace "target not supported" error is generated. I have tried deleting the launch configuration, but it doesn´t work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Oct 2018 07:36:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809243#M2933</guid>
      <dc:creator>zorrotz</dc:creator>
      <dc:date>2018-10-19T07:36:44Z</dc:date>
    </item>
    <item>
      <title>Re: Intruction trace with Kinetis KV46</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809244#M2934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="33318" data-username="zorrotz" href="https://community.nxp.com/people/zorrotz"&gt;Pablo Igor Vicente&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;It seems the Instruction Trace function on MCUXpreso IDE doesn't support KV series,&lt;/P&gt;&lt;P&gt;only support KL and K series.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76157i7DE2B8B41EB058E7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;While I will configure it with development .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 07:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809244#M2934</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-10-23T07:12:03Z</dc:date>
    </item>
    <item>
      <title>Re: Intruction trace with Kinetis KV46</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809245#M2935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately the KV46 silicon does not appear to implement the Coresight Embedded Trace Buffer (ETB) that MCUXpresso IDE requires to provide instruction trace capability.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For comparison here is the list of "Coresight" debug components detected with Kinetis&amp;nbsp;K64 (as displayed by a LinkServer debug connection):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;PRE style="margin: 0.0px 0.0px 0.0px 0.0px;"&gt;Content of CoreSight Debug ROM(s):
RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1)
ROM 1 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)
ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0)
ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)
ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0)
ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU
ROM 1 E0041000: CID B105900D PID 04000BB925 CSt ETM type 0x13 Trace Source - Core
ROM 1 E0042000: CID B105900D PID 04003BB907 CSt ETB type 0x21 Trace Sink - ETB
ROM 1 E0043000: CID B105900D PID 04001BB908 CSt CSTF type 0x12 Trace Link - Trace funnel/router&lt;/PRE&gt;&lt;/BLOCKQUOTE&gt;&lt;P style="margin: 0.0px 0.0px 0.0px 0.0px;"&gt;vs the more limited Coresight capabilities implemented on KV46:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;PRE&gt;Content of CoreSight Debug ROM(s):
RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1)
ROM 1 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)
ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0)
ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)
ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0)
ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU&lt;/PRE&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Note the lack of ETB (along with the lack of ETM / Embedded Trace Macrocell which generates the tracedata to be collected by the ETB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 10:07:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809245#M2935</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-10-23T10:07:43Z</dc:date>
    </item>
    <item>
      <title>Re: Intruction trace with Kinetis KV46</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809246#M2936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven´t seen that is only available in K series.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 12:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Intruction-trace-with-Kinetis-KV46/m-p/809246#M2936</guid>
      <dc:creator>zorrotz</dc:creator>
      <dc:date>2018-10-23T12:45:52Z</dc:date>
    </item>
  </channel>
</rss>