<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error when changing SDK root in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640674#M280</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Massimo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;There are a few methods to install an SDK into the IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) &amp;nbsp;Drag/drop an SDK into the Installed SDKs view. This will create a copy of the SDK package at a default location c:\users\&amp;lt;&amp;gt;\mcuxpresso\SDKPackages. If you right-click in the installed SDKs view, and select &lt;STRONG&gt;Open Default Location,&lt;/STRONG&gt; this folder will be opened in windows explorer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.) Store SDK(s) in a folder on your file system. Point the IDE to the folder containing the SDKs by adding the path to the SDK root list in the IDE&amp;nbsp;Windows&amp;gt;Preferences&amp;gt;MCUXpesso IDE&amp;gt;SDK options. SDKs can be added/removed directly from the folder. If you select an SDK package in the installed SDKs view, right-click, and select &lt;STRONG&gt;Open Location&lt;/STRONG&gt;, the folder containing the selected SDK will be opened. To use option 2, it is not necessary to delete the &amp;lt;&amp;gt;\mcuxpresso\SDKPackages&amp;nbsp;folder.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Mar 2017 14:49:21 GMT</pubDate>
    <dc:creator>bryancole-b4682</dc:creator>
    <dc:date>2017-03-31T14:49:21Z</dc:date>
    <item>
      <title>Error when changing SDK root</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640673#M279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the first impression with the tool is really positive, thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with the SDK install folder. I want to move it for "my Documents" to my second hdd, because my C disk is getting full. I changed the SDK search root in SDK Options inside the IDE, but as soon as I add a new folder, remove the default folder c:\users\&amp;lt;&amp;gt;\mcuxpresso\SDKPackages and click "apply" I get a "null pointer" java error. After some more attempts I don't get the error anymore, but&amp;nbsp;the original folder is there each time I restart the IDE. And right click on "default location" always takes me to the SDK folder that I want to delete.&lt;/P&gt;&lt;P&gt;I have a windows 7 pc.&lt;/P&gt;&lt;P&gt;I cannot also drag and drop an SDK inside the "installed SDK" view. I must right click on import.&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Massimo&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 14:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640673#M279</guid>
      <dc:creator>massimomartelli</dc:creator>
      <dc:date>2017-03-31T14:05:02Z</dc:date>
    </item>
    <item>
      <title>Re: Error when changing SDK root</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640674#M280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Massimo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;There are a few methods to install an SDK into the IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) &amp;nbsp;Drag/drop an SDK into the Installed SDKs view. This will create a copy of the SDK package at a default location c:\users\&amp;lt;&amp;gt;\mcuxpresso\SDKPackages. If you right-click in the installed SDKs view, and select &lt;STRONG&gt;Open Default Location,&lt;/STRONG&gt; this folder will be opened in windows explorer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.) Store SDK(s) in a folder on your file system. Point the IDE to the folder containing the SDKs by adding the path to the SDK root list in the IDE&amp;nbsp;Windows&amp;gt;Preferences&amp;gt;MCUXpesso IDE&amp;gt;SDK options. SDKs can be added/removed directly from the folder. If you select an SDK package in the installed SDKs view, right-click, and select &lt;STRONG&gt;Open Location&lt;/STRONG&gt;, the folder containing the selected SDK will be opened. To use option 2, it is not necessary to delete the &amp;lt;&amp;gt;\mcuxpresso\SDKPackages&amp;nbsp;folder.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 14:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640674#M280</guid>
      <dc:creator>bryancole-b4682</dc:creator>
      <dc:date>2017-03-31T14:49:21Z</dc:date>
    </item>
    <item>
      <title>Re: Error when changing SDK root</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640675#M281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bryan,&lt;/P&gt;&lt;P&gt;Is it possible to change the Default Location for the installed SDK Packages?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 15:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640675#M281</guid>
      <dc:creator>jschoen</dc:creator>
      <dc:date>2017-03-31T15:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: Error when changing SDK root</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640676#M282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears that the default location can not be changed, but I will confirm this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As noted above, SDKs can be stored in other paths on the drive.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 15:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640676#M282</guid>
      <dc:creator>bryancole-b4682</dc:creator>
      <dc:date>2017-03-31T15:28:07Z</dc:date>
    </item>
    <item>
      <title>Re: Error when changing SDK root</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640677#M283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did confirm that the default location is fixed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bryan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 18:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Error-when-changing-SDK-root/m-p/640677#M283</guid>
      <dc:creator>bryancole-b4682</dc:creator>
      <dc:date>2017-04-03T18:15:25Z</dc:date>
    </item>
  </channel>
</rss>