<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786406#M2652</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You @Alice Yang.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to follow your steps to recreate a SDK for my MCU properly and select FreeRTOS as an OS in the New Project Wizard.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems I am running into another slightly related problem. The FreeRTOS demo I am trying to import into MCUXpresso IDE was created via IAR. I did some browsing on this forum and I saw someone mention they used an IAR plugin. I installed one myself, but then realized I also needed the IAR IDE to be installed on my computer to use the IAR plugin (for importing IAR projects into MCUXpresso IDE). It seems I may have to "re-write" the demo in my new project by re-writing all the appropriate C files in the source folder of the project directory......I was wondering if there are any guides out there for someone trying to "re-write" a project that they can't normally import into the IDE (due to the project being written by a different, incompatible IDE)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jun 2018 22:17:30 GMT</pubDate>
    <dc:creator>josephjean-jacq</dc:creator>
    <dc:date>2018-06-15T22:17:30Z</dc:date>
    <item>
      <title>Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786404#M2650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to create a new project using the SDK for the Kinetis K65 MCU, which I was able to create via MCUXpresso SDK builder and import it in the IDE successfully. When I arrive at the 'Configure the project' screen, under 'OS', I am only able to select "baremetal". I don't see any option to select FreeRTOS as shown in the following video tutorial:&amp;nbsp;&lt;A href="https://community.nxp.com/videos/7772"&gt; Video Link : 7772&lt;/A&gt;&amp;nbsp; @ the 2:05 mins mark.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to import/adapt one of the many FreeRTOS demo apps to the K65. I tried looking into the MCUXpresso User Guide, but it only provides advice on debugging FreeRTOS within the MCUXpresso IDE.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once again, any help/pointers is greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2018 22:26:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786404#M2650</guid>
      <dc:creator>josephjean-jacq</dc:creator>
      <dc:date>2018-06-14T22:26:55Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786405#M2651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="320280" data-username="josephjean-jacques" href="https://community.nxp.com/people/josephjean-jacques"&gt;Joseph Jean-Jacques&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you downloas SDK package, please be sure select FreeRTOS system:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60306iB60C48845FE46929/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;then delete the orignal SDK from your IDE, plug the new one. Thus, you can create new project with FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 01:07:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786405#M2651</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-06-15T01:07:40Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786406#M2652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You @Alice Yang.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to follow your steps to recreate a SDK for my MCU properly and select FreeRTOS as an OS in the New Project Wizard.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems I am running into another slightly related problem. The FreeRTOS demo I am trying to import into MCUXpresso IDE was created via IAR. I did some browsing on this forum and I saw someone mention they used an IAR plugin. I installed one myself, but then realized I also needed the IAR IDE to be installed on my computer to use the IAR plugin (for importing IAR projects into MCUXpresso IDE). It seems I may have to "re-write" the demo in my new project by re-writing all the appropriate C files in the source folder of the project directory......I was wondering if there are any guides out there for someone trying to "re-write" a project that they can't normally import into the IDE (due to the project being written by a different, incompatible IDE)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 22:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786406#M2652</guid>
      <dc:creator>josephjean-jacq</dc:creator>
      <dc:date>2018-06-15T22:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786407#M2653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joseph,&lt;/P&gt;&lt;P&gt;I think this is the same problem: In the SDK builder for your SDK, make sure you select your toolchain. I think you selected IAR. Make sure you select MCUXrpresso IDE:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61609iDE816BBDC5DE6DF5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Jun 2018 05:22:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786407#M2653</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2018-06-16T05:22:07Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786408#M2654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response. I did go back to the MCUXpresso SDK builder site and accessed my dashboard. Based on the information presented on my SDK, I did create it with MCUXpresso IDE selected as the tool chain. I think the issue I am dealing is more similar to what was discussed in the following threads:&amp;nbsp;&lt;A href="https://community.nxp.com/thread/436795"&gt;Migraton from IAR project to LPCXpresso IDE&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389088"&gt;https://community.nxp.com/thread/389088&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unless I am going about the process&amp;nbsp;incorrectly in terms of importing a project ( more specifically a FreeRTOS demo app created via IAR).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help again is greatly appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Joseph&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 15:28:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786408#M2654</guid>
      <dc:creator>josephjean-jacq</dc:creator>
      <dc:date>2018-06-18T15:28:32Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786409#M2655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Joseph,&lt;/P&gt;&lt;P&gt;I'm afraid there is no method directly open IAR project on MCUXpresso.&lt;/P&gt;&lt;P&gt;What about your project ? If it is&amp;nbsp; a SDK demo project , you can directly open it based on MCUXpresso IDE SDK.&lt;/P&gt;&lt;P&gt;If it is not a SDK demo , recommend you create a new project on MCUXpresso , then copy&amp;amp;paste application code&lt;/P&gt;&lt;P&gt;from IAR to MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jun 2018 03:48:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786409#M2655</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-06-19T03:48:08Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786410#M2656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joseph,&lt;/P&gt;&lt;P&gt;I don't think that this is an IAR porting thing: if you select the MCUXpresso IDE with FreeRTOS, then the SDK and examples already are setup correctly (no porting needed).&lt;/P&gt;&lt;P&gt;Make sure you have it present in your configuration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61992i1ED12643F9903BB6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then you will have FreeRTOS listed:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61993iEDC38C212BA62B86/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jun 2018 14:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786410#M2656</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2018-06-19T14:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to select FreeRTOS as an OS in New Project Wizard screen</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786411#M2657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You @ Alice Yang and Erich Styger. Forgive me, I am new to the embedded software development world. It has finally "clicked" and I understand it now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FreeRTOS demo that I was trying to use was a demo I grabbed from the FreeRTOS site. It was created for the K60 platform using the IAR IDE. I was going to take that demo and see if I could get it working on the K65. As Erich explained, there is no need to do that since MCUXpresso has a SDK builder where I can create a SDK that is specifically catered to the K65 with FreeRTOS included. From there you import the SDK into the MCUXpresso IDE and you can create a new project based off of this SDK , that is immediately ready and able to compile/run on the K65 development board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have done exactly this. I also didn't realize there was a plethora of examples that came with the SDK that I can use as a starting point, based on my specific needs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once again, Thank you very much for your help Erich and Alice!&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2018 15:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Unable-to-select-FreeRTOS-as-an-OS-in-New-Project-Wizard-screen/m-p/786411#M2657</guid>
      <dc:creator>josephjean-jacq</dc:creator>
      <dc:date>2018-06-20T15:18:10Z</dc:date>
    </item>
  </channel>
</rss>