<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Freertos task aware debug with Jlink probe with relocated application in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779256#M2516</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SDK version is 2.2.0, the manifest version is 3.0.0.&lt;/P&gt;&lt;P&gt;I'm using a real Segger J-Link debug probe (firmware version 6.20g).&lt;/P&gt;&lt;P&gt;At the moment I cannot use P&amp;amp;E, I will try as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Biafra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jan 2018 16:52:54 GMT</pubDate>
    <dc:creator>biafra</dc:creator>
    <dc:date>2018-01-30T16:52:54Z</dc:date>
    <item>
      <title>Freertos task aware debug with Jlink probe with relocated application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779254#M2514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm unsing the latest version of MCUXpresso (10.1.1) and I'm facing an issue (that was present even in the preceeding version 10.1.0).&lt;/P&gt;&lt;P&gt;I'm debugging an application running Freertos using Jlink probe.&lt;/P&gt;&lt;P&gt;The application is relocated and runs from address 0x10200.&lt;/P&gt;&lt;P&gt;If the FreeRTOS plugin is selected the application doesn't run and if I pause the execution the PC in is the bootloader area (where there is some garbage).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2623iA378A073B526D6D0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2556i0A2DCB4EDB7E0237/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;the FreeRTOS plugin isn't&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;selected the application&lt;SPAN&gt;&amp;nbsp;works fine (obviously I can't use the task aware debug feature).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;If the same application runs from address 0, it works fine regrdless of the FreeRTOS plugin is selected or not.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;Is some configuration needed or some other step to work with&amp;nbsp;FreeRTOS plugin selected and the application running from an address other than 0?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;Many thanks&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;Biafra&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jan 2018 10:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779254#M2514</guid>
      <dc:creator>biafra</dc:creator>
      <dc:date>2018-01-11T10:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: Freertos task aware debug with Jlink probe with relocated application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779255#M2515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Biafra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried following the recommendations from this thread?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/468593"&gt; Enable "Select RTOS plugin" failed&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Exactly which SDK and version are you using? [Check the Installed SDKs view in the IDE for both SDK Version and Manifest Version.]&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And are you using a "real" SEGGER J-Link debug probe (we have tested with a J-Link+ here), or are you perhaps using OpenSDA J-Link firmware?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you successfully use the FreeRTOS support provided by&amp;nbsp;P&amp;amp;E and/or LinkServer(CMSIS-DAP / DAP-Link) debug connections? If necessary you can get the firmware for those for the OpenSDA probe from various&amp;nbsp;Kinetis eval board's&amp;nbsp; from &lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fopensda" rel="nofollow" target="_blank"&gt;http://www.nxp.com/opensda&lt;/A&gt;)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 14:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779255#M2515</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2018-01-30T14:59:23Z</dc:date>
    </item>
    <item>
      <title>Re: Freertos task aware debug with Jlink probe with relocated application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779256#M2516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SDK version is 2.2.0, the manifest version is 3.0.0.&lt;/P&gt;&lt;P&gt;I'm using a real Segger J-Link debug probe (firmware version 6.20g).&lt;/P&gt;&lt;P&gt;At the moment I cannot use P&amp;amp;E, I will try as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Biafra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 16:52:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779256#M2516</guid>
      <dc:creator>biafra</dc:creator>
      <dc:date>2018-01-30T16:52:54Z</dc:date>
    </item>
    <item>
      <title>Re: Freertos task aware debug with Jlink probe with relocated application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779257#M2517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried P&amp;amp;E probe, I cannot debug at all. It seems that the program&amp;nbsp;is loaded, but there is no start button available (it is grayed), no activity can be seen and if&amp;nbsp;I hit the pause button, nothing happens and I can only hit the stop button.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Biafra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Feb 2018 14:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Freertos-task-aware-debug-with-Jlink-probe-with-relocated/m-p/779257#M2517</guid>
      <dc:creator>biafra</dc:creator>
      <dc:date>2018-02-05T14:53:27Z</dc:date>
    </item>
  </channel>
</rss>