<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Reading program file from a LPC chip with MCUXpresso</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768029#M2259</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am struggling with getting a bootloader axf file and a program boot axf file into one axf file to program it in one time. &lt;BR /&gt;You would say that you can do it by first programming the bootloader and than the programming the program. If that works you download the complete code out of the chip.&lt;BR /&gt;But I can't find the option in MCUXpresso to read the code from the chip. I am using the LPC-Link 1 for this. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Mar 2018 16:15:01 GMT</pubDate>
    <dc:creator>rudycoppens</dc:creator>
    <dc:date>2018-03-16T16:15:01Z</dc:date>
    <item>
      <title>Reading program file from a LPC chip with MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768029#M2259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am struggling with getting a bootloader axf file and a program boot axf file into one axf file to program it in one time. &lt;BR /&gt;You would say that you can do it by first programming the bootloader and than the programming the program. If that works you download the complete code out of the chip.&lt;BR /&gt;But I can't find the option in MCUXpresso to read the code from the chip. I am using the LPC-Link 1 for this. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 16:15:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768029#M2259</guid>
      <dc:creator>rudycoppens</dc:creator>
      <dc:date>2018-03-16T16:15:01Z</dc:date>
    </item>
    <item>
      <title>Re: Reading program file from a LPC chip with MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768030#M2260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You could use the memory view, as per:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/thread/389034"&gt;Importing / Exporting memory to/from a target MCU&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or it might be easier to convert each of the AXF to s records (or similar) which you can do using the supplied objcopy tool (as per MCUXpresso IDE v10.1 User Guide section 16.11,"Creating bin,hex or S-Record files"), and then "merge" them - for instance using a tool like "srecord" (external link :&amp;nbsp;&lt;A class="link-titled" href="http://srecord.sourceforge.net" title="http://srecord.sourceforge.net"&gt;SRecord 1.64&lt;/A&gt;&amp;nbsp;). &amp;nbsp;You might find this article helpful too :&amp;nbsp;&lt;A class="link-titled" href="https://mcuoneclipse.com/2016/02/26/merging-s19-files/" title="https://mcuoneclipse.com/2016/02/26/merging-s19-files/"&gt;Merging S19 Files | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 17:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768030#M2260</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-16T17:15:59Z</dc:date>
    </item>
    <item>
      <title>Re: Reading program file from a LPC chip with MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768031#M2261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the fast response!&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried your options. I would really like to use the first option with the memory exporting but I can't click on that function, it's not active.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you tell me which programmer you need to do this. I am now using a PLC-Link 1 for programming.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/34293iB7624B4E7D9C455F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Mar 2018 13:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768031#M2261</guid>
      <dc:creator>rudycoppens</dc:creator>
      <dc:date>2018-03-19T13:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: Reading program file from a LPC chip with MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768032#M2262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I suspect you aren't currently connected to the target -&amp;gt;&amp;nbsp;You need to have an active debug connection down to the target MCU in order to view (and hence save) memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This can either be a standard debug connection, or if you have already got everything programmed down to memory, you could start an attach-only connection (see section 10.3.1, "Connecting to a running target (attach)" of the MCUXpresso IDE v10.1 User Guide for more details).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then once the target is paused, open a Memory view onto the start of flash, and you should then be able to save.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Mar 2018 15:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Reading-program-file-from-a-LPC-chip-with-MCUXpresso/m-p/768032#M2262</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-19T15:12:20Z</dc:date>
    </item>
  </channel>
</rss>