<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: when I use mcuxpresso to debug FRDMK64 report error:&amp;quot;op EraseSector (0x0, 0x0, 0x4) status 0x1 - driver reported driver error - INTKFMM driver rc 16 - Flash protection violation   op EraseSector (0x0, 0x0, 0x4) status 0x1 - driver reported driver erro</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/when-I-use-mcuxpresso-to-debug-FRDMK64-report-error-quot-op/m-p/763400#M2177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;does it caused by MPU ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jan 2018 05:32:05 GMT</pubDate>
    <dc:creator>leilovelei100</dc:creator>
    <dc:date>2018-01-29T05:32:05Z</dc:date>
    <item>
      <title>when I use mcuxpresso to debug FRDMK64 report error:"op EraseSector (0x0, 0x0, 0x4) status 0x1 - driver reported driver error - INTKFMM driver rc 16 - Flash protection violation   op EraseSector (0x0, 0x0, 0x4) status 0x1 - driver reported driver error -</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/when-I-use-mcuxpresso-to-debug-FRDMK64-report-error-quot-op/m-p/763399#M2176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="error info.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30463iD47FF6B20016BF1E/image-size/large?v=v2&amp;amp;px=999" role="button" title="error info.png" alt="error info.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jan 2018 04:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/when-I-use-mcuxpresso-to-debug-FRDMK64-report-error-quot-op/m-p/763399#M2176</guid>
      <dc:creator>leilovelei100</dc:creator>
      <dc:date>2018-01-29T04:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: when I use mcuxpresso to debug FRDMK64 report error:"op EraseSector (0x0, 0x0, 0x4) status 0x1 - driver reported driver error - INTKFMM driver rc 16 - Flash protection violation   op EraseSector (0x0, 0x0, 0x4) status 0x1 - driver reported driver erro</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/when-I-use-mcuxpresso-to-debug-FRDMK64-report-error-quot-op/m-p/763400#M2177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;does it caused by MPU ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jan 2018 05:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/when-I-use-mcuxpresso-to-debug-FRDMK64-report-error-quot-op/m-p/763400#M2177</guid>
      <dc:creator>leilovelei100</dc:creator>
      <dc:date>2018-01-29T05:32:05Z</dc:date>
    </item>
    <item>
      <title>Re: when I use mcuxpresso to debug FRDMK64 report error:"op EraseSector (0x0, 0x0, 0x4) status 0x1 - driver reported driver error - INTKFMM driver rc 16 - Flash protection violation   op EraseSector (0x0, 0x0, 0x4) status 0x1 - driver reported driver erro</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/when-I-use-mcuxpresso-to-debug-FRDMK64-report-error-quot-op/m-p/763401#M2178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Firstly, it is possible to accidentally attempt to flash a project for one MCU onto a different MCU - this can lead to errors from the flash driver. The correct flash driver for the K64 MCU is called FTFE_4K - you can check the debug log to see which flash driver is being used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming there was no error as described above, I would suggest you attempt to mass erase this part. This process is described in the User Manual for the IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First location the LinkServer GUI Flash Programmer Icon from the ToolBar (it looks like a small MCU). Then be sure to select the Erase flash memory tab, and check the Mass erase radio button as below. Then click OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33615iF427501C6D731865/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this also fails, I would next try the third tab 'Resurrect locked Kinetis device'. To use this feature, simply select this tab and click OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In both of these cases all data on the flash will be erased.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 12:29:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/when-I-use-mcuxpresso-to-debug-FRDMK64-report-error-quot-op/m-p/763401#M2178</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-01-30T12:29:22Z</dc:date>
    </item>
  </channel>
</rss>