<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Adaware Antivirus kills MCUXpresso IDE in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Adaware-Antivirus-kills-MCUXpresso-IDE/m-p/753014#M1765</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As the MCUxpresso IDE expert said on &lt;A href="https://community.nxp.com/thread/465633"&gt;Bitdefender marks MCUXpresso IDE as a virus&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"Virus scanning on systems we have here are not showing any such issues (though we aren't using&amp;nbsp;Bitdefender). If your are still seeing problems, I suggest you try again to prevent the scan of the IDE."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Apr 2018 07:50:09 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2018-04-03T07:50:09Z</dc:date>
    <item>
      <title>Adaware Antivirus kills MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Adaware-Antivirus-kills-MCUXpresso-IDE/m-p/753013#M1764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When&amp;nbsp;I try to launch a newly&amp;nbsp;installed MCUXpresso on&amp;nbsp;a Windows 7&amp;nbsp;Pro 64-bit PC,&amp;nbsp;the file: MCUXpressoIDE_10.1.1_606\ide\mcuxpressoide.exe is killed by the latest version of Adaware Antivirus 12.3.909.11573 (Bitdefender engine and definition files), so the IDE is not loaded. It may be a false positive, but I don't want to bed on that and switch Adaware off every time MCUXpresso should be used - especially because MCUXpresso seems to contain&amp;nbsp;3rd party software and is not downloaded from an NXP server, but from a general purpose download site, which may be&amp;nbsp;infected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas what to do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Mar 2018 16:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Adaware-Antivirus-kills-MCUXpresso-IDE/m-p/753013#M1764</guid>
      <dc:creator>carstenkanstrup</dc:creator>
      <dc:date>2018-03-30T16:44:52Z</dc:date>
    </item>
    <item>
      <title>Re: Adaware Antivirus kills MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Adaware-Antivirus-kills-MCUXpresso-IDE/m-p/753014#M1765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As the MCUxpresso IDE expert said on &lt;A href="https://community.nxp.com/thread/465633"&gt;Bitdefender marks MCUXpresso IDE as a virus&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"Virus scanning on systems we have here are not showing any such issues (though we aren't using&amp;nbsp;Bitdefender). If your are still seeing problems, I suggest you try again to prevent the scan of the IDE."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 07:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Adaware-Antivirus-kills-MCUXpresso-IDE/m-p/753014#M1765</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-04-03T07:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: Adaware Antivirus kills MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Adaware-Antivirus-kills-MCUXpresso-IDE/m-p/753015#M1766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I know that case and has also referred to that on the other thread&amp;nbsp;&lt;A href="https://community.nxp.com/thread/472966"&gt;Debug problems on MIMXRT1050-EVK&lt;/A&gt;&amp;nbsp;. I have reported the problem to Adaware (hopefully the mcuxpressoide.exe file gets through).&amp;nbsp;Let us see if they can&amp;nbsp;find out if it is a false positive or MCUXpresso is doing something suspicious, which it ought not to do. Anti virus programs&amp;nbsp;must respond to suspicious behavior to be able to detect&amp;nbsp;previously unknown viruses, but this also put some demands on the programmers, who must do everything by the book to prevent a false positive detection.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since others - except for that thread - have not seen similar problems and we also have MCUXpresso running on a Windows 10 laptop with the same version of Adaware without any virus warnings, it is probably a false positive. Unfortunately,&amp;nbsp;Adaware has no way to mark a given file as safe,&amp;nbsp;so I would have to switch off the real time protection every time I would use MCUXpresso and this is&amp;nbsp;an unacceptable&amp;nbsp;solution, as it will also disable the real time protection for everything else&amp;nbsp;running on the computer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 09:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Adaware-Antivirus-kills-MCUXpresso-IDE/m-p/753015#M1766</guid>
      <dc:creator>carstenkanstrup</dc:creator>
      <dc:date>2018-04-03T09:10:10Z</dc:date>
    </item>
  </channel>
</rss>