<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: MCUXpresso IDE and FDRM-K64F programming issue</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751752#M1749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The entire debug console log is attached. I also noticed that the board works fine with PCs running on Window 7. Only PCs with Windows 10 have these issues.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jan 2018 18:12:56 GMT</pubDate>
    <dc:creator>atfarsoni</dc:creator>
    <dc:date>2018-01-24T18:12:56Z</dc:date>
    <item>
      <title>MCUXpresso IDE and FDRM-K64F programming issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751750#M1747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just started using the FRDM-K64F board and encountered several issues:&lt;/P&gt;&lt;P&gt;1- When for the first time the board is connected to the USB port of my PC, the pre-loaded (Bubble) app does not work as expected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2-&amp;nbsp;With the board powered by the USB port, my PC opens a directory MBED (E:\) with several empty files.&lt;/P&gt;&lt;P&gt;3- With all software installed, I tried to program the board using SDK examples, at the end of programming (Debug), I get&amp;nbsp;a connection error. Attached is the debug log console.&lt;/P&gt;&lt;P&gt;Below&amp;nbsp;was also copied from the Console window:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;============= END SCRIPT =============================&lt;BR /&gt;Probe Firmware: MBED CMSIS-DAP (MBED)&lt;BR /&gt;Serial Number: 0240020163867E7C9E7883C4&lt;BR /&gt;VID:PID: 0D28:0204&lt;BR /&gt;USB Path: \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#8&amp;amp;160b5c6&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;connection failed - Nn(05). Wire ACK Fault in DAP access.. Retrying&lt;BR /&gt;Failed on connect: Nn(05). Wire ACK Fault in DAP access&lt;BR /&gt;Connected&amp;amp;Reset. Was: NotConnected. DpID: 00000000. CpuID: 00000000. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Last stub error 0: OK&lt;BR /&gt;Last sticky error: 0x0 AIndex: 0&lt;BR /&gt;Debug bus selected: MemAp 0&lt;BR /&gt;DAP Speed test unexecuted or failed&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;(100) Target Connection Failed&lt;BR /&gt;error closing down debug session - Ee(FF). Redlink interface error 255.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate any help.&lt;/P&gt;&lt;P&gt;Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 01:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751750#M1747</guid>
      <dc:creator>atfarsoni</dc:creator>
      <dc:date>2018-01-24T01:59:58Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE and FDRM-K64F programming issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751751#M1748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You don’t have a viable debug connection. Please post the entire debug console log which captures the output from the script execution. You may need to use the mass erase script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 05:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751751#M1748</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-01-24T05:10:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE and FDRM-K64F programming issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751752#M1749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The entire debug console log is attached. I also noticed that the board works fine with PCs running on Window 7. Only PCs with Windows 10 have these issues.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 18:12:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751752#M1749</guid>
      <dc:creator>atfarsoni</dc:creator>
      <dc:date>2018-01-24T18:12:56Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE and FDRM-K64F programming issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751753#M1750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, we'll let you know what we find.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 18:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751753#M1750</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-01-24T18:14:49Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE and FDRM-K64F programming issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751754#M1751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The console logs I'd like to see can be copied from the MCUXpresso IDE console tab. One console is for gdb-traces. The other is the debug log. See &lt;A href="https://community.nxp.com/thread/389146"&gt;The Debug Log. &lt;/A&gt;Please copy these and paste as a response, or, add as an attachment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT: If you're a Windows 10 user, there have been reports of the OpenSDA v2.1 becoming corrupted. See &lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&amp;amp;tid=vanOpenSDA#TWR-K64F120M" title="https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&amp;amp;tid=vanOpenSDA#TWR-K64F120M"&gt;OpenSDA Serial and Debug Adapter|NXP.&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 22:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-and-FDRM-K64F-programming-issue/m-p/751754#M1751</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-01-24T22:06:10Z</dc:date>
    </item>
  </channel>
</rss>