<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Multiple Instances of Target and IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Multiple-Instances-of-Target-and-IDE/m-p/751058#M1733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeremy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- There is a method about debug two projects on&amp;nbsp; two boards in the same time -&amp;gt;&amp;nbsp; using the different&lt;/P&gt;&lt;P&gt;debug interface. For example one board use JLink, another use P&amp;amp;E&amp;nbsp; , I test on my side , it can work&lt;/P&gt;&lt;P&gt;well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- When both using the Jlink debug method, sorry I don't know how to recognize the corresponding USB port.&lt;/P&gt;&lt;P&gt;There is a tutorial about debugging multiple boards&amp;nbsp; with J-link :&lt;/P&gt;&lt;P&gt;&lt;A class="jivelink9" href="https://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/" title="https://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/"&gt;https://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Nov 2017 07:10:04 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2017-11-07T07:10:04Z</dc:date>
    <item>
      <title>Multiple Instances of Target and IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Multiple-Instances-of-Target-and-IDE/m-p/751057#M1732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to run two different images of a FreeRTOS application on two target systems FRDM-MK66 from my Windows workstation.&amp;nbsp; I created two work spaces and launched one system, then connected a second target system and started a second instance of the IDE.&amp;nbsp; When I attempt to debug the second system, the first IDE is halted and the first target system falls under the control of the second IDE.&amp;nbsp; When I start to debug it asks me to select a debug probe and I've tried one, then the other with the same result.&amp;nbsp; I see in my device manager that two JLink CDC UART ports are created.&amp;nbsp; Is what I'm trying to do not supported or have I missed some detail?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Nov 2017 16:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Multiple-Instances-of-Target-and-IDE/m-p/751057#M1732</guid>
      <dc:creator>jeremyanderson</dc:creator>
      <dc:date>2017-11-06T16:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Instances of Target and IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Multiple-Instances-of-Target-and-IDE/m-p/751058#M1733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeremy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- There is a method about debug two projects on&amp;nbsp; two boards in the same time -&amp;gt;&amp;nbsp; using the different&lt;/P&gt;&lt;P&gt;debug interface. For example one board use JLink, another use P&amp;amp;E&amp;nbsp; , I test on my side , it can work&lt;/P&gt;&lt;P&gt;well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- When both using the Jlink debug method, sorry I don't know how to recognize the corresponding USB port.&lt;/P&gt;&lt;P&gt;There is a tutorial about debugging multiple boards&amp;nbsp; with J-link :&lt;/P&gt;&lt;P&gt;&lt;A class="jivelink9" href="https://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/" title="https://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/"&gt;https://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 07:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Multiple-Instances-of-Target-and-IDE/m-p/751058#M1733</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-11-07T07:10:04Z</dc:date>
    </item>
  </channel>
</rss>