<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: MCUExpresso with LPC-Link2</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633997#M168</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, the connect script is not useful. I didn't have to use it. The required action is to not enable the ISP reset which causes the assertion of the physical reset line. &amp;nbsp;The soft reset from the JTAG commanding is all that's necessary.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If someone wishes to use the ISP pin mode, it is too late in the process when the script is run. The debugger handler already times out looking for the CPU too soon after reset, and never gets a chance to run the delay script. If someone's custom target board uses an active reset supervisor chip, they must not allow the debugger to assert the physical reset (as MCUXpresso is implemented at this time).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;-John DeMar&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;A class="link-titled" href="https://www.linkedin.com/in/jsdemar/" title="https://www.linkedin.com/in/jsdemar/"&gt;https://www.linkedin.com/in/jsdemar/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Apr 2017 21:26:35 GMT</pubDate>
    <dc:creator>JohnDeMar</dc:creator>
    <dc:date>2017-04-24T21:26:35Z</dc:date>
    <item>
      <title>MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633989#M160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running MCUExpresso with our custom LPC4330 hardware and a Keil ULink2 JTAG interface. It has been working fairly well, but we'd like to use the lower-cost LPC-Link2 for other people in our group.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an LPC-Link2 brand new, out of the box. I've followed a variety of misc online instructions, and I believe I have it set up correctly. But, it does not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a definitely source for information on getting the LPC-Link2 running with MCUExpresso?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; -John DeMar&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;A class="link-titled" href="https://www.linkedin.com/in/jsdemar/" title="https://www.linkedin.com/in/jsdemar/"&gt;https://www.linkedin.com/in/jsdemar/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2017 15:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633989#M160</guid>
      <dc:creator>JohnDeMar</dc:creator>
      <dc:date>2017-04-21T15:30:50Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633990#M161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A DOA LPC-Link2 is a very rare occurrence. What is your host system? If Windows, first make sure the appropriate drivers are installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/630577"&gt;Booting LPC-Link2&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two jumpers on the LPC-Link2 board, JP1 and JP2. A connected JP1 boots the probe firmware from flash. To flash the probe firmware, you'll first need LPCScrypt. Instead, if you leave JP1 open, the processor boots to DFU mode. The MCUXpresso IDE will recognize an LPC device, and DFU the probe firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ControlPanel1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11320i3D4274609387717E/image-size/large?v=v2&amp;amp;px=999" role="button" title="ControlPanel1.jpg" alt="ControlPanel1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once the DFU is complete, you should see a CMSIS-DAP probe boot up as a Windows connected device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ControPanel2.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11374iA5B9E1006C4A5320/image-size/large?v=v2&amp;amp;px=999" role="button" title="ControPanel2.jpg" alt="ControPanel2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2017 16:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633990#M161</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-04-21T16:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633991#M162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here's what I get when I boot with jumper 1 removed (DFU mode):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11376iDE333A323269EE0D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ran MCUXpresso and went to the "chip" icon to erase flash:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11396iC398E66655137F4A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It sees the device and could erase the external SPIFI flash in our target. Good so far.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, when I try to run a debugger session, I get this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11445i5A39823CA9AB2087/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I tried with and without JP2 installed (buffer power). Same error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My debug config for the project looks like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11498iA180F9B97B58055A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I used LPCScrypt and flashed it with CMSIS-DAP. Installed jumper 1 and power cycled the LPC-Link2.&lt;/P&gt;&lt;P&gt;It showed up like this in Devices and Printers:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11532iDEB84453EF090652/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;A slightly older version that the one MCUXpresso loads (5.182).&lt;/P&gt;&lt;P&gt;I repeated the session with the same error when trying to start the debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I repeated with LinkServer changed to "LPC-Link (HID)" and "LPC-Link (WinUSB) or RDB-Link" under Properties -&amp;gt; Run/Debug Settings -&amp;gt; (Project debug name) -&amp;gt; Edit Launch Config Properties -&amp;gt; Debugger -&amp;gt; Emulation selection. &amp;nbsp;Same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After all these failed sessions, I have to install the ISP jumper on our target to erase or flash the SPIFI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I went back to the ULink2 and repeated the above with the LPC-Link2 unplugged. The debugging session worked fine under MCUXpresso.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What else can I try??? &amp;nbsp;Our target board is LPC4330 set for SPIFI boot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;-John DeMar&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.linkedin.com%2Fin%2Fjsdemar%2F" rel="nofollow" style="color: #5e89c1; background-color: #ffffff; border: 0px; text-decoration: underline; padding: 0px calc(12px + 0.35ex) 0px 0px;" target="_blank"&gt;https://www.linkedin.com/in/jsdemar/&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2017 21:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633991#M162</guid>
      <dc:creator>JohnDeMar</dc:creator>
      <dc:date>2017-04-21T21:00:26Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633992#M163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on the information above, the IDE has good communications with the debug probe (despite the slightly miss-leading error), the problem is that the LPC-Link2 cannot communicate with the target MCU. (You would see exactly this behaviour if there was no 10 way debug connection to the board).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore initially I would focus on the physical connection from the LPC-Link2 to your target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - check the basics, is the 10 wire debug cable connected to J7 on the LPC-Link2 board&lt;/P&gt;&lt;P&gt;2 - is the wire orientation correct onto your custom LPC4330 hardware&lt;/P&gt;&lt;P&gt;3 - check the target is powered either locally or via the LPC-Link2 (JP2 link made)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate that you have a good debug connection via Keil ULink2 JTAG interface, but the following document may be worth reading:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/388998"&gt;Design Considerations for Debug&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 14:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633992#M163</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-04-24T14:50:39Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633993#M164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC-Link2 can erase and flash our target, so there is&amp;nbsp;not the same as having the 10-pin header disconnected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There appears to be different timing in the LPC-Link2 code when flashing vs debugging. We are looking at the reset circuit implementation on our target. It has an active reset supervisor with an internal pullup, but it also monitors the reset signal and assert a stretch to nominally 150msecs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there open source to the LPC-Link2 code so that I can allow it to wait longer when asserting a reset before looking for the CPU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 15:17:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633993#M164</guid>
      <dc:creator>JohnDeMar</dc:creator>
      <dc:date>2017-04-24T15:17:59Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633994#M165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LPC-Link2 firmware has a couple of proprietary additions, so it's not open source. And, you don't need it. I'd recommend you add a custom reset script with a built in delay. LinkServer includes an example script which can be used to program a delay. See the delayexample.scp in the Scripts folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When a reset script is used, MCUXpresso presumes everything reset related is included in the script. So, for example, you'll need to add a command to send a core reset signal to the part. I've cut and paste a script below should do what you need. Note you'll edit your project debug configuration to use a reset script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Example script:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;100 REM -----------------------------------------------------------------&lt;BR /&gt;110 REM LPC4330 Reset Script (500 ms delay loop)&lt;BR /&gt;120 REM -----------------------------------------------------------------&lt;BR /&gt;130 REM Find probe index and select probe+core&lt;BR /&gt;140 REM -----------------------------------------------------------------&lt;BR /&gt;150 p% = ProbeFirstFound&lt;BR /&gt;160 SelectProbeCore p% 0&lt;BR /&gt;170 REM -----------------------------------------------------------------&lt;BR /&gt;180 REM Ensure reset vector catch is set&lt;BR /&gt;190 REM -----------------------------------------------------------------&lt;BR /&gt;200 CMResetVectorCatchSet this&lt;BR /&gt;210 REM -----------------------------------------------------------------&lt;BR /&gt;220 REM Issue VECTRESET&lt;BR /&gt;230 REM -----------------------------------------------------------------&lt;BR /&gt;240 CMVectResetReq this&lt;BR /&gt;250 REM -----------------------------------------------------------------&lt;BR /&gt;260 REM Set initial timer value (milliseconds * 10)&lt;BR /&gt;270 REM -----------------------------------------------------------------&lt;BR /&gt;280 t% = TIME&lt;BR /&gt;290 PRINT "Time:&amp;nbsp;&amp;nbsp;&amp;nbsp; "; t%&lt;BR /&gt;300 REM -----------------------------------------------------------------&lt;BR /&gt;310 REM Current timer value is v%&lt;BR /&gt;320 REM -----------------------------------------------------------------&lt;BR /&gt;330 REPEAT&lt;BR /&gt;340&amp;nbsp;&amp;nbsp; v% = TIME&lt;BR /&gt;350&amp;nbsp;&amp;nbsp; e% = v% - t%&lt;BR /&gt;360 UNTIL e% &amp;gt;= 5000&lt;BR /&gt;370 REM -----------------------------------------------------------------&lt;BR /&gt;380 REM Elapsed time in milliseconds&lt;BR /&gt;390 REM -----------------------------------------------------------------&lt;BR /&gt;400 e% = e% / 10&lt;BR /&gt;410 PRINT "Elapsed (ms): "; e%&lt;BR /&gt;420 REM CMResetVectorCatchClear this&lt;BR /&gt;430 END&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 16:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633994#M165</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-04-24T16:34:34Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633995#M166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Following this thread: &amp;nbsp;&lt;A href="https://community.nxp.com/thread/442611"&gt;LPCXpresso, LPC-Link2  and RESET line&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I turned&amp;nbsp;off "Pull ISP on reset", under Windows-&amp;gt;Preferences_&amp;gt;LinkServer Options:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14134i2327A7654C5F5680/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Even though I do not have the ISP line attached on our target, the LPC-Link2 still uses the RESET line if that mode is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I set "Attach Only" to "False" under the Project's debugger configuration, which allows scripts to run:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14182iEAA11C1CD38EF83B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I no longer see the RESET signal being asserted low upon initiating a debugger session. That was causing the Reset Supervisor IC to stretch the reset longer than the debugger's wait time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that it doesn't need the reset delay script you suggested. &amp;nbsp;It wouldn't help anyhow because the debug mode looks for the CPU cores before it runs the script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;-John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 18:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633995#M166</guid>
      <dc:creator>JohnDeMar</dc:creator>
      <dc:date>2017-04-24T18:19:13Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633996#M167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Glad to hear you've connected. As you discovered in the other forum thread, the timed delay concept can also be leveraged from a connect script when needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 20:42:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633996#M167</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-04-24T20:42:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso with LPC-Link2</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633997#M168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, the connect script is not useful. I didn't have to use it. The required action is to not enable the ISP reset which causes the assertion of the physical reset line. &amp;nbsp;The soft reset from the JTAG commanding is all that's necessary.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If someone wishes to use the ISP pin mode, it is too late in the process when the script is run. The debugger handler already times out looking for the CPU too soon after reset, and never gets a chance to run the delay script. If someone's custom target board uses an active reset supervisor chip, they must not allow the debugger to assert the physical reset (as MCUXpresso is implemented at this time).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;-John DeMar&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;A class="link-titled" href="https://www.linkedin.com/in/jsdemar/" title="https://www.linkedin.com/in/jsdemar/"&gt;https://www.linkedin.com/in/jsdemar/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 21:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUExpresso-with-LPC-Link2/m-p/633997#M168</guid>
      <dc:creator>JohnDeMar</dc:creator>
      <dc:date>2017-04-24T21:26:35Z</dc:date>
    </item>
  </channel>
</rss>