<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can a program on the LPCEXpresso54608 be downloaded and debugged without Link2? in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741071#M1483</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just to follow up on Jennie's post. There is a debug interface built into the LPCXpresso54608 board that is functionally an LPC-Link2. Alternatively an external debug probe can also be used if required. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Dec 2017 13:17:35 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2017-12-22T13:17:35Z</dc:date>
    <item>
      <title>Can a program on the LPCEXpresso54608 be downloaded and debugged without Link2?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741069#M1481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The question says it all&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2017 16:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741069#M1481</guid>
      <dc:creator>tomstokland</dc:creator>
      <dc:date>2017-12-21T16:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: Can a program on the LPCEXpresso54608 be downloaded and debugged without Link2?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741070#M1482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;LPCXpresso 54008 on board debug probe supports CMSIS-DAP/SEGGER J-Link interface.&lt;/P&gt;&lt;P&gt;There is no option to simulate program without a board under MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Dec 2017 07:20:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741070#M1482</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-12-22T07:20:03Z</dc:date>
    </item>
    <item>
      <title>Re: Can a program on the LPCEXpresso54608 be downloaded and debugged without Link2?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741071#M1483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just to follow up on Jennie's post. There is a debug interface built into the LPCXpresso54608 board that is functionally an LPC-Link2. Alternatively an external debug probe can also be used if required. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Dec 2017 13:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741071#M1483</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-12-22T13:17:35Z</dc:date>
    </item>
    <item>
      <title>Re: Can a program on the LPCEXpresso54608 be downloaded and debugged without Link2?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741072#M1484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The board doesn't show up either as a VSP or any other way. At this point I'm assuming it's defective.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Dec 2017 14:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741072#M1484</guid>
      <dc:creator>tomstokland</dc:creator>
      <dc:date>2017-12-22T14:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: Can a program on the LPCEXpresso54608 be downloaded and debugged without Link2?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741073#M1485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe you can follow this&amp;nbsp; link to update the on-board firmware to see if this can fix the problem, in case the problem is not on the board defective.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/925864"&gt;https://community.nxp.com/message/925864&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Dec 2017 10:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-a-program-on-the-LPCEXpresso54608-be-downloaded-and-debugged/m-p/741073#M1485</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-12-26T10:35:59Z</dc:date>
    </item>
  </channel>
</rss>