<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Download code in flash FRDM-KV10Z in MCUXpresso using Segger/PE Micro in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739972#M1471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am downloading the led gpio SDK example using Segger. The code is working after reset if I select the box which you have suggested.&lt;/P&gt;&lt;P&gt;But if I dont select it, the code is not working after reset.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Nov 2017 11:58:10 GMT</pubDate>
    <dc:creator>shoaibshaikh</dc:creator>
    <dc:date>2017-11-06T11:58:10Z</dc:date>
    <item>
      <title>Download code in flash FRDM-KV10Z in MCUXpresso using Segger/PE Micro</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739970#M1469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;Dear all,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;I am facing problems in downloading my code to flash memory in MCUXpresso 10.0.0 and 10.0.2 in Windows 7 professional.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;I am using FRDM-KV10Z and FRDM-K64F with Segger Jlink as debugger. I also tried using JFlash lite after generating a binary file from the axf file but it does not work. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;&lt;BR /&gt; I found this link (&lt;A _jive_internal="true" href="https://community.nxp.com/thread/449152"&gt;https://community.nxp.com/thread/449152&lt;/A&gt;) which suggested a way using PE Micro debugger. I changed the debug mode to PE Micro by copying (DEBUG_OpenSDA_for_MBED_Bootloader_by_Pemicro_v108_v2.1.bin) file for KV10Z in the bootloader. The code worked in the debug mode but after reconnecting power the code was not working. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;&lt;BR /&gt; Could you kindly inform me how code can be downloaded in flash using Segger for KV10Z and K64F development boards.&lt;BR /&gt; &lt;BR /&gt; Thanks, &lt;BR /&gt; Shoaib&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Nov 2017 13:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739970#M1469</guid>
      <dc:creator>shoaibshaikh</dc:creator>
      <dc:date>2017-11-01T13:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: Download code in flash FRDM-KV10Z in MCUXpresso using Segger/PE Micro</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739971#M1470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="305474" data-username="shoaibshaikh" href="https://community.nxp.com/people/shoaibshaikh"&gt;Shoaib Shaikh&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If&amp;nbsp; you want to use Segger Jlink debug interface, after download project into your chip,&lt;/P&gt;&lt;P&gt;Reset it , it also can work well . Please have a look at my attachment about how to download. I use FRDM-K64 board.&lt;/P&gt;&lt;P&gt;And if it can’t work on your side after reset, please tell me which project do you used .&lt;/P&gt;&lt;P&gt;If SDK example, when import, please check “ Redirect printf/scanf to UART”&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16674i505D8434213F7EEC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Nov 2017 09:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739971#M1470</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-11-03T09:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: Download code in flash FRDM-KV10Z in MCUXpresso using Segger/PE Micro</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739972#M1471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am downloading the led gpio SDK example using Segger. The code is working after reset if I select the box which you have suggested.&lt;/P&gt;&lt;P&gt;But if I dont select it, the code is not working after reset.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Nov 2017 11:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739972#M1471</guid>
      <dc:creator>shoaibshaikh</dc:creator>
      <dc:date>2017-11-06T11:58:10Z</dc:date>
    </item>
    <item>
      <title>Re: Download code in flash FRDM-KV10Z in MCUXpresso using Segger/PE Micro</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739973#M1472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, if your project is configured to output via semihosting (rather than say over UART), then if there is no debug session active, the first semihosting operation will block (due to a hard fault being taken).&amp;nbsp;See section 11.4 "What is Semihosting? and 11.5, "Use of printf" of the MCUXpresso IDE v10.0.2 User Guide for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Aside: the next MCUXpresso IDE release will provide a hard fault handler mechanism to prevent the first semihosting operation when no debugger is connected from blocking. But you can achieve a similar affect now by pulling the handler in from :&amp;nbsp;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/782843?commentID=782843#comment-782843" title="https://community.nxp.com/message/782843?commentID=782843#comment-782843"&gt;https://community.nxp.com/message/782843?commentID=782843#comment-782843&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Nov 2017 13:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Download-code-in-flash-FRDM-KV10Z-in-MCUXpresso-using-Segger-PE/m-p/739973#M1472</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-11-06T13:03:27Z</dc:date>
    </item>
  </channel>
</rss>