<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: MCUXpresso Jlink debug error 'Program file does not exist'</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738827#M1450</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are various steps that can be taken to reduce the code size of generated applications - as the primary goal of these example projects is to function correctly, rather than to be of a minimum code size.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For instance, the code inside the generated project is sufficient to allow you to easily swap between&amp;nbsp;&lt;SPAN&gt;semihosting and&amp;nbsp;UART output for any debug I/O.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if you are happy to use semihosting and never switch your project over to UART output, then you can potentially remove code inside your project that enables to UART.&amp;nbsp;Similar if you are going to always use UART, then you can switch the IDE over to using a non-semihosted version of the C library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more background see the following sections of the MCUXpresso IDE v10.1 User Guide...&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Section 13.4, "What is Semihosting"&lt;/LI&gt;&lt;LI&gt;Section 13.5.5, "Printf when using SDK"&lt;/LI&gt;&lt;LI&gt;Section 16.1, "Quick Settings"&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Feb 2018 10:46:57 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2018-02-19T10:46:57Z</dc:date>
    <item>
      <title>MCUXpresso Jlink debug error 'Program file does not exist'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738821#M1444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello guys,&lt;/P&gt;&lt;P&gt;I'm trying to make first 'blinky' project with MCUXpresso. Unfortunately I stuck over debugging starting, i got 'Program file does not exist' error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8001iA1C9FFD209CF0D2D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My debug configurations below :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8044iB28C0CFA397A071F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Buliding is done without errors :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8086i9AFCE1F877331CA5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I don't have .elf file inside my project catalog, without attention to the project settings :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8130i2B6F45DE60BE732A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What may be wrong with my configuration ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Feb 2018 19:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738821#M1444</guid>
      <dc:creator>mkoc</dc:creator>
      <dc:date>2018-02-12T19:56:46Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Jlink debug error 'Program file does not exist'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738822#M1445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Somehow in your launch config the binary file to debug is not specified:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8094iB3A1D56C7B7A34F1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Use the Browse button to select the .axf file and you shall be able to debug it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 07:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738822#M1445</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2018-02-13T07:04:30Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Jlink debug error 'Program file does not exist'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738823#M1446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How did you try to start the debug session? Did you use the Quickstart Panel's "Debug" button which will trigger the IDE's probe discovery and automatic creation &amp;nbsp;of the launch configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, I suggest that you delete any .launch files from inside your project. Then try using the Quickstart Panel "Debug" button.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more details, please see the supplied MCUXpresso IDE v10.1 User Guide - in particular &amp;nbsp;chapter 3, "Debug Solutions Overview" and chapter 10, "Debugging a Project".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 08:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738823#M1446</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-02-13T08:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Jlink debug error 'Program file does not exist'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738824#M1447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for really fast response, my debugger is works now like a charm.&lt;/P&gt;&lt;P&gt;After all i have additional two questions :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Why almost blank project takes around 60% from 32kB mcu ROM ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Is there any easy option to configure functions for RTT Jlink viewer ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 16:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738824#M1447</guid>
      <dc:creator>mkoc</dc:creator>
      <dc:date>2018-02-13T16:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Jlink debug error 'Program file does not exist'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738825#M1448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With regards to you comment about code size of a blank project, we have noticed that there is an issue with the MCUXpresso IDE v10.1.1 new project wizard for SDK-based MCUs, such that the default compiler options are not being set correctly. This causes unused code from the various source files in your project not to be discarded by the linker&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please try the following&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Right click on your project in the Project Explorer view&lt;/LI&gt;&lt;LI&gt;Select Properties&lt;/LI&gt;&lt;LI&gt;Open up &lt;STRONG&gt;C/C++ Build -&amp;gt; Settings&lt;/STRONG&gt; on the left hand side&lt;/LI&gt;&lt;LI&gt;Now in the &lt;STRONG&gt;Tool Settings&lt;/STRONG&gt; tab, open up &lt;STRONG&gt;MCU C Compiler -&amp;gt; Miscellaneous&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;Change the value in the &lt;STRONG&gt;Other Flags&lt;/STRONG&gt; from:&lt;/LI&gt;&lt;/UL&gt;&lt;PRE style="padding-left: 30px;"&gt;-c -fmessage-length=0&lt;/PRE&gt;&lt;P style="padding-left: 30px;"&gt;to&lt;/P&gt;&lt;PRE style="padding-left: 30px;"&gt;-c -ffunction-sections -fdata-sections -ffreestanding -fno-builtin&lt;/PRE&gt;&lt;UL&gt;&lt;LI&gt;Now change the Configuration at the top of the page from "Debug" to "Release" and repeat the change.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now click "OK", then try rebuilding your project.&amp;nbsp;This should make a noticeable difference to the size of the linked application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[We will be fixing this issue with the new project wizard in the next IDE release.]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regard's to SEGGER's RTT mechanism : No, the IDE has no built in support for making use of this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Feb 2018 13:38:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738825#M1448</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-02-14T13:38:28Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Jlink debug error 'Program file does not exist'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738826#M1449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16943i442F4DF558B90E18/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It works indeed, now is 44%. Is it everything what can be done with ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Feb 2018 17:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738826#M1449</guid>
      <dc:creator>mkoc</dc:creator>
      <dc:date>2018-02-17T17:06:17Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Jlink debug error 'Program file does not exist'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738827#M1450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are various steps that can be taken to reduce the code size of generated applications - as the primary goal of these example projects is to function correctly, rather than to be of a minimum code size.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For instance, the code inside the generated project is sufficient to allow you to easily swap between&amp;nbsp;&lt;SPAN&gt;semihosting and&amp;nbsp;UART output for any debug I/O.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if you are happy to use semihosting and never switch your project over to UART output, then you can potentially remove code inside your project that enables to UART.&amp;nbsp;Similar if you are going to always use UART, then you can switch the IDE over to using a non-semihosted version of the C library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more background see the following sections of the MCUXpresso IDE v10.1 User Guide...&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Section 13.4, "What is Semihosting"&lt;/LI&gt;&lt;LI&gt;Section 13.5.5, "Printf when using SDK"&lt;/LI&gt;&lt;LI&gt;Section 16.1, "Quick Settings"&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Feb 2018 10:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Jlink-debug-error-Program-file-does-not-exist/m-p/738827#M1450</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-02-19T10:46:57Z</dc:date>
    </item>
  </channel>
</rss>