<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックDebugging LPC4370 triple core at the same time</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Debugging-LPC4370-triple-core-at-the-same-time/m-p/728219#M1265</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using two LPC-Link2 boards with a triple core LPC4370 MCU, one serving as debug probe and the other being the target. To program it I'm using MCUXpresso with the proprietary LPCOpen libraries.&lt;/P&gt;&lt;P&gt;I've successfully programmed each core with simple applications like incrementing a variable and blinking the board LED and I can actually see them work, but I'm only able to debug two of the cores (M4 + M0app or M0sub) and not the three cores available in LPC4370 at the same time: when I try to debug the third core, the&amp;nbsp;debug&amp;nbsp;session&amp;nbsp;automatically&amp;nbsp;goes to&amp;nbsp;the ResetISR() routine, staying there until I terminate that debug session. I'm following the procedure in "Debugging via LPC-Link2" of&amp;nbsp;&lt;A href="https://community.nxp.com/thread/390661"&gt;LPC43xx Cortex-M4 / M0 Multicore Applications&lt;/A&gt;.&amp;nbsp;Using only two debug sessions, I'm can interchangeably debug each one of the M0 cores.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is if it possible to debug the three cores at the same time instead of stopping one M0 core debug and start another debug session with another M0 core. I can't find any answer about this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;João&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Mar 2018 13:16:45 GMT</pubDate>
    <dc:creator>joocfpinto</dc:creator>
    <dc:date>2018-03-05T13:16:45Z</dc:date>
    <item>
      <title>Debugging LPC4370 triple core at the same time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Debugging-LPC4370-triple-core-at-the-same-time/m-p/728219#M1265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using two LPC-Link2 boards with a triple core LPC4370 MCU, one serving as debug probe and the other being the target. To program it I'm using MCUXpresso with the proprietary LPCOpen libraries.&lt;/P&gt;&lt;P&gt;I've successfully programmed each core with simple applications like incrementing a variable and blinking the board LED and I can actually see them work, but I'm only able to debug two of the cores (M4 + M0app or M0sub) and not the three cores available in LPC4370 at the same time: when I try to debug the third core, the&amp;nbsp;debug&amp;nbsp;session&amp;nbsp;automatically&amp;nbsp;goes to&amp;nbsp;the ResetISR() routine, staying there until I terminate that debug session. I'm following the procedure in "Debugging via LPC-Link2" of&amp;nbsp;&lt;A href="https://community.nxp.com/thread/390661"&gt;LPC43xx Cortex-M4 / M0 Multicore Applications&lt;/A&gt;.&amp;nbsp;Using only two debug sessions, I'm can interchangeably debug each one of the M0 cores.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is if it possible to debug the three cores at the same time instead of stopping one M0 core debug and start another debug session with another M0 core. I can't find any answer about this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;João&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Mar 2018 13:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Debugging-LPC4370-triple-core-at-the-same-time/m-p/728219#M1265</guid>
      <dc:creator>joocfpinto</dc:creator>
      <dc:date>2018-03-05T13:16:45Z</dc:date>
    </item>
  </channel>
</rss>