<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Upload and run example projects on LCP1549</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726487#M1234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;Hi!&amp;nbsp; &amp;nbsp;I installed MCUXpresso IDE v10.1.1 on my MacBook Pro (macOS High Sierra): I tried to build then debug the example project "periph_blinky" on OM13056: LPCXpresso™ Board for LPC1549. After probe recognition the debugging session never ends.&lt;/P&gt;&lt;P class=""&gt;At the bottom left of the window it says me “Connect to target”, the project is not loaded on the board and the led doesn’t blink. The keys "Resume","Suspend"and"Terminate"&amp;nbsp;keys are never available in the toolbar. Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jan 2018 23:07:35 GMT</pubDate>
    <dc:creator>stevemeister</dc:creator>
    <dc:date>2018-01-15T23:07:35Z</dc:date>
    <item>
      <title>Upload and run example projects on LCP1549</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726487#M1234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;Hi!&amp;nbsp; &amp;nbsp;I installed MCUXpresso IDE v10.1.1 on my MacBook Pro (macOS High Sierra): I tried to build then debug the example project "periph_blinky" on OM13056: LPCXpresso™ Board for LPC1549. After probe recognition the debugging session never ends.&lt;/P&gt;&lt;P class=""&gt;At the bottom left of the window it says me “Connect to target”, the project is not loaded on the board and the led doesn’t blink. The keys "Resume","Suspend"and"Terminate"&amp;nbsp;keys are never available in the toolbar. Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 23:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726487#M1234</guid>
      <dc:creator>stevemeister</dc:creator>
      <dc:date>2018-01-15T23:07:35Z</dc:date>
    </item>
    <item>
      <title>Re: Upload and run example projects on LCP1549</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726488#M1235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What board / debug probe are you using? Is this an LPCXpresso1549 board, and using CMSIS-DAP firmware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you provide the details from the debug log and also the redlinkserver log in the console view, as described in section 16.8, "The Console View" of the MCUXpresso IDE v10.1 User Guide .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 11:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726488#M1235</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-01-17T11:04:31Z</dc:date>
    </item>
    <item>
      <title>Re: Upload and run example projects on LCP1549</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726489#M1236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;I added new screen shots&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 14:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726489#M1236</guid>
      <dc:creator>stevemeister</dc:creator>
      <dc:date>2018-01-19T14:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: Upload and run example projects on LCP1549</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726490#M1237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Towards the end of the console log, there is a message that say 'localhost- no such host'. That implies there is a problem with your network configuration. Every system shound have&amp;nbsp;localhost set up. So I suggest that is where you start.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 21:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Upload-and-run-example-projects-on-LCP1549/m-p/726490#M1237</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2018-01-19T21:53:55Z</dc:date>
    </item>
  </channel>
</rss>