<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wire not connected on Q9080-DX LinkServer in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723703#M1193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both boards are marked as&lt;/P&gt;&lt;P&gt;QN9080 DK-V1.2&lt;/P&gt;&lt;P&gt;R20161129&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Mar 2018 17:18:01 GMT</pubDate>
    <dc:creator>rickdickerson</dc:creator>
    <dc:date>2018-03-27T17:18:01Z</dc:date>
    <item>
      <title>Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723698#M1188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a new Q9080-DX development board that I am trying to debug through the LinkServer CMSIS-DAP interface on a Windows 10 machine using MCUXpresso 10.1.1. I have successfully pushed two example projects to the board and was able to debug them, but I can't connect to the board anymore (the error message is below) for either of those projects. It stopped working while I was developing, so the IDE and development board were in the same state as the previous successful debugging session. No changes were made to the debug configuration between the last successful debugging session and the beginning of the failures. The last application I pushed into the QN9080 is still working, so that chip appears to be alive.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the LPC hardware is still working and configured properly because I still see the virtual comm port in the Windows Device Manager and the probe can be discovered by the debugger. However, when I try to debug the application I get an error stating that the wire is not connected. I have tried restarting MCUXpresso, rebooting the PC, starting a new workspace and deleting and recreating the debug configuration to no avail. The LPC driver version is 2.0.0.0, which I think is up to date.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the failure, the MCUXpresso IDE status bar says that it killed redlinkserv.exe, but I can see the process is still running in the task manager. I tried manually killing that process but it didn't help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would appreciate any help someone can provide in getting this board back up and running.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/246i16283B470F374FF0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/329iCECC6AB35C243D2C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 20:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723698#M1188</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-03-21T20:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723699#M1189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please include &lt;A _jive_internal="true" href="https://community.nxp.com/message/630852"&gt;The Debug Log&lt;/A&gt; in your response. You stated there were no debug configuration changes to blame, but the&amp;nbsp; first question I'll ask is whether your launch configuration uses the qn908xreset.scp reset script?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 21:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723699#M1189</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-21T21:38:33Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723700#M1190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used the default configuration settings and it appears that I am using the qn908xresect.scp script. Nothing is selected in the Reset Handling field though. Should&amp;nbsp;I have&amp;nbsp;something selected there?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/591i719614E29E16BD7E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The qn908cdk_wireless_examples_bluetooth_heart_rate_sensor_bm Debug messages console is empty.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Here is the RedlinkServer log:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Connected on port 3025]&lt;BR /&gt;redlink&amp;gt;ProbeList&lt;BR /&gt;Index = 1&lt;BR /&gt;Manufacturer = NXP Semiconductors&lt;BR /&gt;Description = LPC-LINK2 CMSIS-DAP V5.173&lt;BR /&gt;Serial Number = BTAVCQEQ&lt;BR /&gt;VID:PID = 1FC9:0090&lt;BR /&gt;Path = \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#7&amp;amp;618ad55&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;redlink&amp;gt;ProbeStatus&lt;BR /&gt;Index = 1&lt;BR /&gt;Manufacturer = NXP Semiconductors&lt;BR /&gt;Description = LPC-LINK2 CMSIS-DAP V5.173&lt;BR /&gt;Serial Number = BTAVCQEQ&lt;BR /&gt;VID:PID = 1FC9:0090&lt;BR /&gt;Path = \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#7&amp;amp;618ad55&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;IsOpen = FALSE&lt;BR /&gt;WireInitialized = FALSE&lt;BR /&gt;WireProtocol = JTAG&lt;BR /&gt;CoresConfigured = FALSE&lt;BR /&gt;PacketSize = 1024&lt;BR /&gt;Reference Count = 0&lt;BR /&gt;HasSWV = FALSE&lt;BR /&gt;HasETM = FALSE&lt;BR /&gt;HasJTAG = TRUE&lt;BR /&gt;HasSWD = TRUE&lt;BR /&gt;Probe Type = CMSIS-DAP&lt;BR /&gt;Probe Reference Count = 0&lt;BR /&gt;redlink&amp;gt;ProbeIsOpen 1&lt;BR /&gt;FALSE&lt;BR /&gt;redlink&amp;gt;ProbeOpenByIndex 1 &lt;BR /&gt;Probe Handle 1 Open&lt;BR /&gt;redlink&amp;gt;WireIsConnected 1&lt;BR /&gt;FALSE&lt;BR /&gt;redlink&amp;gt;WireSwdConnect 1&lt;BR /&gt;Wire Ack Fault - target connected?&lt;BR /&gt;redlink&amp;gt;CoresConfigured 1&lt;BR /&gt;FALSE&lt;BR /&gt;redlink&amp;gt;CoreConfig 1&lt;BR /&gt;Wire not connected&lt;BR /&gt;[Closed]&lt;BR /&gt;[Started server]&lt;BR /&gt;[Connected on port 3025]&lt;BR /&gt;redlink&amp;gt;ProbeStatus&lt;BR /&gt;redlink&amp;gt;quit&lt;BR /&gt;[Closed]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;This is the arm-none-eabi-gdb console log&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;GNU gdb (GNU Tools for ARM Embedded Processors 6-2017-q2-update) 7.12.1.20170417-git&lt;BR /&gt;Copyright (C) 2017 Free Software Foundation, Inc.&lt;BR /&gt;&lt;SPAN&gt;License GPLv3+: GNU GPL version 3 or later &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fgnu.org%2Flicenses%2Fgpl.html" rel="nofollow" target="_blank"&gt;http://gnu.org/licenses/gpl.html&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;This is free software: you are free to change and redistribute it.&lt;BR /&gt;There is NO WARRANTY, to the extent permitted by law. Type "show copying"&lt;BR /&gt;and "show warranty" for details.&lt;BR /&gt;This GDB was configured as "--host=i686-w64-mingw32 --target=arm-none-eabi".&lt;BR /&gt;Type "show configuration" for configuration details.&lt;BR /&gt;For bug reporting instructions, please see:&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.gnu.org%2Fsoftware%2Fgdb%2Fbugs%2F" rel="nofollow" target="_blank"&gt;http://www.gnu.org/software/gdb/bugs/&lt;/A&gt;&lt;SPAN&gt;&amp;gt;.&lt;/SPAN&gt;&lt;BR /&gt;Find the GDB manual and other documentation resources online at:&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.gnu.org%2Fsoftware%2Fgdb%2Fdocumentation%2F" rel="nofollow" target="_blank"&gt;http://www.gnu.org/software/gdb/documentation/&lt;/A&gt;&lt;SPAN&gt;&amp;gt;.&lt;/SPAN&gt;&lt;BR /&gt;For help, type "help".&lt;BR /&gt;Type "apropos word" to search for commands related to "word".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;This is the gdb traces console log&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;862,535 2-list-thread-groups&lt;BR /&gt;862,551 2^done,groups=[{id="i1",type="process"}]&lt;BR /&gt;862,551 (gdb) &lt;BR /&gt;865,160 3-gdb-version&lt;BR /&gt;865,175 ~"GNU gdb (GNU Tools for ARM Embedded Processors 6-2017-q2-update) 7.12.1.20170417-git\n"&lt;BR /&gt;865,175 ~"Copyright (C) 2017 Free Software Foundation, Inc.\n"&lt;BR /&gt;&lt;SPAN&gt;865,175 ~"License GPLv3+: GNU GPL version 3 or later &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fgnu.org%2Flicenses%2Fgpl.html" rel="nofollow" target="_blank"&gt;http://gnu.org/licenses/gpl.html&lt;/A&gt;&lt;SPAN&gt;&amp;gt;\nThis is fre\&lt;/SPAN&gt;&lt;BR /&gt;e software: you are free to change and redistribute it.\nThere is NO WARRANTY, to the extent permitt\&lt;BR /&gt;ed by law. Type \"show copying\"\nand \"show warranty\" for details.\n"&lt;BR /&gt;865,175 ~"This GDB was configured as \"--host=i686-w64-mingw32 --target=arm-none-eabi\".\nType \"sho\&lt;BR /&gt;w configuration\" for configuration details."&lt;BR /&gt;865,175 ~"\nFor bug reporting instructions, please see:\n"&lt;BR /&gt;&lt;SPAN&gt;865,175 ~"&amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.gnu.org%2Fsoftware%2Fgdb%2Fbugs%2F" rel="nofollow" target="_blank"&gt;http://www.gnu.org/software/gdb/bugs/&lt;/A&gt;&lt;SPAN&gt;&amp;gt;.\n"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;865,175 ~"Find the GDB manual and other documentation resources online at:\n&amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.gnu.org%2Fsoft" rel="nofollow" target="_blank"&gt;http://www.gnu.org/soft&lt;/A&gt;&lt;SPAN&gt;\&lt;/SPAN&gt;&lt;BR /&gt;ware/gdb/documentation/&amp;gt;.\n"&lt;BR /&gt;865,175 ~"For help, type \"help\".\n"&lt;BR /&gt;865,175 ~"Type \"apropos word\" to search for commands related to \"word\".\n"&lt;BR /&gt;865,175 3^done&lt;BR /&gt;865,175 (gdb) &lt;BR /&gt;865,191 4-environment-cd C:/Users/rdickerson/mcuxpresso/01/SDKPackages/SDK_2.2_QN908XCDK/boards/qn90\&lt;BR /&gt;8xcdk/wireless_examples/bluetooth/ble_relay_proxy_rickd/qn908xcdk_wireless_examples_bluetooth_heart_\&lt;BR /&gt;rate_sensor_bm&lt;BR /&gt;865,239 4^done&lt;BR /&gt;865,239 (gdb) &lt;BR /&gt;865,239 5-gdb-set breakpoint pending on&lt;BR /&gt;865,254 5^done&lt;BR /&gt;865,254 (gdb) &lt;BR /&gt;865,254 6-enable-pretty-printing&lt;BR /&gt;865,270 6^done&lt;BR /&gt;865,270 (gdb) &lt;BR /&gt;865,270 7-gdb-set python print-stack none&lt;BR /&gt;865,271 7^done&lt;BR /&gt;865,271 (gdb) &lt;BR /&gt;865,271 8-gdb-set print object on&lt;BR /&gt;865,286 8^done&lt;BR /&gt;865,286 (gdb) &lt;BR /&gt;865,302 9-gdb-set print sevenbit-strings on&lt;BR /&gt;865,318 9^done&lt;BR /&gt;865,318 (gdb) &lt;BR /&gt;865,318 10-gdb-set charset ISO-8859-1&lt;BR /&gt;865,333 10^done&lt;BR /&gt;865,333 (gdb) &lt;BR /&gt;865,333 11-gdb-set auto-solib-add on&lt;BR /&gt;865,349 11^done&lt;BR /&gt;865,349 (gdb) &lt;BR /&gt;865,349 12-file-exec-and-symbols --thread-group i1 C:/Users/rdickerson/mcuxpresso/01/SDKPackages/SDK\&lt;BR /&gt;_2.2_QN908XCDK/boards/qn908xcdk/wireless_examples/bluetooth/ble_relay_proxy_rickd/qn908xcdk_wireless\&lt;BR /&gt;_examples_bluetooth_heart_rate_sensor_bm/Debug/qn908xcdk_wireless_examples_bluetooth_heart_rate_sens\&lt;BR /&gt;or_bm.axf&lt;BR /&gt;865,380 12^done&lt;BR /&gt;865,380 (gdb) &lt;BR /&gt;865,380 13-interpreter-exec console "set remotetimeout 60000"&lt;BR /&gt;865,396 =cmd-param-changed,param="remotetimeout",value="60000"&lt;BR /&gt;865,396 13^done&lt;BR /&gt;865,396 (gdb) &lt;BR /&gt;867,060 14-target-disconnect&lt;BR /&gt;867,060 15-gdb-exit&lt;BR /&gt;867,075 14^error,msg="You can't do that when your target is `exec'"&lt;BR /&gt;867,075 (gdb) &lt;BR /&gt;867,075 15^exit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Mar 2018 13:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723700#M1190</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-03-22T13:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723701#M1191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you provide any insight into this issue? I suspected the development board may be defective so I purchased another one. I got the Windows message about installing new drivers when I plugged in the new board. I let that process finish and was able to successfully install the heart rate example into the new board. I plugged in the old board to see if the driver update had any effect, but still had the same problems. I then went back to the new development board and could no longer connect to it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A coworker downloaded the QN9080 SDK and has tried both boards with the same failures that I have been seeing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to get the LPC4322 hung up so it won't communicate with the PC? Cycling power on the development board and/or the PC doesn't do any good.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 16:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723701#M1191</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-03-27T16:28:43Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723702#M1192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What version board(s) do you have?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 17:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723702#M1192</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-27T17:13:37Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723703#M1193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both boards are marked as&lt;/P&gt;&lt;P&gt;QN9080 DK-V1.2&lt;/P&gt;&lt;P&gt;R20161129&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 17:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723703#M1193</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-03-27T17:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723704#M1194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible that the heart rate example could be the culprit? On my first board, I successfully downloaded the ble relay proxy example and then the heart rate example. I could not download anything else after that. The heart rate example was the first thing I downloaded to the second development board and I haven't been able to&amp;nbsp;download&amp;nbsp;anything else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My SDK version is 2.2.0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 17:28:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723704#M1194</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-03-27T17:28:57Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723705#M1195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm&amp;nbsp; not certain. Place a jumper on JP15, and reset the board, or power it on/off. This will boot the part into the ISP and will not allow the flashed image to execute. Then, erase flash using the flash utility and flash another example. I've located a QN9080 v1.1 board to test with, but I'd prefer to use the same revision as yourself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 17:44:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723705#M1195</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-27T17:44:31Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723706#M1196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That fixed it!! After following your instructions I have been able to load several example programs into the development board. Thanks!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 18:50:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723706#M1196</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-03-27T18:50:19Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723707#M1197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do see a problem with MCUXpresso terminating the debug session when attempting a Restart. We'll investigate a fix for a future release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 19:01:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723707#M1197</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-27T19:01:13Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723708#M1198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; border: 0px;"&gt;One other minor aside - I notice that your board appears to have old LPC-Link2 probe firmware pre-programmed into it (v5.173). I would suggest that you either remove the header on JP5 (DFUlink) to allow the IDE to softload the current version (v5.18x) or use LPCScrypt to program the current version into flash (see&lt;A _jive_internal="true" class="" data-containerid="11529" data-containertype="14" data-objectid="389045" data-objecttype="1" href="https://community.nxp.com/thread/389045" style="color: #5e89c1; background-color: transparent; border: 0px; font-weight: inherit; padding: 1px 0px 1px calc(12px + 0.35ex);"&gt;LPC-Link2 Debug Probe firmware programming&lt;/A&gt;&amp;nbsp;for more details).&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;Regards,&lt;/P&gt;&lt;P style="color: #51626f; border: 0px;"&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2018 10:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723708#M1198</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-03-28T10:02:43Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723709#M1199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the tip. I upgraded my probe.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 15:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723709#M1199</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-03-29T15:30:31Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723710#M1200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Rick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Heart rate project has enabled low power feature by define&amp;nbsp;cPWR_UsePowerDownMode 1. So the chip will go to Power down state and you can't get connected to an external debugger.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2018 01:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723710#M1200</guid>
      <dc:creator>neoxiong</dc:creator>
      <dc:date>2018-04-02T01:26:56Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723711#M1201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The chip was still&amp;nbsp;advertising BLE&amp;nbsp;and I was able to connect to it with the IoT Toolbox app when I couldn't connect with a debugger. Wouldn't that indicate that the chip wasn't in a low power state?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2018 12:08:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723711#M1201</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-04-02T12:08:50Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723712#M1202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Rick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Between advertising event and connection event, the chip goes to Power Down 0. No clock to support debugger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 06:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723712#M1202</guid>
      <dc:creator>neoxiong</dc:creator>
      <dc:date>2018-04-03T06:09:42Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723713#M1203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That makes perfect sense. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 11:42:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723713#M1203</guid>
      <dc:creator>rickdickerson</dc:creator>
      <dc:date>2018-04-03T11:42:31Z</dc:date>
    </item>
    <item>
      <title>Re: Wire not connected on Q9080-DX LinkServer</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723714#M1204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So if we are developing an Bluetooth application for qn908x, would we always have to reset the board by jumping JP15?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Aug 2018 00:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Wire-not-connected-on-Q9080-DX-LinkServer/m-p/723714#M1204</guid>
      <dc:creator>jlee642</dc:creator>
      <dc:date>2018-08-18T00:42:12Z</dc:date>
    </item>
  </channel>
</rss>