<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: program flashing error</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/program-flashing-error/m-p/717184#M1075</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you plug the debug probe into your computer, what do you see in "Devices and Printers" (assuming you are running on Windows).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Two possibilities...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) You might need to install the mbed serial port driver. There is a link to this in the IDE's &lt;STRONG&gt;&lt;EM&gt;Help -&amp;gt; Additional Resources&lt;/EM&gt;&lt;/STRONG&gt; menu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) For some reason, your board&amp;nbsp;doesn't actually have debug probe firmware programmed into the probe at all. In which can install the latest version yourself.&amp;nbsp;[You might want to do this even if installing the mbed serial port driver worked, as the older firmware is noticeably slower than the latest&amp;nbsp;version.]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest probe firmware for the LPCXpresso-CD boards can be referenced via:&amp;nbsp;&lt;A href="https://community.nxp.com/migration-blogpost/10876"&gt;New debug probe firmware &amp;amp;amp; drivers for MAX boards&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you might also want to read through this ticket :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/471323"&gt;LPCXpresso LPC1769 (OM13085) Can't find debug Probe&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Apr 2018 07:48:42 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2018-04-10T07:48:42Z</dc:date>
    <item>
      <title>program flashing error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/program-flashing-error/m-p/717183#M1074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using LPC1769 CMSIS-DAP rev D1 board with MCUxpresso software v10.1.0. buitl program successfully but when i am trying to flash program on board it gives me error like "&amp;nbsp;No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target". How can I solve this Error. Please reply&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 06:51:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/program-flashing-error/m-p/717183#M1074</guid>
      <dc:creator>ishwarbhoge</dc:creator>
      <dc:date>2018-04-10T06:51:25Z</dc:date>
    </item>
    <item>
      <title>Re: program flashing error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/program-flashing-error/m-p/717184#M1075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you plug the debug probe into your computer, what do you see in "Devices and Printers" (assuming you are running on Windows).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Two possibilities...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) You might need to install the mbed serial port driver. There is a link to this in the IDE's &lt;STRONG&gt;&lt;EM&gt;Help -&amp;gt; Additional Resources&lt;/EM&gt;&lt;/STRONG&gt; menu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) For some reason, your board&amp;nbsp;doesn't actually have debug probe firmware programmed into the probe at all. In which can install the latest version yourself.&amp;nbsp;[You might want to do this even if installing the mbed serial port driver worked, as the older firmware is noticeably slower than the latest&amp;nbsp;version.]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest probe firmware for the LPCXpresso-CD boards can be referenced via:&amp;nbsp;&lt;A href="https://community.nxp.com/migration-blogpost/10876"&gt;New debug probe firmware &amp;amp;amp; drivers for MAX boards&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you might also want to read through this ticket :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/471323"&gt;LPCXpresso LPC1769 (OM13085) Can't find debug Probe&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 07:48:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/program-flashing-error/m-p/717184#M1075</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-04-10T07:48:42Z</dc:date>
    </item>
  </channel>
</rss>