<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Add a library</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2398361#M10735</link>
    <description>&lt;P&gt;This is part of my problem. The file does not have any extension - it is simply "IRemote-4.7.1" and is represented in my downloads as a folder. &amp;nbsp;I don't think I am using an older version of the SDK, it is version 26.06.00. Could it be that I have not loaded the actual IRemote library - I just pressed the DOWNLOAD button&lt;/P&gt;</description>
    <pubDate>Thu, 23 Jul 2026 14:07:45 GMT</pubDate>
    <dc:creator>Julian99</dc:creator>
    <dc:date>2026-07-23T14:07:45Z</dc:date>
    <item>
      <title>Add a library</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2397808#M10733</link>
      <description>&lt;P&gt;I have just migrated from CodeWarrior and also have just installed MCUX on my new iMAC. I am working on a new project that includes &amp;nbsp;IR remote control and I would like to use the IRemote library (from GitHub). &amp;nbsp;I have downloaded the library file But I cannot add it to SDK_2.x_LPCXpresso824MAX (which is the development board I am using). I followed the instructions in the document "How to create and use a static library", but the instructions and screen shots appear to be from a much earlier version than mine.&lt;/P&gt;&lt;P&gt;Does anyone have an "idiot guide" that will solve my problem?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jul 2026 12:18:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2397808#M10733</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2026-07-22T12:18:23Z</dc:date>
    </item>
    <item>
      <title>Re: Add a library</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2397911#M10734</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;What type of file do you have for the library? The .a extension or .h?&lt;/P&gt;
&lt;P&gt;The steps mentioned in Chapter 2 "adding user static library in user application" Page 5 from &lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE-Knowledge-Base/How-to-create-and-use-static-library-in-MCUXpresso-IDE/ta-p/1112789?attachment-id=77172" target="_blank"&gt;How to create and use static library in MCUXpresso IDE&lt;/A&gt; still apply for newer version of MCUXpresso IDE, the windows shown in the guide are the same in recent version of MCUXpresso. Do you have an issue with a step?&lt;/P&gt;
&lt;P&gt;Also could you help confirm which version are you using?&lt;/P&gt;
&lt;P&gt;For the SDK; I see you wrote "SDK_2.x_" could you confirm which older version are you using? You could update to use the recent SDK version 26.06, you can download it from &lt;A href="https://mcuxpresso.nxp.com/select" target="_blank"&gt;SDK Builder&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jul 2026 21:14:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2397911#M10734</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-07-22T21:14:16Z</dc:date>
    </item>
    <item>
      <title>Re: Add a library</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2398361#M10735</link>
      <description>&lt;P&gt;This is part of my problem. The file does not have any extension - it is simply "IRemote-4.7.1" and is represented in my downloads as a folder. &amp;nbsp;I don't think I am using an older version of the SDK, it is version 26.06.00. Could it be that I have not loaded the actual IRemote library - I just pressed the DOWNLOAD button&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jul 2026 14:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2398361#M10735</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2026-07-23T14:07:45Z</dc:date>
    </item>
    <item>
      <title>Re: Add a library</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2398415#M10736</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;You probably download the whole Github folders for the library, usually Github users save the .h/.c/.hpp/.cpp etc in the src folder.&lt;/P&gt;
&lt;P&gt;You could download only the necessary .h/.a files from src folder or search for them in the Github instead of download the whole Github project, and follow the guide to add library and path to linker.&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jul 2026 17:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Add-a-library/m-p/2398415#M10736</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-07-23T17:00:09Z</dc:date>
    </item>
  </channel>
</rss>