<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Power level adc mcxa153</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Power-level-adc-mcxa153/m-p/2324474#M10649</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240937"&gt;@Transidico&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This window configures the power level at which the ADC will operate, as described in its description. In the case of the MCXA153, the ADC supports two power modes, Low Power Mode and High Power Mode. Each of which requires specific configurations (such as clock source selection, register bit settings, etc.). For more details, refer to section 40.3.1 “Power Control Mode” in the RM.&lt;BR /&gt;Additionally, I highly recommend reviewing the &lt;A href="https://docs.nxp.com/bundle/AN14390/page/topics/introduction.html" target="_self"&gt;AN14390&lt;/A&gt;, which provides a detailed explanation of the ADC peripheral and can be very helpful for understanding its operation.&lt;BR /&gt;&lt;BR /&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
    <pubDate>Fri, 27 Feb 2026 17:46:36 GMT</pubDate>
    <dc:creator>Habib_MS</dc:creator>
    <dc:date>2026-02-27T17:46:36Z</dc:date>
    <item>
      <title>Power level adc mcxa153</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Power-level-adc-mcxa153/m-p/2323871#M10645</link>
      <description>&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I am setting up the ADC on the MCXA153 board and would like to know what the various configurable power level modes in the peripherals mean. Where can I find them? What do they mean?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2026-02-26 165444.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377920i8DAA42027550AE94/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2026-02-26 165444.png" alt="Screenshot 2026-02-26 165444.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Feb 2026 15:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Power-level-adc-mcxa153/m-p/2323871#M10645</guid>
      <dc:creator>Transidico</dc:creator>
      <dc:date>2026-02-26T15:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: Power level adc mcxa153</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Power-level-adc-mcxa153/m-p/2324474#M10649</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240937"&gt;@Transidico&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This window configures the power level at which the ADC will operate, as described in its description. In the case of the MCXA153, the ADC supports two power modes, Low Power Mode and High Power Mode. Each of which requires specific configurations (such as clock source selection, register bit settings, etc.). For more details, refer to section 40.3.1 “Power Control Mode” in the RM.&lt;BR /&gt;Additionally, I highly recommend reviewing the &lt;A href="https://docs.nxp.com/bundle/AN14390/page/topics/introduction.html" target="_self"&gt;AN14390&lt;/A&gt;, which provides a detailed explanation of the ADC peripheral and can be very helpful for understanding its operation.&lt;BR /&gt;&lt;BR /&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
      <pubDate>Fri, 27 Feb 2026 17:46:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Power-level-adc-mcxa153/m-p/2324474#M10649</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2026-02-27T17:46:36Z</dc:date>
    </item>
  </channel>
</rss>