<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: Ethernet Communication</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2088907#M10357</link>
    <description>helle &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239163"&gt;@mayliu1&lt;/a&gt;&lt;BR /&gt;Thanks for replay&lt;BR /&gt;&lt;BR /&gt;Based on the example, I tried, but I am unable to receive and transmit the frame.&lt;BR /&gt;&lt;BR /&gt;I modified the code to create a simpler version. using evkbmimxrt1170_enet_txrx_transfer_cm7 example code please guide me what will be need to change. i am attech project file.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;#include "fsl_debug_console.h"&lt;BR /&gt;&lt;BR /&gt;#include "fsl_silicon_id.h"&lt;BR /&gt;&lt;BR /&gt;#include "fsl_enet.h"&lt;BR /&gt;&lt;BR /&gt;#include "fsl_phy.h"&lt;BR /&gt;&lt;BR /&gt;#include "board.h"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;#include "fsl_phyrtl8201.h"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;#include "fsl_enet.h"&lt;BR /&gt;&lt;BR /&gt;#include "board.h"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;#define EXAMPLE_ENET ENET&lt;BR /&gt;&lt;BR /&gt;#define EXAMPLE_CLOCK_FREQ CLOCK_GetRootClockFreq(kCLOCK_Root_Bus)&lt;BR /&gt;&lt;BR /&gt;#define ENET_RXBD_NUM 4&lt;BR /&gt;&lt;BR /&gt;#define ENET_TXBD_NUM 4&lt;BR /&gt;&lt;BR /&gt;#define ENET_RXBUFF_SIZE ENET_FRAME_MAX_FRAMELEN&lt;BR /&gt;&lt;BR /&gt;#define ENET_TXBUFF_SIZE ENET_FRAME_MAX_FRAMELEN&lt;BR /&gt;&lt;BR /&gt;#define ENET_DATA_LENGTH 1000&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Buffer descriptors */&lt;BR /&gt;&lt;BR /&gt;AT_NONCACHEABLE_SECTION_ALIGN(enet_rx_bd_struct_t g_rxBuffDescrip[ENET_RXBD_NUM], ENET_BUFF_ALIGNMENT);&lt;BR /&gt;&lt;BR /&gt;AT_NONCACHEABLE_SECTION_ALIGN(enet_tx_bd_struct_t g_txBuffDescrip[ENET_TXBD_NUM], ENET_BUFF_ALIGNMENT);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Data buffers */&lt;BR /&gt;&lt;BR /&gt;SDK_ALIGN(uint8_t g_rxDataBuff[ENET_RXBD_NUM][ENET_RXBUFF_SIZE], ENET_BUFF_ALIGNMENT);&lt;BR /&gt;&lt;BR /&gt;SDK_ALIGN(uint8_t g_txDataBuff[ENET_TXBD_NUM][ENET_TXBUFF_SIZE], ENET_BUFF_ALIGNMENT);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* MAC address */&lt;BR /&gt;&lt;BR /&gt;uint8_t g_macAddr[6] =&lt;BR /&gt;&lt;BR /&gt;{ 0x02, 0x12, 0x13, 0x14, 0x15, 0x16 };&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* ENET handle */&lt;BR /&gt;&lt;BR /&gt;static enet_handle_t g_handle;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;static void BuildTestFrame(uint8_t *frame)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;/* Destination MAC (broadcast) */&lt;BR /&gt;&lt;BR /&gt;for (int i = 0; i &amp;lt; 6; i++)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;frame[i] = 0xFF;&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Source MAC */&lt;BR /&gt;&lt;BR /&gt;memcpy(&amp;amp;frame[6], g_macAddr, 6);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* EtherType/Length */&lt;BR /&gt;&lt;BR /&gt;frame[12] = 0x08; // IPv4&lt;BR /&gt;&lt;BR /&gt;frame[13] = 0x00;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Simple payload */&lt;BR /&gt;&lt;BR /&gt;for (int i = 14; i &amp;lt; ENET_DATA_LENGTH; i++)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;frame[i] = i % 256;&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;void InitEthernet(void)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;enet_config_t config;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Prepare buffer configuration */&lt;BR /&gt;&lt;BR /&gt;enet_buffer_config_t buffConfig =&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;ENET_RXBD_NUM,&lt;BR /&gt;&lt;BR /&gt;ENET_TXBD_NUM,&lt;BR /&gt;&lt;BR /&gt;ENET_RXBUFF_SIZE,&lt;BR /&gt;&lt;BR /&gt;ENET_TXBUFF_SIZE, g_rxBuffDescrip, g_txBuffDescrip, &amp;amp;g_rxDataBuff[0][0], &amp;amp;g_txDataBuff[0][0],&lt;BR /&gt;&lt;BR /&gt;true,&lt;BR /&gt;&lt;BR /&gt;true,&lt;BR /&gt;&lt;BR /&gt;NULL };&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Get default ENET configuration */&lt;BR /&gt;&lt;BR /&gt;ENET_GetDefaultConfig(&amp;amp;config);&lt;BR /&gt;&lt;BR /&gt;config.miiMode = kENET_RmiiMode;&lt;BR /&gt;&lt;BR /&gt;config.miiSpeed = kENET_MiiSpeed100M;&lt;BR /&gt;&lt;BR /&gt;config.miiDuplex = kENET_MiiFullDuplex;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Initialize ENET */&lt;BR /&gt;&lt;BR /&gt;ENET_Init(EXAMPLE_ENET, &amp;amp;g_handle, &amp;amp;config, &amp;amp;buffConfig, g_macAddr, EXAMPLE_CLOCK_FREQ);&lt;BR /&gt;&lt;BR /&gt;ENET_ActiveRead(EXAMPLE_ENET);&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;int main(void)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;uint8_t txFrame[ENET_DATA_LENGTH];&lt;BR /&gt;&lt;BR /&gt;uint8_t rxBuffer[ENET_RXBUFF_SIZE];&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Initialize hardware */&lt;BR /&gt;&lt;BR /&gt;BOARD_InitHardware();&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Initialize Ethernet */&lt;BR /&gt;&lt;BR /&gt;InitEthernet();&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Build test frame */&lt;BR /&gt;&lt;BR /&gt;BuildTestFrame(txFrame);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;while (1)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;uint32_t frameLength = 0;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Check for received frames */&lt;BR /&gt;&lt;BR /&gt;if (ENET_GetRxFrameSize(&amp;amp;g_handle, &amp;amp;frameLength, 0) == kStatus_Success)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;if (frameLength &amp;gt; 0)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;/* Read the frame */&lt;BR /&gt;&lt;BR /&gt;if (ENET_ReadFrame(EXAMPLE_ENET, &amp;amp;g_handle, rxBuffer, frameLength, 0, NULL) == kStatus_Success)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;/* Process received frame here */&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Send test frame */&lt;BR /&gt;&lt;BR /&gt;status_t ENET_SendFrame(ENET_Type *base, enet_handle_t *handle, const uint8_t *data, uint32_t length, uint8_t ringId,&lt;BR /&gt;&lt;BR /&gt;bool tsFlag, void *context);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;ENET_SendFrame(EXAMPLE_ENET, &amp;amp;g_handle, txFrame, ENET_DATA_LENGTH, 0, false, NULL);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Small delay */&lt;BR /&gt;&lt;BR /&gt;for (volatile int i = 0; i &amp;lt; 1000000; i++);&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;in that i am getting also error undefined reference to `PHY_LinkStatusChange'&lt;BR /&gt;</description>
    <pubDate>Tue, 29 Apr 2025 04:43:23 GMT</pubDate>
    <dc:creator>Govind89</dc:creator>
    <dc:date>2025-04-29T04:43:23Z</dc:date>
    <item>
      <title>Ethernet Communication</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2088184#M10351</link>
      <description>&lt;P class=""&gt;I am new to i.MX RT1170 development and using the EVKBMIMXRT1170 board. I'm working with the built-in example code&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;evkbmimxrt1170_enet_txrx_transfer_cm7&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;for Ethernet functionality, but I'm finding it difficult to understand how it works.&lt;/P&gt;&lt;P class=""&gt;I would like to request a simpler, bare-metal code example that focuses just on basic Ethernet operations:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;Ethernet configuration&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Ethernet initialization&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Ethernet frame transmission&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Ethernet frame reception&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;I need this in API-style simple code without RTOS, using MCUXpresso IDE. Please provide guidance and the simplest base code for Ethernet functionality on my EVKBMIMXRT1170 development board.&lt;BR /&gt;&lt;LI-PRODUCT title="i.MX-RT1170" id="i.MX-RT1170"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="MCUXpresso-IDE" id="MCUXpresso-IDE"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Apr 2025 08:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2088184#M10351</guid>
      <dc:creator>Govind89</dc:creator>
      <dc:date>2025-04-28T08:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Communication</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2088894#M10356</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234971"&gt;@Govind89&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;I think the project you imported is already without FREERTOS, if you want more&amp;nbsp;&lt;SPAN&gt;Ethernet&amp;nbsp;demo, you can check by import&amp;nbsp; SDK example.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mayliu1_0-1745898661549.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335405iEC4F586E1607CB8E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mayliu1_0-1745898661549.png" alt="mayliu1_0-1745898661549.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you want know more about the SDK API. you can refer to the document "MCUXpresso SDK API Reference Manual"&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/api_doc/dev/329/index.html" target="_blank"&gt;https://mcuxpresso.nxp.com/api_doc/dev/329/index.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Wish it helps you.&lt;BR /&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Wish you a nice day!&lt;/P&gt;
&lt;P&gt;Best Regards&lt;BR /&gt;MayLiu&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 04:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2088894#M10356</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-04-29T04:08:24Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Communication</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2088907#M10357</link>
      <description>helle &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239163"&gt;@mayliu1&lt;/a&gt;&lt;BR /&gt;Thanks for replay&lt;BR /&gt;&lt;BR /&gt;Based on the example, I tried, but I am unable to receive and transmit the frame.&lt;BR /&gt;&lt;BR /&gt;I modified the code to create a simpler version. using evkbmimxrt1170_enet_txrx_transfer_cm7 example code please guide me what will be need to change. i am attech project file.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;#include "fsl_debug_console.h"&lt;BR /&gt;&lt;BR /&gt;#include "fsl_silicon_id.h"&lt;BR /&gt;&lt;BR /&gt;#include "fsl_enet.h"&lt;BR /&gt;&lt;BR /&gt;#include "fsl_phy.h"&lt;BR /&gt;&lt;BR /&gt;#include "board.h"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;#include "fsl_phyrtl8201.h"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;#include "fsl_enet.h"&lt;BR /&gt;&lt;BR /&gt;#include "board.h"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;#define EXAMPLE_ENET ENET&lt;BR /&gt;&lt;BR /&gt;#define EXAMPLE_CLOCK_FREQ CLOCK_GetRootClockFreq(kCLOCK_Root_Bus)&lt;BR /&gt;&lt;BR /&gt;#define ENET_RXBD_NUM 4&lt;BR /&gt;&lt;BR /&gt;#define ENET_TXBD_NUM 4&lt;BR /&gt;&lt;BR /&gt;#define ENET_RXBUFF_SIZE ENET_FRAME_MAX_FRAMELEN&lt;BR /&gt;&lt;BR /&gt;#define ENET_TXBUFF_SIZE ENET_FRAME_MAX_FRAMELEN&lt;BR /&gt;&lt;BR /&gt;#define ENET_DATA_LENGTH 1000&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Buffer descriptors */&lt;BR /&gt;&lt;BR /&gt;AT_NONCACHEABLE_SECTION_ALIGN(enet_rx_bd_struct_t g_rxBuffDescrip[ENET_RXBD_NUM], ENET_BUFF_ALIGNMENT);&lt;BR /&gt;&lt;BR /&gt;AT_NONCACHEABLE_SECTION_ALIGN(enet_tx_bd_struct_t g_txBuffDescrip[ENET_TXBD_NUM], ENET_BUFF_ALIGNMENT);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Data buffers */&lt;BR /&gt;&lt;BR /&gt;SDK_ALIGN(uint8_t g_rxDataBuff[ENET_RXBD_NUM][ENET_RXBUFF_SIZE], ENET_BUFF_ALIGNMENT);&lt;BR /&gt;&lt;BR /&gt;SDK_ALIGN(uint8_t g_txDataBuff[ENET_TXBD_NUM][ENET_TXBUFF_SIZE], ENET_BUFF_ALIGNMENT);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* MAC address */&lt;BR /&gt;&lt;BR /&gt;uint8_t g_macAddr[6] =&lt;BR /&gt;&lt;BR /&gt;{ 0x02, 0x12, 0x13, 0x14, 0x15, 0x16 };&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* ENET handle */&lt;BR /&gt;&lt;BR /&gt;static enet_handle_t g_handle;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;static void BuildTestFrame(uint8_t *frame)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;/* Destination MAC (broadcast) */&lt;BR /&gt;&lt;BR /&gt;for (int i = 0; i &amp;lt; 6; i++)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;frame[i] = 0xFF;&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Source MAC */&lt;BR /&gt;&lt;BR /&gt;memcpy(&amp;amp;frame[6], g_macAddr, 6);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* EtherType/Length */&lt;BR /&gt;&lt;BR /&gt;frame[12] = 0x08; // IPv4&lt;BR /&gt;&lt;BR /&gt;frame[13] = 0x00;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Simple payload */&lt;BR /&gt;&lt;BR /&gt;for (int i = 14; i &amp;lt; ENET_DATA_LENGTH; i++)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;frame[i] = i % 256;&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;void InitEthernet(void)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;enet_config_t config;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Prepare buffer configuration */&lt;BR /&gt;&lt;BR /&gt;enet_buffer_config_t buffConfig =&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;ENET_RXBD_NUM,&lt;BR /&gt;&lt;BR /&gt;ENET_TXBD_NUM,&lt;BR /&gt;&lt;BR /&gt;ENET_RXBUFF_SIZE,&lt;BR /&gt;&lt;BR /&gt;ENET_TXBUFF_SIZE, g_rxBuffDescrip, g_txBuffDescrip, &amp;amp;g_rxDataBuff[0][0], &amp;amp;g_txDataBuff[0][0],&lt;BR /&gt;&lt;BR /&gt;true,&lt;BR /&gt;&lt;BR /&gt;true,&lt;BR /&gt;&lt;BR /&gt;NULL };&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Get default ENET configuration */&lt;BR /&gt;&lt;BR /&gt;ENET_GetDefaultConfig(&amp;amp;config);&lt;BR /&gt;&lt;BR /&gt;config.miiMode = kENET_RmiiMode;&lt;BR /&gt;&lt;BR /&gt;config.miiSpeed = kENET_MiiSpeed100M;&lt;BR /&gt;&lt;BR /&gt;config.miiDuplex = kENET_MiiFullDuplex;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Initialize ENET */&lt;BR /&gt;&lt;BR /&gt;ENET_Init(EXAMPLE_ENET, &amp;amp;g_handle, &amp;amp;config, &amp;amp;buffConfig, g_macAddr, EXAMPLE_CLOCK_FREQ);&lt;BR /&gt;&lt;BR /&gt;ENET_ActiveRead(EXAMPLE_ENET);&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;int main(void)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;uint8_t txFrame[ENET_DATA_LENGTH];&lt;BR /&gt;&lt;BR /&gt;uint8_t rxBuffer[ENET_RXBUFF_SIZE];&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Initialize hardware */&lt;BR /&gt;&lt;BR /&gt;BOARD_InitHardware();&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Initialize Ethernet */&lt;BR /&gt;&lt;BR /&gt;InitEthernet();&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Build test frame */&lt;BR /&gt;&lt;BR /&gt;BuildTestFrame(txFrame);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;while (1)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;uint32_t frameLength = 0;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Check for received frames */&lt;BR /&gt;&lt;BR /&gt;if (ENET_GetRxFrameSize(&amp;amp;g_handle, &amp;amp;frameLength, 0) == kStatus_Success)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;if (frameLength &amp;gt; 0)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;/* Read the frame */&lt;BR /&gt;&lt;BR /&gt;if (ENET_ReadFrame(EXAMPLE_ENET, &amp;amp;g_handle, rxBuffer, frameLength, 0, NULL) == kStatus_Success)&lt;BR /&gt;&lt;BR /&gt;{&lt;BR /&gt;&lt;BR /&gt;/* Process received frame here */&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Send test frame */&lt;BR /&gt;&lt;BR /&gt;status_t ENET_SendFrame(ENET_Type *base, enet_handle_t *handle, const uint8_t *data, uint32_t length, uint8_t ringId,&lt;BR /&gt;&lt;BR /&gt;bool tsFlag, void *context);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;ENET_SendFrame(EXAMPLE_ENET, &amp;amp;g_handle, txFrame, ENET_DATA_LENGTH, 0, false, NULL);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;/* Small delay */&lt;BR /&gt;&lt;BR /&gt;for (volatile int i = 0; i &amp;lt; 1000000; i++);&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;in that i am getting also error undefined reference to `PHY_LinkStatusChange'&lt;BR /&gt;</description>
      <pubDate>Tue, 29 Apr 2025 04:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2088907#M10357</guid>
      <dc:creator>Govind89</dc:creator>
      <dc:date>2025-04-29T04:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Communication</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2089794#M10359</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234971"&gt;@Govind89&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your updated information.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I don't recommend modifying the NXP SDK demo code ,because it may introduce additional issues. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Since the NXP SDK demo is already well-optimized , and it was rigorously tested to ensure proper functionality, I suggest you refer to the example code as it is(when the demo runs ok, then you can modify the code you want to test). &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Additionally, I suggest you check&amp;nbsp; the README file for this demo to confirm your development environment is correctly configured.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mayliu1_0-1745985202094.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335705i2E7CB5080A5477E0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mayliu1_0-1745985202094.png" alt="mayliu1_0-1745985202094.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Wish it helps you.&lt;BR /&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Wish you a nice day!&lt;/P&gt;
&lt;P&gt;Best Regards&lt;BR /&gt;MayLiu&lt;/P&gt;</description>
      <pubDate>Wed, 30 Apr 2025 03:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2089794#M10359</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-04-30T03:55:54Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Communication</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2089827#M10361</link>
      <description>Thank you for your response. Additionally, I would like to inquire about communication between two RT boards using Ethernet. Both boards have 1 Gbps and 100 Mbps ports available. Could you please advise which example I should follow for this setup?</description>
      <pubDate>Wed, 30 Apr 2025 04:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2089827#M10361</guid>
      <dc:creator>Govind89</dc:creator>
      <dc:date>2025-04-30T04:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Communication</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2090579#M10365</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234971"&gt;@Govind89&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you can check the example in SDK import Wizard.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mayliu1_0-1746098335143.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335944i2EDE9580E2430E40/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mayliu1_0-1746098335143.png" alt="mayliu1_0-1746098335143.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;MayLiu&lt;/P&gt;</description>
      <pubDate>Thu, 01 May 2025 11:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Ethernet-Communication/m-p/2090579#M10365</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-05-01T11:19:42Z</dc:date>
    </item>
  </channel>
</rss>