<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic flash_config generation in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/flash-config-generation/m-p/2050287#M10270</link>
    <description>&lt;P&gt;I'm using a&amp;nbsp;MIMXRT685SFFOB with Winbond&amp;nbsp;W25Q128JV flash connected to FlexSPI A. I'm trying to use the mcuxpresso IDE to generate flash_config.c/.h for my zephyr based BSP, but the IDE never updates these files to match my configuration.&lt;BR /&gt;&lt;BR /&gt;My steps:&lt;BR /&gt;1) New C/C++ Project wizard -&amp;gt; select&amp;nbsp; MIMXRT685s&lt;BR /&gt;2) Pick&amp;nbsp;MIMXRT685SFFOB and add component: Board Components&amp;gt;Device&amp;gt;SDK Drivers&amp;gt; Select both flash_config&lt;BR /&gt;3) In Memory Configuration, I add Flash at location 0x800_0000 and size 0x100_0000 with driver MIMXRT600_FlexSPI_A_SFDP_QSPI.cfx&lt;BR /&gt;4) When the project is created, I can see the folder "flash_config" with the source and header file&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;However, flash_config.c always has .sFlashA1Size =0, .sFlashA2Size = 0, and .sFlashB1Size = 0x400_0000, which makes me believe this was not generated based off my parameters entered in the wizard. When I click Project Settings&amp;gt;Memory I do see the flash entry I created.&lt;BR /&gt;&lt;BR /&gt;What am I doing wrong to generate the flash_config I with my parameters?&lt;BR /&gt;&lt;BR /&gt;Also, I have followed the SuperMonkey QSPI bringup page and it doesn't help, but I do see their flash_config.c has .sFlashA1Size is non zero.&lt;BR /&gt;&lt;BR /&gt;Any help is appreciated!&lt;/P&gt;</description>
    <pubDate>Mon, 24 Feb 2025 23:00:47 GMT</pubDate>
    <dc:creator>rvanee</dc:creator>
    <dc:date>2025-02-24T23:00:47Z</dc:date>
    <item>
      <title>flash_config generation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/flash-config-generation/m-p/2050287#M10270</link>
      <description>&lt;P&gt;I'm using a&amp;nbsp;MIMXRT685SFFOB with Winbond&amp;nbsp;W25Q128JV flash connected to FlexSPI A. I'm trying to use the mcuxpresso IDE to generate flash_config.c/.h for my zephyr based BSP, but the IDE never updates these files to match my configuration.&lt;BR /&gt;&lt;BR /&gt;My steps:&lt;BR /&gt;1) New C/C++ Project wizard -&amp;gt; select&amp;nbsp; MIMXRT685s&lt;BR /&gt;2) Pick&amp;nbsp;MIMXRT685SFFOB and add component: Board Components&amp;gt;Device&amp;gt;SDK Drivers&amp;gt; Select both flash_config&lt;BR /&gt;3) In Memory Configuration, I add Flash at location 0x800_0000 and size 0x100_0000 with driver MIMXRT600_FlexSPI_A_SFDP_QSPI.cfx&lt;BR /&gt;4) When the project is created, I can see the folder "flash_config" with the source and header file&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;However, flash_config.c always has .sFlashA1Size =0, .sFlashA2Size = 0, and .sFlashB1Size = 0x400_0000, which makes me believe this was not generated based off my parameters entered in the wizard. When I click Project Settings&amp;gt;Memory I do see the flash entry I created.&lt;BR /&gt;&lt;BR /&gt;What am I doing wrong to generate the flash_config I with my parameters?&lt;BR /&gt;&lt;BR /&gt;Also, I have followed the SuperMonkey QSPI bringup page and it doesn't help, but I do see their flash_config.c has .sFlashA1Size is non zero.&lt;BR /&gt;&lt;BR /&gt;Any help is appreciated!&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 23:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/flash-config-generation/m-p/2050287#M10270</guid>
      <dc:creator>rvanee</dc:creator>
      <dc:date>2025-02-24T23:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: flash_config generation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/flash-config-generation/m-p/2052051#M10278</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247275"&gt;@rvanee&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The changes made in the project wizard's memory configuration are done for the Linker file, not the flash_config drivers. These drivers need to be changed manually by the user.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 17:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/flash-config-generation/m-p/2052051#M10278</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-02-26T17:59:53Z</dc:date>
    </item>
  </channel>
</rss>