<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 MCUXpresso IDE 11 &amp;amp; 24 cannot copy the source code when importing the PN7462 SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-amp-24-cannot-copy-the-source-code-when/m-p/1974910#M10086</link>
    <description>&lt;P&gt;大家好！咨询一个问题，比较着急。&lt;/P&gt;&lt;P&gt;使用MCUXpresso IDE 11 &amp;amp; 24开发PN7462的项目，下载了官方的sdk(SW3683.zip, NxpNfcRdLib_PN7462_v07.10.00_Pub.zip)，并按照UM10883文档的说明导入项目，但是只有这三个项目可以导入(NxpNfcRdLib, FreeRTOS, phOsal)源代码，其他的项目只能导入项目名字和结构目录，但是源代码无法导入。&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello everyone! I have a question and it’s quite urgent.&lt;/P&gt;&lt;P&gt;I am using MCUXpresso IDE 11 &amp;amp; 24 to develop a project for the PN7462. I downloaded the official SDKs (SW3683.zip, NxpNfcRdLib_PN7462_v07.10.00_Pub.zip) and followed the instructions in the UM10883 document to import the projects. However, only three projects (NxpNfcRdLib, FreeRTOS, phOsal) successfully imported with source code. For the other projects, only the project names and directory structures are imported, but the source code is missing.“​&lt;/P&gt;</description>
    <pubDate>Wed, 16 Oct 2024 07:18:48 GMT</pubDate>
    <dc:creator>Eric84</dc:creator>
    <dc:date>2024-10-16T07:18:48Z</dc:date>
    <item>
      <title>MCUXpresso IDE 11 &amp; 24 cannot copy the source code when importing the PN7462 SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-amp-24-cannot-copy-the-source-code-when/m-p/1974910#M10086</link>
      <description>&lt;P&gt;大家好！咨询一个问题，比较着急。&lt;/P&gt;&lt;P&gt;使用MCUXpresso IDE 11 &amp;amp; 24开发PN7462的项目，下载了官方的sdk(SW3683.zip, NxpNfcRdLib_PN7462_v07.10.00_Pub.zip)，并按照UM10883文档的说明导入项目，但是只有这三个项目可以导入(NxpNfcRdLib, FreeRTOS, phOsal)源代码，其他的项目只能导入项目名字和结构目录，但是源代码无法导入。&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello everyone! I have a question and it’s quite urgent.&lt;/P&gt;&lt;P&gt;I am using MCUXpresso IDE 11 &amp;amp; 24 to develop a project for the PN7462. I downloaded the official SDKs (SW3683.zip, NxpNfcRdLib_PN7462_v07.10.00_Pub.zip) and followed the instructions in the UM10883 document to import the projects. However, only three projects (NxpNfcRdLib, FreeRTOS, phOsal) successfully imported with source code. For the other projects, only the project names and directory structures are imported, but the source code is missing.“​&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 07:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-amp-24-cannot-copy-the-source-code-when/m-p/1974910#M10086</guid>
      <dc:creator>Eric84</dc:creator>
      <dc:date>2024-10-16T07:18:48Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE 11 &amp; 24 cannot copy the source code when importing the PN7462 SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-amp-24-cannot-copy-the-source-code-when/m-p/1975394#M10088</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You could try importing the library and demo application following the same steps that are described on the &lt;A href="https://www.nxp.com/docs/en/application-note/AN12550.pdf" target="_blank"&gt;AN12550&lt;/A&gt; Chapter 5.3.1. It's implemented on the PN5190 SDK, but it works fine for the PN7462 SDK.&lt;/P&gt;
&lt;P&gt;After you have followed the guide, the imported project shall be listed in the "Project Explorer" window, with all the sources.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Itzel_UV_0-1729100602204.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/305079i68E766C277F4C24D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Itzel_UV_0-1729100602204.png" alt="Itzel_UV_0-1729100602204.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Itzel_UV_0-1729100602204.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With this method you shouldn't have trouble importing the library, but if there are still some troubles, don't hesitate and come back with more questions.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Itzel&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 17:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-amp-24-cannot-copy-the-source-code-when/m-p/1975394#M10088</guid>
      <dc:creator>Itzel_UV</dc:creator>
      <dc:date>2024-10-16T17:47:08Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE 11 &amp; 24 cannot copy the source code when importing the PN7462 SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-amp-24-cannot-copy-the-source-code-when/m-p/1975670#M10089</link>
      <description>&lt;P&gt;Thank you so much!&lt;/P&gt;&lt;P&gt;I followed the method you shared, and it’s already resolved. I’m so happy!&lt;/P&gt;&lt;P&gt;However, I still hope that the related tutorials and IDE can support the direct integration of the SDK.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 03:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-amp-24-cannot-copy-the-source-code-when/m-p/1975670#M10089</guid>
      <dc:creator>Eric84</dc:creator>
      <dc:date>2024-10-17T03:37:50Z</dc:date>
    </item>
  </channel>
</rss>