<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Gui Flash Tool - Repeat on completion, programs only two times in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Gui-Flash-Tool-Repeat-on-completion-programs-only-two-times/m-p/1974225#M10085</link>
    <description>&lt;P&gt;I worked around the problem by using the LinkServer software.&lt;/P&gt;</description>
    <pubDate>Tue, 15 Oct 2024 11:16:21 GMT</pubDate>
    <dc:creator>wojtek327</dc:creator>
    <dc:date>2024-10-15T11:16:21Z</dc:date>
    <item>
      <title>Gui Flash Tool - Repeat on completion, programs only two times</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Gui-Flash-Tool-Repeat-on-completion-programs-only-two-times/m-p/1974095#M10084</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to program several boards using the GUI Flash Tool with MCU Link Pro. Programming LPC1769. I am using MCUXpresso IDE (MCUXpresso IDE v24.9 [Build 25] [2024-09-26]), and I have updated MCU Link Pro to the latest version. I checked the "Repeat on completion" flag. After clicking "Run," the tool successfully programs two boards, but on the third attempt, the programming process closes.&lt;/P&gt;&lt;P&gt;After clicking "Yes" to the prompt, "Do you want to perform the same operation again?" the programming stops, and I have to reopen the GUI Flash Tool. It seems like it can't reconnect with the probe after this. Is there any solution to this?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 09:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Gui-Flash-Tool-Repeat-on-completion-programs-only-two-times/m-p/1974095#M10084</guid>
      <dc:creator>wojtek327</dc:creator>
      <dc:date>2024-10-15T09:04:24Z</dc:date>
    </item>
    <item>
      <title>Re: Gui Flash Tool - Repeat on completion, programs only two times</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Gui-Flash-Tool-Repeat-on-completion-programs-only-two-times/m-p/1974225#M10085</link>
      <description>&lt;P&gt;I worked around the problem by using the LinkServer software.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 11:16:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Gui-Flash-Tool-Repeat-on-completion-programs-only-two-times/m-p/1974225#M10085</guid>
      <dc:creator>wojtek327</dc:creator>
      <dc:date>2024-10-15T11:16:21Z</dc:date>
    </item>
    <item>
      <title>Re: Gui Flash Tool - Repeat on completion, programs only two times</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Gui-Flash-Tool-Repeat-on-completion-programs-only-two-times/m-p/1974971#M10087</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241988"&gt;@wojtek327&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your sharing.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 08:19:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Gui-Flash-Tool-Repeat-on-completion-programs-only-two-times/m-p/1974971#M10087</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-10-16T08:19:55Z</dc:date>
    </item>
  </channel>
</rss>