<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config ToolsのトピックRe: K22F FSL_CLOCK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-FSL-CLOCK/m-p/974519#M822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oswaldo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl_clock is a driver for bus and core clock configuration of the selected device. You can write your own code to call the functions from this driver&amp;nbsp;in right order or you can you Config Tools, that will generate the initialization code for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use source clock for ADC peripheral, you can use peripheral tool, that allows to configure ADC driver (including source clock)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also start with any example project provided inside the SDK package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jun 2019 08:52:16 GMT</pubDate>
    <dc:creator>marek-trmac</dc:creator>
    <dc:date>2019-06-27T08:52:16Z</dc:date>
    <item>
      <title>K22F FSL_CLOCK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-FSL-CLOCK/m-p/974518#M821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;PRE class="" data-placeholder="Traducción" dir="ltr" style="text-align: left;"&gt;&lt;SPAN lang="en"&gt;Hello I do not know the function of the file fsl_clock. I want to make conditions so that I can choose which clock source to use,
 the modes of operation, divisors, and more. I'm working on the IAR compiler, MCUXpresso has the tools to guide me,
 but I do not want to be dependent on the software for the clock settings. But I think this file has those conditions but I'm not sure, can someone advise me?&lt;/SPAN&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2019 22:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-FSL-CLOCK/m-p/974518#M821</guid>
      <dc:creator>oswaldo-153</dc:creator>
      <dc:date>2019-06-26T22:03:33Z</dc:date>
    </item>
    <item>
      <title>Re: K22F FSL_CLOCK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-FSL-CLOCK/m-p/974519#M822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oswaldo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl_clock is a driver for bus and core clock configuration of the selected device. You can write your own code to call the functions from this driver&amp;nbsp;in right order or you can you Config Tools, that will generate the initialization code for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use source clock for ADC peripheral, you can use peripheral tool, that allows to configure ADC driver (including source clock)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also start with any example project provided inside the SDK package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jun 2019 08:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-FSL-CLOCK/m-p/974519#M822</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2019-06-27T08:52:16Z</dc:date>
    </item>
  </channel>
</rss>