<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config ToolsのトピックK22F CLOCK SETTINGS</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-CLOCK-SETTINGS/m-p/964868#M811</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to make some clock settings, I want to change the clock values of the system, the bus and the core.&lt;BR /&gt;But I'm not sure if it's in the clock_config.c file, can someone help me&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jun 2019 13:53:47 GMT</pubDate>
    <dc:creator>oswaldo-153</dc:creator>
    <dc:date>2019-06-24T13:53:47Z</dc:date>
    <item>
      <title>K22F CLOCK SETTINGS</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-CLOCK-SETTINGS/m-p/964868#M811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to make some clock settings, I want to change the clock values of the system, the bus and the core.&lt;BR /&gt;But I'm not sure if it's in the clock_config.c file, can someone help me&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 13:53:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-CLOCK-SETTINGS/m-p/964868#M811</guid>
      <dc:creator>oswaldo-153</dc:creator>
      <dc:date>2019-06-24T13:53:47Z</dc:date>
    </item>
    <item>
      <title>Re: K22F CLOCK SETTINGS</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-CLOCK-SETTINGS/m-p/964869#M812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="343007" data-username="oswaldo-153@hotmail.com" href="https://community.nxp.com/people/oswaldo-153@hotmail.com"&gt;Oswaldo Tovar&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Yes, you can config clock_config.c and clock_config.h files.&lt;/P&gt;&lt;P&gt;Also you can use MCUXpresso config tool about config Clocks to config it , then generate code,&lt;/P&gt;&lt;P&gt;this also set the code in clock_config.c and clock_config.h files:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89708i7665DC0BEC731BDC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jun 2019 08:30:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-CLOCK-SETTINGS/m-p/964869#M812</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-06-25T08:30:03Z</dc:date>
    </item>
    <item>
      <title>Re: K22F CLOCK SETTINGS</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-CLOCK-SETTINGS/m-p/964870#M813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oswaldo,&lt;/P&gt;&lt;P&gt;the file on the screenshot contains clock configuration file for new project created for processor, i.e.&amp;nbsp;the file contains&amp;nbsp;default clock configuration (bus and core). It is possible to import this configuration into Clocks tool, modify and update the file.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jun 2019 08:32:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/K22F-CLOCK-SETTINGS/m-p/964870#M813</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2019-06-25T08:32:14Z</dc:date>
    </item>
  </channel>
</rss>